BLE5-Stack 2.01.00 (SDK 3.30) to BLE5-Stack 2.01.01 (SDK 3.40)

This section will describe a way to migrate a project from BLE5-Stack 2.01.00 to a BLE5-Stack 2.01.01 project.

The changes you need to address to port your project:

  1. API changes (affecting RTLS example projects rtls_master/passive/slave):

    What is affected

    How to update

    RTLSAoa_processAoaResults()

    Function arguments: Change input order, add new and delete obsolete

    rtlsAoaConfigReq_t

    Remove struct member antArraySwitch, and rename member pAntArray renamed to pAntPattern

    RTLSCtrl_aoaResultEvt()

    Function arguments: Change input order, add new and delete obsolete

    RTLSCtrl_connResultEvt()

    Function arguments: Add new argument connHandle

    RTLSCtrl_initAntenna()

    Function arguments: Add new argument pinState

    RTLSCtrl_processDataSent()

    Function arguments: Add new argument connHandle

    RTLSCtrl_sendRtlsRemoteCmd()

    Function arguments: Add new argument connHandle

    RTLSCtrl_syncEventNotify()

    Function arguments: Add new argument connHandle

    RTLSCtrl_updateConnStateAndSyncEvt()

    Name: Rename to RTLSCtrl_updateConnState() Function arguments: Add new argument connHandle

    RTLSSrv_initAntArray()

    Function arguments: Only call with argument mainAntenna

  2. New link layer antenna structure cteAntProp_t, declared in ble_user_config.c, and is now used to control antenna switching. Edit this structure to run on custom AoA boards. See the Angle of Arrival section of the BLE5 User’s Guide and the Simplelink Academy AoA lab for more information.

  3. There are new values to use in the TX power back-off table. This table is declared in the txPwrBackoffVal_t structure in ble_user_config.c. The new defined values can be found in hci.h.

  4. The OAD example projects simple_peripheral_oad_onchip and simple_peripheral_oad_offchip include RCOSC calibration files (rcosc_calibration.c and rcosc_calibration.h).

  5. The crystal-less BAW wireless MCU, CC2652RB, is now supported by SysConfig in the example projects.

  6. XDCtools updated from version 3.60.00.24_core to 3.60.02.34_core.