BLE5-Stack 2.00.02 (SDK 3.10) to BLE5-Stack 2.00.03 (SDK 3.10)

This section will describe a way to migrate a project from BLE5-Stack 2.00.02 to a BLE5-Stack 2.00.03 project.

Note

BLE5-Stack 2.00.03 is identical to BLE5-Stack 2.00.02 except for CC1352P devices. If you’re not using CC1352P, there is no need to update to BLE5-Stack 2.00.03.

The only necessary changes when porting from BLE5-Stack 2.00.02 to BLE5-Stack 2.00.03 is related to RF settings.

  1. Replace the ble_user_config.c and ble_user_config.h files with the ones found in the BLE5-Stack 2.00.03. You can find these files at the following locations: <SDK_INSTALL_DIR>\source\ti\ble5stack\icall\app\ and <SDK_INSTALL_DIR>\source\ti\ble5stack\icall\inc\

  2. Double-check any HCI TX power defines used. In BLE5-Stack 2.00.03, the HCI_EXT_SetTxPowerCmd() has been updated to use a slightly different table of TX power defines. If you are using this command or any other command that takes a TX power define, please make sure you are using an existing define (listed below).

  • HCI_EXT_TX_POWER_MINUS_20_DBM

  • HCI_EXT_TX_POWER_MINUS_15_DBM

  • HCI_EXT_TX_POWER_MINUS_10_DBM

  • HCI_EXT_TX_POWER_MINUS_5_DBM

  • HCI_EXT_TX_POWER_0_DBM

  • HCI_EXT_TX_POWER_1_DBM

  • HCI_EXT_TX_POWER_2_DBM

  • HCI_EXT_TX_POWER_3_DBM

  • HCI_EXT_TX_POWER_4_DBM

  • HCI_EXT_TX_POWER_5_DBM

  • HCI_EXT_TX_POWER_14_DBM

  • HCI_EXT_TX_POWER_15_DBM

  • HCI_EXT_TX_POWER_16_DBM

  • HCI_EXT_TX_POWER_17_DBM

  • HCI_EXT_TX_POWER_18_DBM

  • HCI_EXT_TX_POWER_19_DBM

  • HCI_EXT_TX_POWER_20_DBM