![]() |
![]() |
SYS/BIOS
7.00
|
#include <ti/sysbios/knl/Mailbox.h>
Data Fields | |
IHeap_Handle | heap |
The IHeap instance used for dynamic creates. More... | |
Event_Handle | readerEvent |
Mailbox not empty event if using Events. Default is null. More... | |
unsigned int | readerEventId |
Mailbox not empty event Id if using Events. Default is 1. More... | |
Event_Handle | writerEvent |
Mailbox not full event if using Events. Default is null. More... | |
unsigned int | writerEventId |
Mailbox not full event Id if using Events. More... | |
void * | buf |
The address of the buffer used for creating messages. More... | |
unsigned int | bufSize |
The size of the buffer that 'buf' references. More... | |
IHeap_Handle Mailbox_Params::heap |
The IHeap instance used for dynamic creates.
This heap is used only for dynamic instances is ignored for static instances.
Event_Handle Mailbox_Params::readerEvent |
Mailbox not empty event if using Events. Default is null.
Posted whenever a mailbox is written to. Reader task pends on this event. Note that the configuration parameter Semaphore.supportsEvents has to be set to true for Mailbox to support Events.
unsigned int Mailbox_Params::readerEventId |
Mailbox not empty event Id if using Events. Default is 1.
Posted whenever a mailbox is written to. Reader task pends on this eventId. Note that the configuration parameter Semaphore.supportsEvents has to be set to true for Mailbox to support Events.
Event_Handle Mailbox_Params::writerEvent |
Mailbox not full event if using Events. Default is null.
Posted whenever a mailbox is read from. Writer task pends on this event. Note that the configuration parameter Semaphore.supportsEvents has to be set to true for Mailbox to support * Events.
unsigned int Mailbox_Params::writerEventId |
Mailbox not full event Id if using Events.
Posted whenever a mailbox is read from. Writer task pends on this eventId. Note that the configuration parameter Semaphore.supportsEvents has to be set to true for Mailbox to support Events.
void* Mailbox_Params::buf |
The address of the buffer used for creating messages.
This property is only used for dynamically created Mailboxes. If set to 'null', the messages will be allocated from the heap during runtime, otherwise the user may set this to a buffer of their creation to be used for allocating the messages.
The module will split the buf into "numMsgs" number of blocks (one block per Mailbox message).
Please note that if the buffer is user supplied, then it is the user's responsibility to ensure that it is aligned properly and is also large enough to contain "numMsgs" number of blocks. The size of each block is defined as follows:
Since the buffer must be a aligned properly, it may be necessary to 'round up' the total size of the buffer to the next multiple of the alignment for odd sized messages.
unsigned int Mailbox_Params::bufSize |
The size of the buffer that 'buf' references.
This property is only used for dynamically created Mailboxes.