SYS/BIOS  7.00
Data Fields
Hwi_Struct Struct Reference

#include <ti/sysbios/family/arm/v8m/Hwi.h>

Data Fields

uintptr_t arg
 ISR function argument. Default is 0. More...
 
Hwi_FuncPtr fxn
 
uintptr_t irp
 
uint8_t priority
 Interrupt priority. More...
 
int16_t intNum
 
void ** hookEnv
 

Field Documentation

§ arg

uintptr_t Hwi_Struct::arg

ISR function argument. Default is 0.

§ fxn

Hwi_FuncPtr Hwi_Struct::fxn

§ irp

uintptr_t Hwi_Struct::irp

§ priority

uint8_t Hwi_Struct::priority

Interrupt priority.

The default value of -1 is used as a flag to indicate the lowest (logical) device-specific priority value.

Not all targets/devices support this instance parameter. On those that don't, this parameter is ignored.

§ intNum

int16_t Hwi_Struct::intNum

§ hookEnv

void* * Hwi_Struct::hookEnv

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale