![]() |
![]() |
SYS/BIOS
7.00
|
Stat structure for the HeapBuf_getExtendedStats function. More...
#include <ti/sysbios/heaps/HeapBuf.h>
Data Fields | |
unsigned int | maxAllocatedBlocks |
The maximum number of blocks allocated from this heap at any single point in time, during the lifetime of this HeapBuf instance. The configuration parameter HeapBuf.trackMaxAllocs must be set to true for this field to have any meaning. Otherwise, this field will be set to '0'. More... | |
unsigned int | numAllocatedBlocks |
The total number of blocks currently allocated in this HeapBuf instance. More... | |
Stat structure for the HeapBuf_getExtendedStats function.
unsigned int HeapBuf_ExtendedStats::maxAllocatedBlocks |
The maximum number of blocks allocated from this heap at any single point in time, during the lifetime of this HeapBuf instance. The configuration parameter HeapBuf.trackMaxAllocs must be set to true for this field to have any meaning. Otherwise, this field will be set to '0'.
unsigned int HeapBuf_ExtendedStats::numAllocatedBlocks |
The total number of blocks currently allocated in this HeapBuf instance.