![]() |
![]() |
rflib
|
RAT related IO parameter structure. More...
#include <RFCC26X2.h>
Data Fields | |
RF_RatOutputMode | mode |
The mode the GPO should operate in. More... | |
RF_RatOutputSelect | select |
The signal which shall be connected to the GPO. More... | |
RAT related IO parameter structure.
These parameters are used with the RF_ratCompare() or RF_ratCapture() calls.
RF_RatOutputMode RF_RatConfigOutput::mode |
The mode the GPO should operate in.
RF_RatOutputSelect RF_RatConfigOutput::select |
The signal which shall be connected to the GPO.