![]() |
![]() |
NVSSPI25X attributes. More...
#include <NVSSPI25X.h>
Data Fields | |
size_t | regionBaseOffset |
size_t | regionSize |
size_t | sectorSize |
uint8_t * | verifyBuf |
size_t | verifyBufSize |
SPI_Handle * | spiHandle |
uint16_t | spiIndex |
uint32_t | spiBitRate |
uint16_t | spiCsnGpioIndex |
SPI Flash Chip Select GPIO index. More... | |
uint32_t | statusPollDelayUs |
External Flash Status Poll Delay. More... | |
NVSSPI25X attributes.
The 'regionBaseOffset' is the offset, in bytes, from the base of the SPI flash, of the flash region to be managed.
The 'regionSize' must be an integer multiple of the flash sector size.
The 'sectorSize' is SPI flash device specific. This parameter should correspond to the number of bytes erased when the 'SPIFLASH_SUBSECTOR_ERASE' (0x20) command is issued to the device.
The 'verifyBuf' and 'verifyBufSize' parameters are used by the NVS_write() command when either 'NVS_WRITE_PRE_VERIFY' or 'NVS_WRITE_POST_VERIFY' functions are requested in the 'flags' argument. The 'verifyBuf' is used to successively read back portions of the flash to compare with the data being written to it.
size_t NVSSPI25X_HWAttrs::regionBaseOffset |
Offset from base of SPI flash
size_t NVSSPI25X_HWAttrs::regionSize |
The size of the region in bytes
size_t NVSSPI25X_HWAttrs::sectorSize |
Erase sector size
uint8_t* NVSSPI25X_HWAttrs::verifyBuf |
Write Pre/Post verify buffer
size_t NVSSPI25X_HWAttrs::verifyBufSize |
Write Pre/Post verify buffer size
SPI_Handle* NVSSPI25X_HWAttrs::spiHandle |
ptr to SPI handle if provided by user.
uint16_t NVSSPI25X_HWAttrs::spiIndex |
SPI instance index from Board file
uint32_t NVSSPI25X_HWAttrs::spiBitRate |
SPI bit rate in Hz
uint16_t NVSSPI25X_HWAttrs::spiCsnGpioIndex |
SPI Flash Chip Select GPIO index.
This field should be set to either an index within the GPIO driver's GPIO_Config table, or to NVSSPI25X_SPI_MANAGES_CS. see SPI Flash Chip Select Management for more details.
uint32_t NVSSPI25X_HWAttrs::statusPollDelayUs |
External Flash Status Poll Delay.
This field determines how many microseconds the driver waits after querying the external flash status. Increasing this value can help mitigate CPU starvation if the external flash is busy for long periods of time, but may also result in increased latency.