![]() |
![]() |
A structure containing the parameters of an elliptic curve in short Weierstrass form. More...
#include <ECCParams.h>
Data Fields | |
const ECCParams_CurveType | curveType |
const uint8_t * | prime |
const uint8_t * | a |
const uint8_t * | b |
const uint8_t * | order |
uint8_t | cofactor |
const size_t | length |
const uint8_t * | generatorX |
const uint8_t * | generatorY |
A structure containing the parameters of an elliptic curve in short Weierstrass form.
Elliptical Curve Cryptography (ECC) prime curve.
The equation used to define the curve is expressed in the short Weierstrass form y^3 = x^2 + a*x + b
const ECCParams_CurveType ECCParams_CurveParams::curveType |
const uint8_t* ECCParams_CurveParams::prime |
const uint8_t* ECCParams_CurveParams::a |
const uint8_t* ECCParams_CurveParams::b |
const uint8_t* ECCParams_CurveParams::order |
uint8_t ECCParams_CurveParams::cofactor |
const size_t ECCParams_CurveParams::length |
const uint8_t* ECCParams_CurveParams::generatorX |
const uint8_t* ECCParams_CurveParams::generatorY |