![]() |
![]() |
ADCBufCC26XX Object. More...
#include <ADCBufCC26XX.h>
Data Fields | |
bool | isOpen |
bool | conversionInProgress |
bool | inputScalingEnabled |
bool | keepADCSemaphore |
bool | adcSemaphoreInPossession |
uint8_t | currentChannel |
ADCBufCC26XX_Reference_Source | refSource |
ADCBufCC26XX_Sampling_Mode | samplingMode |
ADCBufCC26XX_Sampling_Duration | samplingDuration |
ADCBuf_Callback | callbackFxn |
ADCBuf_Recurrence_Mode | recurrenceMode |
ADCBuf_Return_Mode | returnMode |
uint16_t * | activeSampleBuffer |
HwiP_Struct | hwi |
SwiP_Struct | swi |
SemaphoreP_Struct | conversionComplete |
ADCBuf_Conversion * | currentConversion |
PIN_State | pinState |
PIN_Handle | pinHandle |
UDMACC26XX_Handle | udmaHandle |
GPTimerCC26XX_Handle | timerHandle |
uint32_t | semaphoreTimeout |
uint32_t | samplingFrequency |
ADCBufCC26XX Object.
The application must not access any member variables of this structure!
bool ADCBufCC26XX_Object::isOpen |
< Has the obj been opened Is the ADC currently doing conversions
bool ADCBufCC26XX_Object::conversionInProgress |
Is the analogue input scaled
bool ADCBufCC26XX_Object::inputScalingEnabled |
Should the driver keep the ADC semaphore after a conversion
bool ADCBufCC26XX_Object::keepADCSemaphore |
Does the driver currently possess the ADC semaphore
bool ADCBufCC26XX_Object::adcSemaphoreInPossession |
The current virtual channel the ADCBuf driver is sampling on
uint8_t ADCBufCC26XX_Object::currentChannel |
Reference source for the ADC to use
ADCBufCC26XX_Reference_Source ADCBufCC26XX_Object::refSource |
Synchronous or asynchronous sampling mode
ADCBufCC26XX_Sampling_Mode ADCBufCC26XX_Object::samplingMode |
Time the ADC spends sampling in ADCBufCC26XX_SAMPING_MODE_SYNCHRONOUS
ADCBufCC26XX_Sampling_Duration ADCBufCC26XX_Object::samplingDuration |
Pointer to callback function
ADCBuf_Callback ADCBufCC26XX_Object::callbackFxn |
Should we convert continuously or one-shot
ADCBuf_Recurrence_Mode ADCBufCC26XX_Object::recurrenceMode |
Mode for all conversions
ADCBuf_Return_Mode ADCBufCC26XX_Object::returnMode |
The last complete sample buffer used by the DMA
uint16_t* ADCBufCC26XX_Object::activeSampleBuffer |
HwiP_Struct ADCBufCC26XX_Object::hwi |
< Hwi object Swi object
SwiP_Struct ADCBufCC26XX_Object::swi |
ADC semaphore
SemaphoreP_Struct ADCBufCC26XX_Object::conversionComplete |
Pointer to the current conversion struct
ADCBuf_Conversion* ADCBufCC26XX_Object::currentConversion |
PIN_State ADCBufCC26XX_Object::pinState |
< Pin state object Pin handle
PIN_Handle ADCBufCC26XX_Object::pinHandle |
UDMACC26XX_Handle ADCBufCC26XX_Object::udmaHandle |
< UDMA handle
GPTimerCC26XX_Handle ADCBufCC26XX_Object::timerHandle |
< Handle to underlying GPTimer peripheral Timeout for read semaphore in ADCBuf_RETURN_MODE_BLOCKING
uint32_t ADCBufCC26XX_Object::semaphoreTimeout |
Frequency in Hz at which the ADC is triggered
uint32_t ADCBufCC26XX_Object::samplingFrequency |