![]() |
![]() |
Power manager interface for CC26X2.
============================================================================
The Power header file should be included in an application as follows:
Refer to Power.h for a complete description of APIs.
This header file defines the power resources, constraints, events, sleep states and transition latencies for CC26X2.
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
#include <ti/drivers/Temperature.h>
#include <ti/devices/DeviceFamily.h>
Go to the source code of this file.
Data Structures | |
struct | PowerCC26X2_Config |
Global configuration structure. More... | |
struct | PowerCC26X2_ModuleState |
PowerCC26X2_ModuleState. More... | |
Macros | |
#define | PowerCC26X2_RESUMETIMESTANDBY 750 |
#define | PowerCC26X2_TOTALTIMESTANDBY 1000 |
#define | PowerCC26X2_WAKEDELAYSTANDBY 240 |
#define | PowerCC26X2_INITIALWAITRCOSC_LF 1000 |
#define | PowerCC26X2_RETRYWAITRCOSC_LF 1000 |
#define | PowerCC26X2_INITIALWAITXOSC_HF 50 |
#define | PowerCC26X2_RETRYWAITXOSC_HF 50 |
#define | PowerCC26X2_INITIALWAITXOSC_LF 10000 |
#define | PowerCC26X2_RETRYWAITXOSC_LF 5000 |
#define | PowerCC26X2_PERIPH_PKA PowerCC26XX_PERIPH_PKA |
#define | PowerCC26X2_PERIPH_UART1 PowerCC26XX_PERIPH_UART1 |
#define | PowerCC26X2_PERIPH_SSI1 PowerCC26XX_PERIPH_SSI1 |
#define | PowerCC26X2_PERIPH_UART2 PowerCC26XX_PERIPH_UART2 |
#define | PowerCC26X2_PERIPH_UART3 PowerCC26XX_PERIPH_UART3 |
#define | PowerCC26X2_PERIPH_SSI2 PowerCC26XX_PERIPH_SSI2 |
#define | PowerCC26X2_PERIPH_SSI3 PowerCC26XX_PERIPH_SSI3 |
#define | PowerCC26X2_PERIPH_I2C1 PowerCC26XX_PERIPH_I2C1 |
#define | PowerCC26X2_HPOSC_RTC_COMPENSATION_DELTA 3 |
Functions | |
void | PowerCC26X2_enableHposcRtcCompensation (void) |
Enable RTC compensation when SCLK_LF is derived from HPOSC. More... | |
#define PowerCC26X2_RESUMETIMESTANDBY 750 |
The latency to reserve for resume from STANDBY (usec).
#define PowerCC26X2_TOTALTIMESTANDBY 1000 |
The total latency to reserve for entry to and exit from STANDBY (usec).
#define PowerCC26X2_WAKEDELAYSTANDBY 240 |
The initial delay when waking from STANDBY (usec).
#define PowerCC26X2_INITIALWAITRCOSC_LF 1000 |
The initial wait time (usec) before checking if RCOSC_LF is stable.
#define PowerCC26X2_RETRYWAITRCOSC_LF 1000 |
The retry wait time (usec) when checking to see if RCOSC_LF is stable.
#define PowerCC26X2_INITIALWAITXOSC_HF 50 |
The initial wait time (usec) before checking if XOSC_HF is stable.
#define PowerCC26X2_RETRYWAITXOSC_HF 50 |
The retry wait time (usec) when checking to see if XOSC_HF is stable.
#define PowerCC26X2_INITIALWAITXOSC_LF 10000 |
The initial wait time (usec) before checking if XOSC_LF is stable.
#define PowerCC26X2_RETRYWAITXOSC_LF 5000 |
The retry wait time (usec) when checking to see if XOSC_LF is stable.
#define PowerCC26X2_PERIPH_PKA PowerCC26XX_PERIPH_PKA |
< Resource ID: PKA Module Resource ID: UART1
#define PowerCC26X2_PERIPH_UART1 PowerCC26XX_PERIPH_UART1 |
Resource ID: SSI1
#define PowerCC26X2_PERIPH_SSI1 PowerCC26XX_PERIPH_SSI1 |
#define PowerCC26X2_PERIPH_UART2 PowerCC26XX_PERIPH_UART2 |
< Resource ID: UART2 Resource ID: UART3
#define PowerCC26X2_PERIPH_UART3 PowerCC26XX_PERIPH_UART3 |
Resource ID: SSI2
#define PowerCC26X2_PERIPH_SSI2 PowerCC26XX_PERIPH_SSI2 |
Resource ID: SSI3
#define PowerCC26X2_PERIPH_SSI3 PowerCC26XX_PERIPH_SSI3 |
Resource ID: I2C1
#define PowerCC26X2_PERIPH_I2C1 PowerCC26XX_PERIPH_I2C1 |
#define PowerCC26X2_HPOSC_RTC_COMPENSATION_DELTA 3 |
The temperature delta in degrees C before the RTC is re-compensated when SCLK_LF is derived from SCLK_HF and SCLK_HF is supplied by HPOSC.
void PowerCC26X2_enableHposcRtcCompensation | ( | void | ) |
Enable RTC compensation when SCLK_LF is derived from HPOSC.
Enables automatic compensation for temperature based clock drift of the RTC when SCLK_LF is derived from HPOSC.
It only needs to be called once after the system boots.
This function should only be called when SCLK_LF is configured to be drived from HPOSC.