Data Structures | Macros | Typedefs | Functions | Variables
CryptoKey.h File Reference

Detailed Description

The CryptoKey type is an opaque representation of a cryptographic key.

============================================================================

Warning
This is a beta API. It may change in future releases.

Cryptographic keying material may be stored on an embedded system multiple ways.

Each storage option requires different approaches to handling the keying material when performing a crypto operation. In order to separate these concerns from the API of the various crypto drivers available with TI-RTOS, the CryptoKey type abstracts away from these details. It does not contain any cryptographic keying material itself but instead contains the details necessary for drivers to use the keying material. The driver implementation handles preparing and moving the keying material as necessary to perform the desired crypto operation.

The same CryptoKey may be passed to crypto APIs of different modes subject to restrictions placed on the key by their storage types. Plaintext keys may be used without restriction while key store keys have their permitted uses restricted when the keying material is loaded. These restrictions are specified in a CryptoKey_SecurityPolicy that is device-specific and depends on the hardware capability of the device.

An application should never access a field within a CryptoKey struct itself. Where needed, helper functions are provided to do so.

Before using a CryptoKey in another crypto API call, it must be initialized with a call to one of the initialization functions.

The keystore CryptoKeys may be used to load a key into a key store after its respective _init call.

CryptoKeys can be initialized "blank", without keying material but with an empty buffer or key store entry, to encode the destination of a key to be created in the future. This way, keys may be generated securely within a key store for example and never even be stored in RAM temporarily.

Not all devices support all CryptoKey functionality. This is hardware-dependent.

#include <stdint.h>
#include <stdbool.h>
Include dependency graph for CryptoKey.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  CryptoKey_Plaintext
 Plaintext CryptoKey datastructure. More...
 
struct  CryptoKey_KeyStore
 Key store CryptoKey datastructure. More...
 
struct  CryptoKey
 CryptoKey datastructure. More...
 

Macros

#define CryptoKey_STATUS_RESERVED   (-32)
 
#define CryptoKey_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define CryptoKey_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define CryptoKey_STATUS_UNDEFINED_ENCODING   (-2)
 Returned if the encoding of a CryptoKey is not a CryptoKey_Encoding value. More...
 

Typedefs

typedef uint8_t CryptoKey_Encoding
 List of the different types of CryptoKey. More...
 
typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy
 Structure that specifies the restrictions on a CryptoKey. More...
 

Functions

int_fast16_t CryptoKey_getCryptoKeyType (CryptoKey *keyHandle, CryptoKey_Encoding *keyType)
 Gets the key type of the CryptoKey. More...
 
int_fast16_t CryptoKey_isBlank (CryptoKey *keyHandle, bool *isBlank)
 Wheather the CryptoKey is 'blank' or represents valid keying material. More...
 
int_fast16_t CryptoKey_markAsBlank (CryptoKey *keyHandle)
 Marks a CryptoKey as 'blank'. More...
 
int_fast16_t CryptoKey_initSecurityPolicy (CryptoKey_SecurityPolicy *policy)
 Function to initialize the CryptoKey_SecurityPolicy struct to its defaults. More...
 

Variables

static const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U
 
static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U
 
static const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U
 
static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U
 

Typedef Documentation

§ CryptoKey_Encoding

typedef uint8_t CryptoKey_Encoding

List of the different types of CryptoKey.

§ CryptoKey_SecurityPolicy

typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy

Structure that specifies the restrictions on a CryptoKey.

This structure is device-specific and declared here in incomplete form. The structure is fully defined in CryptoKeyDEVICE.h. This creates a link-time binding when using the structure with key store functions. If the instance of the CryptoKey_SecurityPolicy is kept in a device-specific application-file, the generic application code may still use references to it despite being an incomplete type in the generic application file at compile time.

Function Documentation

§ CryptoKey_getCryptoKeyType()

int_fast16_t CryptoKey_getCryptoKeyType ( CryptoKey keyHandle,
CryptoKey_Encoding keyType 
)

Gets the key type of the CryptoKey.

Parameters
[in]keyHandlePointer to a CryptoKey
[out]keyTypeType of the CryptoKey
Returns
Returns a status code

§ CryptoKey_isBlank()

int_fast16_t CryptoKey_isBlank ( CryptoKey keyHandle,
bool *  isBlank 
)

Wheather the CryptoKey is 'blank' or represents valid keying material.

Parameters
[in]keyHandlePointer to a CryptoKey
[out]isBlankWheather the CryptoKey is 'blank' or not
Returns
Returns a status code

§ CryptoKey_markAsBlank()

int_fast16_t CryptoKey_markAsBlank ( CryptoKey keyHandle)

Marks a CryptoKey as 'blank'.

The CryptoKey will be unlinked from any previously connected keying material

Parameters
[in]keyHandlePointer to a CryptoKey
Returns
Returns a status code

§ CryptoKey_initSecurityPolicy()

int_fast16_t CryptoKey_initSecurityPolicy ( CryptoKey_SecurityPolicy policy)

Function to initialize the CryptoKey_SecurityPolicy struct to its defaults.

This will zero-out all fields that cannot be set to safe defaults

Parameters
[in]policyPointer to a CryptoKey_SecurityPolicy
Returns
Returns a status code

Variable Documentation

§ CryptoKey_PLAINTEXT

const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U
static

§ CryptoKey_BLANK_PLAINTEXT

const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U
static

§ CryptoKey_KEYSTORE

const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U
static

§ CryptoKey_BLANK_KEYSTORE

const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U
static
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale