TI-15.4 Stack API
4.40.00.12
|
#include <api_mac.h>
Data Fields | |
ApiMac_sAddr_t | coordAddress |
uint16_t | coordPanId |
uint16_t | superframeSpec |
uint8_t | logicalChannel |
uint8_t | channelPage |
bool | gtsPermit |
uint8_t | linkQuality |
uint32_t | timestamp |
bool | securityFailure |
ApiMac_sec_t | sec |
PAN descriptor type
ApiMac_sAddr_t _apimac_pandesc::coordAddress |
The address of the coordinator sending the beacon
uint16_t _apimac_pandesc::coordPanId |
The PAN ID of the network
uint16_t _apimac_pandesc::superframeSpec |
The superframe specification of the network, this field contains the beacon order, superframe order, final CAP slot, battery life extension, PAN coordinator bit, and association permit flag. Use the following macros to parse this field: APIMAC_SFS_BEACON_ORDER(), APIMAC_SFS_SUPERFRAME_ORDER(), APIMAC_SFS_FINAL_CAP_SLOT() APIMAC_SFS_BLE(), APIMAC_SFS_PAN_COORDINATOR(), and APIMAC_SFS_ASSOCIATION_PERMIT().
uint8_t _apimac_pandesc::logicalChannel |
The logical channel of the network
uint8_t _apimac_pandesc::channelPage |
The current channel page occupied by the network
bool _apimac_pandesc::gtsPermit |
TRUE if coordinator accepts GTS requests. This field is not used for enhanced beacons.
uint8_t _apimac_pandesc::linkQuality |
The link quality of the received beacon
uint32_t _apimac_pandesc::timestamp |
The time at which the beacon was received, in backoffs
bool _apimac_pandesc::securityFailure |
TRUE if there was an error in the security processing
ApiMac_sec_t _apimac_pandesc::sec |
The security parameters for the received beacon frame