#include <rf_ieee_cmd.h>
|
struct { |
uint8_t corr:6 |
| The correlation value. More...
|
|
uint8_t bIgnore:1 |
| 1 if the packet should be rejected by frame filtering, 0 otherwise More...
|
|
uint8_t bCrcErr:1 |
| 1 if the packet was received with CRC error, 0 otherwise More...
|
|
} | status |
|
struct { |
uint8_t corr:6 |
| The correlation value. More...
|
|
uint8_t bIgnore:1 |
| 1 if the packet should be rejected by frame filtering, 0 otherwise More...
|
|
uint8_t bCrcErr:1 |
| 1 if the packet was received with CRC error, 0 otherwise More...
|
|
} | status |
|
struct { |
uint8_t corr:6 |
| The correlation value. More...
|
|
uint8_t bIgnore:1 |
| 1 if the packet should be rejected by frame filtering, 0 otherwise More...
|
|
uint8_t bCrcErr:1 |
| 1 if the packet was received with CRC error, 0 otherwise More...
|
|
} | status |
|
§ corr
uint8_t rfc_ieeeRxCorrCrc_s::corr |
§ bIgnore
uint8_t rfc_ieeeRxCorrCrc_s::bIgnore |
1 if the packet should be rejected by frame filtering, 0 otherwise
§ bCrcErr
uint8_t rfc_ieeeRxCorrCrc_s::bCrcErr |
1 if the packet was received with CRC error, 0 otherwise
§ status [1/3]
struct { ... } rfc_ieeeRxCorrCrc_s::status |
§ status [2/3]
struct { ... } rfc_ieeeRxCorrCrc_s::status |
§ status [3/3]
struct { ... } rfc_ieeeRxCorrCrc_s::status |
The documentation for this struct was generated from the following file: