#include <rf_ieee_coex.h>
§ __dummy0
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy0 |
§ __dummy1
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy1 |
§ __dummy2
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy2 |
§ __dummy3
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy3 |
§ __dummy4
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy4 |
§ __dummy5
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy5 |
§ __dummy6
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy6 |
§ __dummy7
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy7 |
§ __dummy8
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy8 |
§ __dummy9
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy9 |
§ __dummy10
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy10 |
§ __dummy11
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy11 |
§ __dummy12
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy12 |
§ __dummy13
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy13 |
§ __dummy14
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy14 |
§ __dummy15
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy15 |
§ __dummy16
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy16 |
§ __dummy17
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy17 |
§ __dummy18
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy18 |
§ __dummy19
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy19 |
§ __dummy20
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy20 |
§ __dummy21
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy21 |
§ __dummy22
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy22 |
§ __dummy23
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy23 |
§ __dummy24
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy24 |
§ __dummy25
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy25 |
§ __dummy26
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy26 |
§ __dummy27
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy27 |
§ __dummy28
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy28 |
§ __dummy29
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy29 |
§ __dummy30
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy30 |
§ __dummy31
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy31 |
§ __dummy32
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy32 |
§ __dummy33
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy33 |
§ __dummy34
uint32_t rfc_ieeeCoexGlobalEnable_s::__dummy34 |
§ __dummy35
uint16_t rfc_ieeeCoexGlobalEnable_s::__dummy35 |
§ __dummy36
uint8_t rfc_ieeeCoexGlobalEnable_s::__dummy36 |
§ coExGlobalEnable
uint8_t rfc_ieeeCoexGlobalEnable_s::coExGlobalEnable |
0 = CoEx features disabled. All other values = CoEx enabled.
The documentation for this struct was generated from the following file: