#include <rf_ble_cmd.h>
§ nTxScanReq
uint16_t rfc_bleScannerOutput_s::nTxScanReq |
Number of transmitted SCAN_REQ packets.
§ nBackedOffScanReq
uint16_t rfc_bleScannerOutput_s::nBackedOffScanReq |
Number of SCAN_REQ packets not sent due to backoff procedure.
§ nRxAdvOk
uint16_t rfc_bleScannerOutput_s::nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored.
§ nRxAdvIgnored
uint16_t rfc_bleScannerOutput_s::nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored.
§ nRxAdvNok
uint16_t rfc_bleScannerOutput_s::nRxAdvNok |
Number of ADV*_IND packets received with CRC error.
§ nRxScanRspOk
uint16_t rfc_bleScannerOutput_s::nRxScanRspOk |
Number of SCAN_RSP packets received with CRC OK and not ignored.
§ nRxScanRspIgnored
uint16_t rfc_bleScannerOutput_s::nRxScanRspIgnored |
Number of SCAN_RSP packets received with CRC OK, but ignored.
§ nRxScanRspNok
uint16_t rfc_bleScannerOutput_s::nRxScanRspNok |
Number of SCAN_RSP packets received with CRC error.
§ nRxAdvBufFull
uint8_t rfc_bleScannerOutput_s::nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue.
§ nRxScanRspBufFull
uint8_t rfc_bleScannerOutput_s::nRxScanRspBufFull |
Number of SCAN_RSP packets received that did not fit in Rx queue.
§ lastRssi
int8_t rfc_bleScannerOutput_s::lastRssi |
The RSSI of the last received packet (signed)
§ __dummy0
uint8_t rfc_bleScannerOutput_s::__dummy0 |
§ timeStamp
ratmr_t rfc_bleScannerOutput_s::timeStamp |
Time stamp of the last successfully received ADV*_IND packet that was not ignored.
The documentation for this struct was generated from the following file: