#include <rf_ble_cmd.h>
§ nRxOk
uint16_t rfc_bleGenericRxOutput_s::nRxOk |
Number of packets received with CRC OK.
§ nRxNok
uint16_t rfc_bleGenericRxOutput_s::nRxNok |
Number of packets received with CRC error.
§ nRxBufFull
uint16_t rfc_bleGenericRxOutput_s::nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space.
§ lastRssi
int8_t rfc_bleGenericRxOutput_s::lastRssi |
The RSSI of the last received packet (signed)
§ __dummy0
uint8_t rfc_bleGenericRxOutput_s::__dummy0 |
§ timeStamp
ratmr_t rfc_bleGenericRxOutput_s::timeStamp |
Time stamp of the last received packet.
The documentation for this struct was generated from the following file: