#include <rf_ble_cmd.h>
|
uint16_t | nTxReq |
| Number of transmitted AUX_SCAN_REQ, SCAN_REQ, AUX_CONNECT_REQ, or CONNECT_IND packets. More...
|
|
uint16_t | nBackedOffReq |
| Number of AUX_SCAN_REQ, SCAN_REQ, or AUX_CONNECT_REQ packets not sent due to backoff procedure. More...
|
|
uint16_t | nRxAdvOk |
| Number of ADV*_IND packets received with CRC OK and not ignored. More...
|
|
uint16_t | nRxAdvIgnored |
| Number of ADV*_IND packets received with CRC OK, but ignored. More...
|
|
uint16_t | nRxAdvNok |
| Number of ADV*_IND packets received with CRC error. More...
|
|
uint16_t | nRxRspOk |
| Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC OK and not ignored. More...
|
|
uint16_t | nRxRspIgnored |
| Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC OK, but ignored. More...
|
|
uint16_t | nRxRspNok |
| Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC error. More...
|
|
uint8_t | nRxAdvBufFull |
| Number of ADV*_IND packets received that did not fit in Rx queue. More...
|
|
uint8_t | nRxRspBufFull |
| Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received that did not fit in Rx queue. More...
|
|
int8_t | lastRssi |
| The RSSI of the last received packet (signed) More...
|
|
uint8_t | __dummy0 |
|
ratmr_t | timeStamp |
| Time stamp of the last successfully received ADV_IND packet that was not ignored. More...
|
|
§ nTxReq
uint16_t rfc_ble5ScanInitOutput_s::nTxReq |
Number of transmitted AUX_SCAN_REQ, SCAN_REQ, AUX_CONNECT_REQ, or CONNECT_IND packets.
§ nBackedOffReq
uint16_t rfc_ble5ScanInitOutput_s::nBackedOffReq |
Number of AUX_SCAN_REQ, SCAN_REQ, or AUX_CONNECT_REQ packets not sent due to backoff procedure.
§ nRxAdvOk
uint16_t rfc_ble5ScanInitOutput_s::nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored.
§ nRxAdvIgnored
uint16_t rfc_ble5ScanInitOutput_s::nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored.
§ nRxAdvNok
uint16_t rfc_ble5ScanInitOutput_s::nRxAdvNok |
Number of ADV*_IND packets received with CRC error.
§ nRxRspOk
uint16_t rfc_ble5ScanInitOutput_s::nRxRspOk |
Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC OK and not ignored.
§ nRxRspIgnored
uint16_t rfc_ble5ScanInitOutput_s::nRxRspIgnored |
Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC OK, but ignored.
§ nRxRspNok
uint16_t rfc_ble5ScanInitOutput_s::nRxRspNok |
Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received with CRC error.
§ nRxAdvBufFull
uint8_t rfc_ble5ScanInitOutput_s::nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue.
§ nRxRspBufFull
uint8_t rfc_ble5ScanInitOutput_s::nRxRspBufFull |
Number of AUX_SCAN_RSP, SCAN_RSP, or AUX_CONNECT_RSP packets received that did not fit in Rx queue.
§ lastRssi
int8_t rfc_ble5ScanInitOutput_s::lastRssi |
The RSSI of the last received packet (signed)
§ __dummy0
uint8_t rfc_ble5ScanInitOutput_s::__dummy0 |
§ timeStamp
ratmr_t rfc_ble5ScanInitOutput_s::timeStamp |
Time stamp of the last successfully received ADV_IND packet that was not ignored.
The documentation for this struct was generated from the following file: