#include <rf_ble_cmd.h>
|
uint16_t | __dummy0 |
|
uint8_t | __dummy1 |
|
uint8_t | auxPtrTargetType |
| Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed. More...
|
|
ratmr_t | auxPtrTargetTime |
| Time of start of packet to which auxPtr points. More...
|
|
uint8_t * | pAdvPkt |
| Pointer to extended advertising packet for the ADV_EXT_IND packet. More...
|
|
uint32_t | accessAddress |
| Access address used on the periodic advertisement. More...
|
|
uint8_t | crcInit0 |
| CRC initialization value used on the periodic advertisement – least significant byte. More...
|
|
uint8_t | crcInit1 |
| CRC initialization value used on the periodic advertisement – middle byte. More...
|
|
uint8_t | crcInit2 |
| CRC initialization value used on the periodic advertisement – most significant byte. More...
|
|
§ __dummy0
uint16_t rfc_ble5AdvPerPar_s::__dummy0 |
§ __dummy1
uint8_t rfc_ble5AdvPerPar_s::__dummy1 |
§ auxPtrTargetType
uint8_t rfc_ble5AdvPerPar_s::auxPtrTargetType |
Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed.
§ auxPtrTargetTime
ratmr_t rfc_ble5AdvPerPar_s::auxPtrTargetTime |
Time of start of packet to which auxPtr points.
§ pAdvPkt
uint8_t * rfc_ble5AdvPerPar_s::pAdvPkt |
Pointer to extended advertising packet for the ADV_EXT_IND packet.
§ accessAddress
uint32_t rfc_ble5AdvPerPar_s::accessAddress |
Access address used on the periodic advertisement.
§ crcInit0
uint8_t rfc_ble5AdvPerPar_s::crcInit0 |
CRC initialization value used on the periodic advertisement – least significant byte.
§ crcInit1
uint8_t rfc_ble5AdvPerPar_s::crcInit1 |
CRC initialization value used on the periodic advertisement – middle byte.
§ crcInit2
uint8_t rfc_ble5AdvPerPar_s::crcInit2 |
CRC initialization value used on the periodic advertisement – most significant byte.
The documentation for this struct was generated from the following file: