#include <rf_ble_cmd.h>
§ __pad0__
uint8_t rfc_ble5AdvExtPar_s::__pad0__ |
§ deviceAddrType
uint8_t rfc_ble5AdvExtPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
§ advConfig [1/3]
struct { ... } rfc_ble5AdvExtPar_s::advConfig |
§ __dummy0
uint8_t rfc_ble5AdvExtPar_s::__dummy0 |
§ __dummy1
uint8_t rfc_ble5AdvExtPar_s::__dummy1 |
§ auxPtrTargetType
uint8_t rfc_ble5AdvExtPar_s::auxPtrTargetType |
Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed.
§ auxPtrTargetTime
ratmr_t rfc_ble5AdvExtPar_s::auxPtrTargetTime |
Time of start of packet to which auxPtr points.
§ pAdvPkt
uint8_t * rfc_ble5AdvExtPar_s::pAdvPkt |
Pointer to extended advertising packet for the ADV_EXT_IND packet.
§ pDeviceAddress
uint16_t * rfc_ble5AdvExtPar_s::pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType
is inverted.
§ advConfig [2/3]
struct { ... } rfc_ble5AdvExtPar_s::advConfig |
§ advConfig [3/3]
struct { ... } rfc_ble5AdvExtPar_s::advConfig |
The documentation for this struct was generated from the following file: