rflib
|
Go to the source code of this file.
Macros | |
Operation finished normally | |
#define | HID_DONE_OK 0x5400 |
Operation ended normally. More... | |
#define | HID_DONE_RXTIMEOUT 0x5401 |
Operation stopped after end trigger while waiting for sync. More... | |
#define | HID_DONE_NOSYNC 0x5402 |
Timeout of subsequent Rx. More... | |
#define | HID_DONE_RXERR 0x5403 |
Operation ended after CRC error. More... | |
#define | HID_DONE_ENDED 0x5404 |
Operation stopped after end trigger during reception. More... | |
#define | HID_DONE_STOPPED 0x5405 |
Operation stopped after stop command. More... | |
#define | HID_DONE_ABORT 0x5406 |
Operation aborted by abort command. More... | |
Operation finished with error | |
#define | HID_ERROR_PAR 0x5800 |
Illegal parameter. More... | |
#define | HID_ERROR_RXBUF 0x5801 |
No available Rx buffer at the start of a packet. More... | |
#define | HID_ERROR_NO_SETUP 0x5802 |
Radio was not set up in a compatible mode. More... | |
#define | HID_ERROR_NO_FS 0x5803 |
Synth was not programmed when running Rx or Tx. More... | |
#define | HID_ERROR_RXOVF 0x5804 |
Rx overflow observed during operation. More... | |
#define | HID_ERROR_TXUNF 0x5805 |
Tx underflow observed during operation. More... | |
#define HID_DONE_OK 0x5400 |
Operation ended normally.
#define HID_DONE_RXTIMEOUT 0x5401 |
Operation stopped after end trigger while waiting for sync.
#define HID_DONE_NOSYNC 0x5402 |
Timeout of subsequent Rx.
#define HID_DONE_RXERR 0x5403 |
Operation ended after CRC error.
#define HID_DONE_ENDED 0x5404 |
Operation stopped after end trigger during reception.
#define HID_DONE_STOPPED 0x5405 |
Operation stopped after stop command.
#define HID_DONE_ABORT 0x5406 |
Operation aborted by abort command.
#define HID_ERROR_PAR 0x5800 |
Illegal parameter.
#define HID_ERROR_RXBUF 0x5801 |
No available Rx buffer at the start of a packet.
#define HID_ERROR_NO_SETUP 0x5802 |
Radio was not set up in a compatible mode.
#define HID_ERROR_NO_FS 0x5803 |
Synth was not programmed when running Rx or Tx.
#define HID_ERROR_RXOVF 0x5804 |
Rx overflow observed during operation.
#define HID_ERROR_TXUNF 0x5805 |
Tx underflow observed during operation.