AESCTRDRBGXX Object. More...
#include <AESCTRDRBGXX.h>
Data Fields | |
uint8_t | keyingMaterial [AESCTRDRBG_AES_KEY_LENGTH_256] |
uint8_t | counter [AESCTRDRBG_AES_BLOCK_SIZE_BYTES] |
CryptoKey | key |
AESCTR_Handle | ctrHandle |
size_t | seedLength |
uint32_t | reseedCounter |
uint32_t | reseedInterval |
int_fast16_t | returnStatus |
bool | isOpen |
bool | isInstantiated |
AESCTRDRBGXX Object.
The application must not access any member variables of this structure!
uint8_t AESCTRDRBGXX_Object::keyingMaterial[AESCTRDRBG_AES_KEY_LENGTH_256] |
uint8_t AESCTRDRBGXX_Object::counter[AESCTRDRBG_AES_BLOCK_SIZE_BYTES] |
CryptoKey AESCTRDRBGXX_Object::key |
AESCTR_Handle AESCTRDRBGXX_Object::ctrHandle |
size_t AESCTRDRBGXX_Object::seedLength |
uint32_t AESCTRDRBGXX_Object::reseedCounter |
uint32_t AESCTRDRBGXX_Object::reseedInterval |
int_fast16_t AESCTRDRBGXX_Object::returnStatus |
bool AESCTRDRBGXX_Object::isOpen |
bool AESCTRDRBGXX_Object::isInstantiated |