Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message for one-step operations.
More...
#include <AESCCM.h>
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message for one-step operations.
§ key
§ aad
uint8_t* AESCCM_OneStepOperation::aad |
A buffer of length aadLength
containing additional authentication data to be authenticated/verified but not encrypted/decrypted.
§ input
uint8_t* AESCCM_OneStepOperation::input |
- Encryption: The plaintext buffer to be encrypted and authenticated in the CCM operation.
- Decryption: The ciphertext to be decrypted and verified.
§ output
uint8_t* AESCCM_OneStepOperation::output |
- Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
- Decryption: The plaintext derived from the decrypted and verified ciphertext is copied here.
§ nonce
uint8_t* AESCCM_OneStepOperation::nonce |
A buffer containing a nonce. Nonces must be unique to each CCM operation and may not be reused. If nonceInternallyGenerated is set, the nonce will be generated by AESCCM_oneStepEncrypt() and copied to this buffer.
§ mac
uint8_t* AESCCM_OneStepOperation::mac |
- Encryption: The buffer where the message authentication code is copied.
- Decryption: The buffer containing the received message authentication code.
§ aadLength
size_t AESCCM_OneStepOperation::aadLength |
Length of the total aad
in bytes. Either aadLength
or inputLength
must be non-zero. Unlike this field in AESCCM_SegmentedAADOperation, the length doesn't need to be block-aligned.
§ inputLength
size_t AESCCM_OneStepOperation::inputLength |
Length of the input/output data in bytes. Either aadLength
or inputLength
must be non-zero. Unlike this field in AESCCM_SegmentedDataOperation, the length doesn't need to be block-aligned.
§ nonceLength
uint8_t AESCCM_OneStepOperation::nonceLength |
Length of nonce
in bytes. Valid nonce lengths are [7, 8, ... 13].
§ macLength
uint8_t AESCCM_OneStepOperation::macLength |
Length of mac
in bytes. Valid MAC lengths are [0, 4, 6, 8, 10, 12, 14, 16]. A length of 0 disables authentication and verification. This is only permitted when using CCM*.
§ nonceInternallyGenerated
bool AESCCM_OneStepOperation::nonceInternallyGenerated |
When true, the nonce buffer passed into AESCCM_oneStepEncrypt() will be overwritten with a randomly generated nonce. Not supported by all implementations.
The documentation for this struct was generated from the following file: