NoRTOS framework global configuration. More...
#include <NoRTOS.h>
Data Fields | |
void(* | idleCallback )(void) |
uint32_t | clockTickPeriod |
int | swiIntNum |
NoRTOS framework global configuration.
The NoRTOS_Config structure contains a set of values utilized by the NoRTOS framework.
The NoRTOS_getConfig() API can be used to retrieve the current settings. When changing one or more of these settings, a NoRTOS_Config structure should first be populated with the current settings by calling NoRTOS_getConfig(), after which the particular setting(s) that needs to be changed should be set and given to the NoRTOS framework by calling NoRTOS_setConfig().
void(* _NoRTOS_Config::idleCallback) (void) |
Function that is called when a TI Driver "suspends" its operation
uint32_t _NoRTOS_Config::clockTickPeriod |
Period of the internal Clock module's periodic "tick" (microsecs)
int _NoRTOS_Config::swiIntNum |
Hardware interrupt posted by software to achieve the Swi (Software interrupt) scheduling paradigm