Define a typedef for deprecated operation AESCBC_Operation. Existing code should be refactored to use AESCBC_OneStepOperation. This reference may be removed at some point in the future
Define a typedef for deprecated operation AESCCM_Operation. Existing code should be refactored to use AESCCM_OneStepOperation. This reference may be removed at some point in the future
Define a typedef for deprecated operation AESCTR_Operation. Existing code should be refactored to use AESCTR_OneStepOperation. This reference may be removed at some point in the future.
Define a typedef for deprecated operation AESGCM_Operation. Existing code should be refactored to use AESGCM_OneStepOperation. This reference may be removed at some point in the future