49 #ifndef ti_drivers_ecdsa_ECDSACC26X1__include 50 #define ti_drivers_ecdsa_ECDSACC26X1__include 59 #include <ti/devices/DeviceFamily.h> 60 #include DeviceFamily_constructPath(driverlib/rom_ecc.h) 98 uint32_t eccWorkZone[288];
TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:608
ECDSACC26X1 Object.
Definition: ECDSACC26X1.h:93
uint8_t trngIntPriority
TRNG Peripheral's interrupt priority.
Definition: ECDSACC26X1.h:85
TRNG driver implementation for the CC26XX family.
bool isOpen
Definition: ECDSACC26X1.h:94
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSACC26X1.h:96
ECDSA_CallbackFxn callbackFxn
Definition: ECDSACC26X1.h:95
ECDSACC26X1 Hardware Attributes.
Definition: ECDSACC26X1.h:72
ECC_State eccState
Definition: ECDSACC26X1.h:97