CC26xx Driver Library
rom.h File Reference
#include "../inc/hw_types.h"

Data Structures

struct  HARD_API_T
 

Macros

#define __HAPI_H__
 
#define ROM_HAPI_TABLE_ADDR   0x10000048
 
#define P_HARD_API   ((HARD_API_T*) ROM_HAPI_TABLE_ADDR)
 
#define HapiCrc32(a, b, c)   P_HARD_API->Crc32(a,b,c)
 
#define HapiGetFlashSize()   P_HARD_API->FlashGetSize()
 
#define HapiGetChipId()   P_HARD_API->GetChipId()
 
#define HapiSectorErase(a)   MemBusWrkAroundHapiEraseSector(a)
 
#define HapiProgramFlash(a, b, c)   MemBusWrkAroundHapiProgramFlash(a,b,c)
 
#define HapiResetDevice()   P_HARD_API->ResetDevice()
 
#define HapiFletcher32(a, b, c)   P_HARD_API->Fletcher32(a,b,c)
 
#define HapiMinValue(a, b)   P_HARD_API->MinValue(a,b)
 
#define HapiMaxValue(a, b)   P_HARD_API->MaxValue(a,b)
 
#define HapiMeanValue(a, b)   P_HARD_API->MeanValue(a,b)
 
#define HapiStandDeviationValue(a, b)   P_HARD_API->StandDeviationValue(a,b)
 
#define HapiHFSourceSafeSwitch()   P_HARD_API->HFSourceSafeSwitch()
 
#define HapiSelectCompAInput(a)   P_HARD_API->SelectCompAInput(a)
 
#define HapiSelectCompARef(a)   P_HARD_API->SelectCompARef(a)
 
#define HapiSelectADCCompBInput(a)   P_HARD_API->SelectADCCompBInput(a)
 
#define HapiSelectDACVref(a)   P_HARD_API->SelectDACVref(a)
 
#define COMPA_IN_NC   0x00
 
#define COMPA_IN_AUXIO7   0x09
 
#define COMPA_IN_AUXIO6   0x0A
 
#define COMPA_IN_AUXIO5   0x0B
 
#define COMPA_IN_AUXIO4   0x0C
 
#define COMPA_IN_AUXIO3   0x0D
 
#define COMPA_IN_AUXIO2   0x0E
 
#define COMPA_IN_AUXIO1   0x0F
 
#define COMPA_IN_AUXIO0   0x10
 
#define COMPA_IN_AUXIO26   COMPA_IN_AUXIO7
 
#define COMPA_IN_AUXIO25   COMPA_IN_AUXIO6
 
#define COMPA_IN_AUXIO24   COMPA_IN_AUXIO5
 
#define COMPA_IN_AUXIO23   COMPA_IN_AUXIO4
 
#define COMPA_IN_AUXIO22   COMPA_IN_AUXIO3
 
#define COMPA_IN_AUXIO21   COMPA_IN_AUXIO2
 
#define COMPA_IN_AUXIO20   COMPA_IN_AUXIO1
 
#define COMPA_IN_AUXIO19   COMPA_IN_AUXIO0
 
#define COMPA_REF_NC   0x00
 
#define COMPA_REF_DCOUPL   0x01
 
#define COMPA_REF_VSS   0x02
 
#define COMPA_REF_VDDS   0x03
 
#define COMPA_REF_ADCVREFP   0x04
 
#define COMPA_REF_AUXIO7   0x09
 
#define COMPA_REF_AUXIO6   0x0A
 
#define COMPA_REF_AUXIO5   0x0B
 
#define COMPA_REF_AUXIO4   0x0C
 
#define COMPA_REF_AUXIO3   0x0D
 
#define COMPA_REF_AUXIO2   0x0E
 
#define COMPA_REF_AUXIO1   0x0F
 
#define COMPA_REF_AUXIO0   0x10
 
#define COMPA_REF_AUXIO26   COMPA_REF_AUXIO7
 
#define COMPA_REF_AUXIO25   COMPA_REF_AUXIO6
 
#define COMPA_REF_AUXIO24   COMPA_REF_AUXIO5
 
#define COMPA_REF_AUXIO23   COMPA_REF_AUXIO4
 
#define COMPA_REF_AUXIO22   COMPA_REF_AUXIO3
 
#define COMPA_REF_AUXIO21   COMPA_REF_AUXIO2
 
#define COMPA_REF_AUXIO20   COMPA_REF_AUXIO1
 
#define COMPA_REF_AUXIO19   COMPA_REF_AUXIO0
 
#define ADC_COMPB_IN_NC   0x00
 
#define ADC_COMPB_IN_DCOUPL   0x03
 
#define ADC_COMPB_IN_VSS   0x04
 
#define ADC_COMPB_IN_VDDS   0x05
 
#define ADC_COMPB_IN_AUXIO7   0x09
 
#define ADC_COMPB_IN_AUXIO6   0x0A
 
#define ADC_COMPB_IN_AUXIO5   0x0B
 
#define ADC_COMPB_IN_AUXIO4   0x0C
 
#define ADC_COMPB_IN_AUXIO3   0x0D
 
#define ADC_COMPB_IN_AUXIO2   0x0E
 
#define ADC_COMPB_IN_AUXIO1   0x0F
 
#define ADC_COMPB_IN_AUXIO0   0x10
 
#define ADC_COMPB_IN_AUXIO26   ADC_COMPB_IN_AUXIO7
 
#define ADC_COMPB_IN_AUXIO25   ADC_COMPB_IN_AUXIO6
 
#define ADC_COMPB_IN_AUXIO24   ADC_COMPB_IN_AUXIO5
 
#define ADC_COMPB_IN_AUXIO23   ADC_COMPB_IN_AUXIO4
 
#define ADC_COMPB_IN_AUXIO22   ADC_COMPB_IN_AUXIO3
 
#define ADC_COMPB_IN_AUXIO21   ADC_COMPB_IN_AUXIO2
 
#define ADC_COMPB_IN_AUXIO20   ADC_COMPB_IN_AUXIO1
 
#define ADC_COMPB_IN_AUXIO19   ADC_COMPB_IN_AUXIO0
 
#define DAC_REF_NC   0x00
 
#define DAC_REF_DCOUPL   0x01
 
#define DAC_REF_VSS   0x02
 
#define DAC_REF_VDDS   0x03
 
#define ROM_API_TABLE   ((uint32_t *) 0x10000180)
 
#define ROM_VERSION   (ROM_API_TABLE[0])
 
#define ROM_API_AON_EVENT_TABLE   ((uint32_t*) (ROM_API_TABLE[1]))
 
#define ROM_API_AON_IOC_TABLE   ((uint32_t*) (ROM_API_TABLE[2]))
 
#define ROM_API_AON_RTC_TABLE   ((uint32_t*) (ROM_API_TABLE[3]))
 
#define ROM_API_AUX_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[5]))
 
#define ROM_API_AUX_TDC_TABLE   ((uint32_t*) (ROM_API_TABLE[6]))
 
#define ROM_API_DDI_TABLE   ((uint32_t*) (ROM_API_TABLE[9]))
 
#define ROM_API_FLASH_TABLE   ((uint32_t*) (ROM_API_TABLE[10]))
 
#define ROM_API_I2C_TABLE   ((uint32_t*) (ROM_API_TABLE[11]))
 
#define ROM_API_INTERRUPT_TABLE   ((uint32_t*) (ROM_API_TABLE[12]))
 
#define ROM_API_IOC_TABLE   ((uint32_t*) (ROM_API_TABLE[13]))
 
#define ROM_API_PRCM_TABLE   ((uint32_t*) (ROM_API_TABLE[14]))
 
#define ROM_API_SMPH_TABLE   ((uint32_t*) (ROM_API_TABLE[15]))
 
#define ROM_API_SSI_TABLE   ((uint32_t*) (ROM_API_TABLE[17]))
 
#define ROM_API_TIMER_TABLE   ((uint32_t*) (ROM_API_TABLE[18]))
 
#define ROM_API_TRNG_TABLE   ((uint32_t*) (ROM_API_TABLE[19]))
 
#define ROM_API_UART_TABLE   ((uint32_t*) (ROM_API_TABLE[20]))
 
#define ROM_API_UDMA_TABLE   ((uint32_t*) (ROM_API_TABLE[21]))
 
#define ROM_API_VIMS_TABLE   ((uint32_t*) (ROM_API_TABLE[22]))
 
#define ROM_API_OSC_TABLE   ((uint32_t*) (ROM_API_TABLE[24]))
 
#define ROM_API_AUX_ADC_TABLE   ((uint32_t*) (ROM_API_TABLE[25]))
 
#define ROM_API_SYS_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[26]))
 
#define ROM_API_AON_BATMON_TABLE   ((uint32_t*) (ROM_API_TABLE[27]))
 
#define ROM_API_SETUP_ROM_TABLE   ((uint32_t*) (ROM_API_TABLE[28]))
 
#define ROM_API_I2S_TABLE   ((uint32_t*) (ROM_API_TABLE[29]))
 
#define ROM_API_PWR_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[30]))
 
#define ROM_API_AES_TABLE   ((uint32_t*) (ROM_API_TABLE[31]))
 
#define ROM_API_PKA_TABLE   ((uint32_t*) (ROM_API_TABLE[32]))
 
#define ROM_API_SHA2_TABLE   ((uint32_t*) (ROM_API_TABLE[33]))
 
#define ROM_AONEventMcuWakeUpSet
 
#define ROM_AONEventMcuWakeUpGet
 
#define ROM_AONEventMcuSet
 
#define ROM_AONEventMcuGet
 
#define ROM_AONRTCCurrent64BitValueGet
 
#define ROM_AUXTDCConfigSet
 
#define ROM_AUXTDCMeasurementDone
 
#define ROM_DDI16BitWrite
 
#define ROM_DDI16BitfieldWrite
 
#define ROM_DDI16BitRead
 
#define ROM_DDI16BitfieldRead
 
#define ROM_DDI32RegWrite
 
#define ROM_FlashProtectionSet
 
#define ROM_FlashProtectionGet
 
#define ROM_FlashProtectionSave
 
#define ROM_FlashEfuseReadRow
 
#define ROM_FlashDisableSectorsForWrite
 
#define ROM_I2CMasterInitExpClk
 
#define ROM_I2CMasterErr
 
#define ROM_IntPriorityGroupingSet
 
#define ROM_IntPriorityGroupingGet
 
#define ROM_IntPrioritySet
 
#define ROM_IntPriorityGet
 
#define ROM_IntEnable
 
#define ROM_IntDisable
 
#define ROM_IntPendSet
 
#define ROM_IntPendGet
 
#define ROM_IntPendClear
 
#define ROM_IOCPortConfigureSet
 
#define ROM_IOCPortConfigureGet
 
#define ROM_IOCIOShutdownSet
 
#define ROM_IOCIOModeSet
 
#define ROM_IOCIOIntSet
 
#define ROM_IOCIOPortPullSet
 
#define ROM_IOCIOHystSet
 
#define ROM_IOCIOInputSet
 
#define ROM_IOCIOSlewCtrlSet
 
#define ROM_IOCIODrvStrengthSet
 
#define ROM_IOCIOPortIdSet
 
#define ROM_IOCIntEnable
 
#define ROM_IOCIntDisable
 
#define ROM_IOCPinTypeGpioInput
 
#define ROM_IOCPinTypeGpioOutput
 
#define ROM_IOCPinTypeUart
 
#define ROM_IOCPinTypeSsiMaster
 
#define ROM_IOCPinTypeSsiSlave
 
#define ROM_IOCPinTypeI2c
 
#define ROM_IOCPinTypeAux
 
#define ROM_PRCMInfClockConfigureSet
 
#define ROM_PRCMInfClockConfigureGet
 
#define ROM_PRCMAudioClockConfigSet
 
#define ROM_PRCMPowerDomainOn
 
#define ROM_PRCMPowerDomainOff
 
#define ROM_PRCMPeripheralRunEnable
 
#define ROM_PRCMPeripheralRunDisable
 
#define ROM_PRCMPeripheralSleepEnable
 
#define ROM_PRCMPeripheralSleepDisable
 
#define ROM_PRCMPeripheralDeepSleepEnable
 
#define ROM_PRCMPeripheralDeepSleepDisable
 
#define ROM_PRCMDeepSleep
 
#define ROM_PRCMAudioClockConfigSetOverride
 
#define ROM_SMPHAcquire
 
#define ROM_SSIConfigSetExpClk
 
#define ROM_SSIDataPut
 
#define ROM_SSIDataPutNonBlocking
 
#define ROM_SSIDataGet
 
#define ROM_SSIDataGetNonBlocking
 
#define ROM_TimerConfigure
 
#define ROM_TimerLevelControl
 
#define ROM_TimerStallControl
 
#define ROM_TimerWaitOnTriggerControl
 
#define ROM_TimerIntervalLoadMode
 
#define ROM_TimerMatchUpdateMode
 
#define ROM_TRNGConfigure
 
#define ROM_TRNGNumberGet
 
#define ROM_UARTFIFOLevelGet
 
#define ROM_UARTConfigSetExpClk
 
#define ROM_UARTConfigGetExpClk
 
#define ROM_UARTDisable
 
#define ROM_UARTCharGetNonBlocking
 
#define ROM_UARTCharGet
 
#define ROM_UARTCharPutNonBlocking
 
#define ROM_UARTCharPut
 
#define ROM_uDMAChannelAttributeEnable
 
#define ROM_uDMAChannelAttributeDisable
 
#define ROM_uDMAChannelAttributeGet
 
#define ROM_uDMAChannelControlSet
 
#define ROM_uDMAChannelTransferSet
 
#define ROM_uDMAChannelScatterGatherSet
 
#define ROM_uDMAChannelSizeGet
 
#define ROM_uDMAChannelModeGet
 
#define ROM_VIMSConfigure
 
#define ROM_VIMSModeSet
 
#define ROM_VIMSModeGet
 
#define ROM_VIMSModeSafeSet
 
#define ROM_OSCClockSourceGet
 
#define ROM_OSCClockSourceSet
 
#define ROM_OSC_HPOSCRelativeFrequencyOffsetToRFCoreFormatConvert
 
#define ROM_AUXADCAdjustValueForGainAndOffset
 
#define ROM_AUXADCDisable
 
#define ROM_AUXADCDisableInputScaling
 
#define ROM_AUXADCEnableAsync
 
#define ROM_AUXADCEnableSyncNoBugWorkaround
 
#define ROM_AUXADCFlushFifo
 
#define ROM_AUXADCGetAdjustmentGain
 
#define ROM_AUXADCGetAdjustmentOffset
 
#define ROM_AUXADCMicrovoltsToValue
 
#define ROM_AUXADCPopFifo
 
#define ROM_AUXADCReadFifo
 
#define ROM_AUXADCUnadjustValueForGainAndOffset
 
#define ROM_AUXADCValueToMicrovolts
 
#define ROM_SysCtrlResetSourceGet
 
#define ROM_SysCtrl_DCDC_VoltageConditionalControl
 
#define ROM_AONBatMonTemperatureGetDegC
 
#define ROM_SetupAfterColdResetWakeupFromShutDownCfg1
 
#define ROM_SetupAfterColdResetWakeupFromShutDownCfg2
 
#define ROM_SetupAfterColdResetWakeupFromShutDownCfg3
 
#define ROM_SetupGetTrimForAdcShModeEn
 
#define ROM_SetupGetTrimForAdcShVbufEn
 
#define ROM_SetupGetTrimForAmpcompCtrl
 
#define ROM_SetupGetTrimForAmpcompTh1
 
#define ROM_SetupGetTrimForAmpcompTh2
 
#define ROM_SetupGetTrimForAnabypassValue1
 
#define ROM_SetupGetTrimForDblrLoopFilterResetVoltage
 
#define ROM_SetupGetTrimForRadcExtCfg
 
#define ROM_SetupGetTrimForRcOscLfIBiasTrim
 
#define ROM_SetupGetTrimForRcOscLfRtuneCtuneTrim
 
#define ROM_SetupGetTrimForXoscHfCtl
 
#define ROM_SetupGetTrimForXoscHfFastStart
 
#define ROM_SetupGetTrimForXoscHfIbiastherm
 
#define ROM_SetupGetTrimForXoscLfRegulatorAndCmirrwrRatio
 
#define ROM_SetupSetAonRtcSubSecInc
 
#define ROM_SetupSetCacheModeAccordingToCcfgSetting
 
#define ROM_SetupStepVddrTrimTo
 
#define ROM_I2SPointerSet
 
#define ROM_I2SSampleStampGet
 
#define ROM_PowerCtrlSourceSet
 
#define ROM_AESConfigureCCMCtrl
 
#define ROM_AESReadFromKeyStore
 
#define ROM_AESReadTag
 
#define ROM_AESSetInitializationVector
 
#define ROM_AESStartDMAOperation
 
#define ROM_AESVerifyTag
 
#define ROM_AESWaitForIRQFlags
 
#define ROM_AESWriteCCMInitializationVector
 
#define ROM_PKABigNumAddGetResult
 
#define ROM_PKABigNumCmpGetResult
 
#define ROM_PKABigNumInvModGetResult
 
#define ROM_PKABigNumModGetResult
 
#define ROM_PKABigNumMultGetResult
 
#define ROM_PKAEccAddGetResult
 
#define ROM_PKAEccAddStart
 
#define ROM_PKAEccMultiplyGetResult
 
#define ROM_PKAEccMultiplyStart
 
#define ROM_PKAGetOpsStatus
 
#define ROM_PKABigNumAddStart
 
#define ROM_PKABigNumCmpStart
 
#define ROM_PKABigNumInvModStart
 
#define ROM_PKABigNumModStart
 
#define ROM_PKABigNumMultiplyStart
 
#define ROM_PKABigNumSubGetResult
 
#define ROM_PKABigNumSubStart
 
#define ROM_PKAArrayAllZeros
 
#define ROM_PKABigNumDivideGetQuotient
 
#define ROM_PKABigNumDivideGetRemainder
 
#define ROM_PKABigNumDivideStart
 
#define ROM_PKAEccVerifyPublicKeyWeierstrassStart
 
#define ROM_PKAZeroOutArray
 
#define ROM_PKAEccMontgomeryMultiplyStart
 
#define ROM_SHA2ComputeFinalHash
 
#define ROM_SHA2ComputeHash
 
#define ROM_SHA2ComputeInitialHash
 
#define ROM_SHA2ComputeIntermediateHash
 
#define ROM_SHA2StartDMAOperation
 
#define ROM_SHA2WaitForIRQFlags
 

Typedefs

typedef uint32_t(* FPTR_CRC32_T) (uint8_t *, uint32_t, uint32_t)
 
typedef uint32_t(* FPTR_GETFLSIZE_T) (void)
 
typedef uint32_t(* FPTR_GETCHIPID_T) (void)
 
typedef uint32_t(* FPTR_RESERVED1_T) (uint32_t)
 
typedef uint32_t(* FPTR_RESERVED2_T) (void)
 
typedef uint32_t(* FPTR_RESERVED3_T) (uint8_t *, uint32_t, uint32_t)
 
typedef void(* FPTR_RESETDEV_T) (void)
 
typedef uint32_t(* FPTR_FLETCHER32_T) (uint16_t *, uint16_t, uint16_t)
 
typedef uint32_t(* FPTR_MINVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_MAXVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_MEANVAL_T) (uint32_t *, uint32_t)
 
typedef uint32_t(* FPTR_STDDVAL_T) (uint32_t *, uint32_t)
 
typedef void(* FPTR_HFSOURCESAFESWITCH_T) (void)
 
typedef void(* FPTR_RESERVED4_T) (uint32_t)
 
typedef void(* FPTR_RESERVED5_T) (uint32_t)
 
typedef void(* FPTR_COMPAIN_T) (uint8_t)
 
typedef void(* FPTR_COMPAREF_T) (uint8_t)
 
typedef void(* FPTR_ADCCOMPBIN_T) (uint8_t)
 
typedef void(* FPTR_DACVREF_T) (uint8_t)
 

Functions

uint32_t MemBusWrkAroundHapiProgramFlash (uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
 
uint32_t MemBusWrkAroundHapiEraseSector (uint32_t ui32Address)
 

Macro Definition Documentation

§ __HAPI_H__

#define __HAPI_H__

§ ADC_COMPB_IN_AUXIO0

#define ADC_COMPB_IN_AUXIO0   0x10

§ ADC_COMPB_IN_AUXIO1

#define ADC_COMPB_IN_AUXIO1   0x0F

§ ADC_COMPB_IN_AUXIO19

#define ADC_COMPB_IN_AUXIO19   ADC_COMPB_IN_AUXIO0

§ ADC_COMPB_IN_AUXIO2

#define ADC_COMPB_IN_AUXIO2   0x0E

§ ADC_COMPB_IN_AUXIO20

#define ADC_COMPB_IN_AUXIO20   ADC_COMPB_IN_AUXIO1

§ ADC_COMPB_IN_AUXIO21

#define ADC_COMPB_IN_AUXIO21   ADC_COMPB_IN_AUXIO2

§ ADC_COMPB_IN_AUXIO22

#define ADC_COMPB_IN_AUXIO22   ADC_COMPB_IN_AUXIO3

§ ADC_COMPB_IN_AUXIO23

#define ADC_COMPB_IN_AUXIO23   ADC_COMPB_IN_AUXIO4

§ ADC_COMPB_IN_AUXIO24

#define ADC_COMPB_IN_AUXIO24   ADC_COMPB_IN_AUXIO5

§ ADC_COMPB_IN_AUXIO25

#define ADC_COMPB_IN_AUXIO25   ADC_COMPB_IN_AUXIO6

§ ADC_COMPB_IN_AUXIO26

#define ADC_COMPB_IN_AUXIO26   ADC_COMPB_IN_AUXIO7

§ ADC_COMPB_IN_AUXIO3

#define ADC_COMPB_IN_AUXIO3   0x0D

§ ADC_COMPB_IN_AUXIO4

#define ADC_COMPB_IN_AUXIO4   0x0C

§ ADC_COMPB_IN_AUXIO5

#define ADC_COMPB_IN_AUXIO5   0x0B

§ ADC_COMPB_IN_AUXIO6

#define ADC_COMPB_IN_AUXIO6   0x0A

§ ADC_COMPB_IN_AUXIO7

#define ADC_COMPB_IN_AUXIO7   0x09

§ ADC_COMPB_IN_DCOUPL

#define ADC_COMPB_IN_DCOUPL   0x03

§ ADC_COMPB_IN_NC

#define ADC_COMPB_IN_NC   0x00

§ ADC_COMPB_IN_VDDS

#define ADC_COMPB_IN_VDDS   0x05

§ ADC_COMPB_IN_VSS

#define ADC_COMPB_IN_VSS   0x04

§ COMPA_IN_AUXIO0

#define COMPA_IN_AUXIO0   0x10

§ COMPA_IN_AUXIO1

#define COMPA_IN_AUXIO1   0x0F

§ COMPA_IN_AUXIO19

#define COMPA_IN_AUXIO19   COMPA_IN_AUXIO0

§ COMPA_IN_AUXIO2

#define COMPA_IN_AUXIO2   0x0E

§ COMPA_IN_AUXIO20

#define COMPA_IN_AUXIO20   COMPA_IN_AUXIO1

§ COMPA_IN_AUXIO21

#define COMPA_IN_AUXIO21   COMPA_IN_AUXIO2

§ COMPA_IN_AUXIO22

#define COMPA_IN_AUXIO22   COMPA_IN_AUXIO3

§ COMPA_IN_AUXIO23

#define COMPA_IN_AUXIO23   COMPA_IN_AUXIO4

§ COMPA_IN_AUXIO24

#define COMPA_IN_AUXIO24   COMPA_IN_AUXIO5

§ COMPA_IN_AUXIO25

#define COMPA_IN_AUXIO25   COMPA_IN_AUXIO6

§ COMPA_IN_AUXIO26

#define COMPA_IN_AUXIO26   COMPA_IN_AUXIO7

§ COMPA_IN_AUXIO3

#define COMPA_IN_AUXIO3   0x0D

§ COMPA_IN_AUXIO4

#define COMPA_IN_AUXIO4   0x0C

§ COMPA_IN_AUXIO5

#define COMPA_IN_AUXIO5   0x0B

§ COMPA_IN_AUXIO6

#define COMPA_IN_AUXIO6   0x0A

§ COMPA_IN_AUXIO7

#define COMPA_IN_AUXIO7   0x09

§ COMPA_IN_NC

#define COMPA_IN_NC   0x00

§ COMPA_REF_ADCVREFP

#define COMPA_REF_ADCVREFP   0x04

§ COMPA_REF_AUXIO0

#define COMPA_REF_AUXIO0   0x10

§ COMPA_REF_AUXIO1

#define COMPA_REF_AUXIO1   0x0F

§ COMPA_REF_AUXIO19

#define COMPA_REF_AUXIO19   COMPA_REF_AUXIO0

§ COMPA_REF_AUXIO2

#define COMPA_REF_AUXIO2   0x0E

§ COMPA_REF_AUXIO20

#define COMPA_REF_AUXIO20   COMPA_REF_AUXIO1

§ COMPA_REF_AUXIO21

#define COMPA_REF_AUXIO21   COMPA_REF_AUXIO2

§ COMPA_REF_AUXIO22

#define COMPA_REF_AUXIO22   COMPA_REF_AUXIO3

§ COMPA_REF_AUXIO23

#define COMPA_REF_AUXIO23   COMPA_REF_AUXIO4

§ COMPA_REF_AUXIO24

#define COMPA_REF_AUXIO24   COMPA_REF_AUXIO5

§ COMPA_REF_AUXIO25

#define COMPA_REF_AUXIO25   COMPA_REF_AUXIO6

§ COMPA_REF_AUXIO26

#define COMPA_REF_AUXIO26   COMPA_REF_AUXIO7

§ COMPA_REF_AUXIO3

#define COMPA_REF_AUXIO3   0x0D

§ COMPA_REF_AUXIO4

#define COMPA_REF_AUXIO4   0x0C

§ COMPA_REF_AUXIO5

#define COMPA_REF_AUXIO5   0x0B

§ COMPA_REF_AUXIO6

#define COMPA_REF_AUXIO6   0x0A

§ COMPA_REF_AUXIO7

#define COMPA_REF_AUXIO7   0x09

§ COMPA_REF_DCOUPL

#define COMPA_REF_DCOUPL   0x01

§ COMPA_REF_NC

#define COMPA_REF_NC   0x00

§ COMPA_REF_VDDS

#define COMPA_REF_VDDS   0x03

§ COMPA_REF_VSS

#define COMPA_REF_VSS   0x02

§ DAC_REF_DCOUPL

#define DAC_REF_DCOUPL   0x01

§ DAC_REF_NC

#define DAC_REF_NC   0x00

§ DAC_REF_VDDS

#define DAC_REF_VDDS   0x03

§ DAC_REF_VSS

#define DAC_REF_VSS   0x02

§ HapiCrc32

#define HapiCrc32 (   a,
  b,
 
)    P_HARD_API->Crc32(a,b,c)

§ HapiFletcher32

#define HapiFletcher32 (   a,
  b,
 
)    P_HARD_API->Fletcher32(a,b,c)

§ HapiGetChipId

#define HapiGetChipId ( )    P_HARD_API->GetChipId()

§ HapiGetFlashSize

#define HapiGetFlashSize ( )    P_HARD_API->FlashGetSize()

§ HapiHFSourceSafeSwitch

#define HapiHFSourceSafeSwitch ( )    P_HARD_API->HFSourceSafeSwitch()

Referenced by OSCHfSourceSwitch().

§ HapiMaxValue

#define HapiMaxValue (   a,
 
)    P_HARD_API->MaxValue(a,b)

§ HapiMeanValue

#define HapiMeanValue (   a,
 
)    P_HARD_API->MeanValue(a,b)

§ HapiMinValue

#define HapiMinValue (   a,
 
)    P_HARD_API->MinValue(a,b)

§ HapiProgramFlash

#define HapiProgramFlash (   a,
  b,
 
)    MemBusWrkAroundHapiProgramFlash(a,b,c)

§ HapiResetDevice

#define HapiResetDevice ( )    P_HARD_API->ResetDevice()

§ HapiSectorErase

#define HapiSectorErase (   a)    MemBusWrkAroundHapiEraseSector(a)

§ HapiSelectADCCompBInput

#define HapiSelectADCCompBInput (   a)    P_HARD_API->SelectADCCompBInput(a)

Referenced by AUXADCSelectInput().

§ HapiSelectCompAInput

#define HapiSelectCompAInput (   a)    P_HARD_API->SelectCompAInput(a)

§ HapiSelectCompARef

#define HapiSelectCompARef (   a)    P_HARD_API->SelectCompARef(a)

§ HapiSelectDACVref

#define HapiSelectDACVref (   a)    P_HARD_API->SelectDACVref(a)

§ HapiStandDeviationValue

#define HapiStandDeviationValue (   a,
 
)    P_HARD_API->StandDeviationValue(a,b)

§ P_HARD_API

#define P_HARD_API   ((HARD_API_T*) ROM_HAPI_TABLE_ADDR)

§ ROM_AESConfigureCCMCtrl

#define ROM_AESConfigureCCMCtrl
Value:
((void (*)(uint32_t nonceLength, uint32_t macLength, bool encrypt)) \
ROM_API_AES_TABLE[0])

§ ROM_AESReadFromKeyStore

#define ROM_AESReadFromKeyStore
Value:
((uint32_t (*)(uint32_t keyStoreArea)) \
ROM_API_AES_TABLE[1])

§ ROM_AESReadTag

#define ROM_AESReadTag
Value:
((uint32_t (*)(uint8_t *tag, uint32_t tagLength)) \
ROM_API_AES_TABLE[2])

§ ROM_AESSetInitializationVector

#define ROM_AESSetInitializationVector
Value:
((void (*)(const uint32_t *initializationVector)) \
ROM_API_AES_TABLE[3])

§ ROM_AESStartDMAOperation

#define ROM_AESStartDMAOperation
Value:
((void (*)(const uint8_t *channel0Addr, uint32_t channel0Length, uint8_t *channel1Addr, uint32_t channel1Length)) \
ROM_API_AES_TABLE[4])

§ ROM_AESVerifyTag

#define ROM_AESVerifyTag
Value:
((uint32_t (*)(const uint8_t *tag, uint32_t tagLength)) \
ROM_API_AES_TABLE[5])

§ ROM_AESWaitForIRQFlags

#define ROM_AESWaitForIRQFlags
Value:
((uint32_t (*)(uint32_t irqFlags)) \
ROM_API_AES_TABLE[6])

§ ROM_AESWriteCCMInitializationVector

#define ROM_AESWriteCCMInitializationVector
Value:
((void (*)(const uint8_t *nonce, uint32_t nonceLength)) \
ROM_API_AES_TABLE[7])

§ ROM_AONBatMonTemperatureGetDegC

#define ROM_AONBatMonTemperatureGetDegC
Value:
((int32_t (*)(void)) \
ROM_API_AON_BATMON_TABLE[0])

§ ROM_AONEventMcuGet

#define ROM_AONEventMcuGet
Value:
((uint32_t (*)(uint32_t ui32MCUEvent)) \
ROM_API_AON_EVENT_TABLE[5])

§ ROM_AONEventMcuSet

#define ROM_AONEventMcuSet
Value:
((void (*)(uint32_t ui32MCUEvent, uint32_t ui32EventSrc)) \
ROM_API_AON_EVENT_TABLE[4])

§ ROM_AONEventMcuWakeUpGet

#define ROM_AONEventMcuWakeUpGet
Value:
((uint32_t (*)(uint32_t ui32MCUWUEvent)) \
ROM_API_AON_EVENT_TABLE[1])

§ ROM_AONEventMcuWakeUpSet

#define ROM_AONEventMcuWakeUpSet
Value:
((void (*)(uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc)) \
ROM_API_AON_EVENT_TABLE[0])

§ ROM_AONRTCCurrent64BitValueGet

#define ROM_AONRTCCurrent64BitValueGet
Value:
((uint64_t (*)(void)) \
ROM_API_AON_RTC_TABLE[12])

§ ROM_API_AES_TABLE

#define ROM_API_AES_TABLE   ((uint32_t*) (ROM_API_TABLE[31]))

§ ROM_API_AON_BATMON_TABLE

#define ROM_API_AON_BATMON_TABLE   ((uint32_t*) (ROM_API_TABLE[27]))

§ ROM_API_AON_EVENT_TABLE

#define ROM_API_AON_EVENT_TABLE   ((uint32_t*) (ROM_API_TABLE[1]))

§ ROM_API_AON_IOC_TABLE

#define ROM_API_AON_IOC_TABLE   ((uint32_t*) (ROM_API_TABLE[2]))

§ ROM_API_AON_RTC_TABLE

#define ROM_API_AON_RTC_TABLE   ((uint32_t*) (ROM_API_TABLE[3]))

§ ROM_API_AUX_ADC_TABLE

#define ROM_API_AUX_ADC_TABLE   ((uint32_t*) (ROM_API_TABLE[25]))

§ ROM_API_AUX_CTRL_TABLE

#define ROM_API_AUX_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[5]))

§ ROM_API_AUX_TDC_TABLE

#define ROM_API_AUX_TDC_TABLE   ((uint32_t*) (ROM_API_TABLE[6]))

§ ROM_API_DDI_TABLE

#define ROM_API_DDI_TABLE   ((uint32_t*) (ROM_API_TABLE[9]))

§ ROM_API_FLASH_TABLE

#define ROM_API_FLASH_TABLE   ((uint32_t*) (ROM_API_TABLE[10]))

Referenced by FlashProgram(), and FlashSectorErase().

§ ROM_API_I2C_TABLE

#define ROM_API_I2C_TABLE   ((uint32_t*) (ROM_API_TABLE[11]))

§ ROM_API_I2S_TABLE

#define ROM_API_I2S_TABLE   ((uint32_t*) (ROM_API_TABLE[29]))

§ ROM_API_INTERRUPT_TABLE

#define ROM_API_INTERRUPT_TABLE   ((uint32_t*) (ROM_API_TABLE[12]))

§ ROM_API_IOC_TABLE

#define ROM_API_IOC_TABLE   ((uint32_t*) (ROM_API_TABLE[13]))

§ ROM_API_OSC_TABLE

#define ROM_API_OSC_TABLE   ((uint32_t*) (ROM_API_TABLE[24]))

§ ROM_API_PKA_TABLE

#define ROM_API_PKA_TABLE   ((uint32_t*) (ROM_API_TABLE[32]))

§ ROM_API_PRCM_TABLE

#define ROM_API_PRCM_TABLE   ((uint32_t*) (ROM_API_TABLE[14]))

§ ROM_API_PWR_CTRL_TABLE

#define ROM_API_PWR_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[30]))

§ ROM_API_SETUP_ROM_TABLE

#define ROM_API_SETUP_ROM_TABLE   ((uint32_t*) (ROM_API_TABLE[28]))

§ ROM_API_SHA2_TABLE

#define ROM_API_SHA2_TABLE   ((uint32_t*) (ROM_API_TABLE[33]))

§ ROM_API_SMPH_TABLE

#define ROM_API_SMPH_TABLE   ((uint32_t*) (ROM_API_TABLE[15]))

§ ROM_API_SSI_TABLE

#define ROM_API_SSI_TABLE   ((uint32_t*) (ROM_API_TABLE[17]))

§ ROM_API_SYS_CTRL_TABLE

#define ROM_API_SYS_CTRL_TABLE   ((uint32_t*) (ROM_API_TABLE[26]))

§ ROM_API_TABLE

#define ROM_API_TABLE   ((uint32_t *) 0x10000180)

§ ROM_API_TIMER_TABLE

#define ROM_API_TIMER_TABLE   ((uint32_t*) (ROM_API_TABLE[18]))

§ ROM_API_TRNG_TABLE

#define ROM_API_TRNG_TABLE   ((uint32_t*) (ROM_API_TABLE[19]))

§ ROM_API_UART_TABLE

#define ROM_API_UART_TABLE   ((uint32_t*) (ROM_API_TABLE[20]))

§ ROM_API_UDMA_TABLE

#define ROM_API_UDMA_TABLE   ((uint32_t*) (ROM_API_TABLE[21]))

§ ROM_API_VIMS_TABLE

#define ROM_API_VIMS_TABLE   ((uint32_t*) (ROM_API_TABLE[22]))

§ ROM_AUXADCAdjustValueForGainAndOffset

#define ROM_AUXADCAdjustValueForGainAndOffset
Value:
((int32_t (*)(int32_t adcValue, int32_t gain, int32_t offset)) \
ROM_API_AUX_ADC_TABLE[0])

§ ROM_AUXADCDisable

#define ROM_AUXADCDisable
Value:
((void (*)(void)) \
ROM_API_AUX_ADC_TABLE[1])

§ ROM_AUXADCDisableInputScaling

#define ROM_AUXADCDisableInputScaling
Value:
((void (*)(void)) \
ROM_API_AUX_ADC_TABLE[2])

§ ROM_AUXADCEnableAsync

#define ROM_AUXADCEnableAsync
Value:
((void (*)(uint32_t refSource, uint32_t trigger)) \
ROM_API_AUX_ADC_TABLE[3])

§ ROM_AUXADCEnableSyncNoBugWorkaround

#define ROM_AUXADCEnableSyncNoBugWorkaround
Value:
((void (*)(uint32_t refSource, uint32_t sampleTime, uint32_t trigger)) \
ROM_API_AUX_ADC_TABLE[4])

Referenced by AUXADCEnableSync().

§ ROM_AUXADCFlushFifo

#define ROM_AUXADCFlushFifo
Value:
((void (*)(void)) \
ROM_API_AUX_ADC_TABLE[5])

§ ROM_AUXADCGetAdjustmentGain

#define ROM_AUXADCGetAdjustmentGain
Value:
((int32_t (*)(uint32_t refSource)) \
ROM_API_AUX_ADC_TABLE[6])

§ ROM_AUXADCGetAdjustmentOffset

#define ROM_AUXADCGetAdjustmentOffset
Value:
((int32_t (*)(uint32_t refSource)) \
ROM_API_AUX_ADC_TABLE[7])

§ ROM_AUXADCMicrovoltsToValue

#define ROM_AUXADCMicrovoltsToValue
Value:
((int32_t (*)(int32_t fixedRefVoltage, int32_t microvolts)) \
ROM_API_AUX_ADC_TABLE[8])

§ ROM_AUXADCPopFifo

#define ROM_AUXADCPopFifo
Value:
((uint32_t (*)(void)) \
ROM_API_AUX_ADC_TABLE[9])

§ ROM_AUXADCReadFifo

#define ROM_AUXADCReadFifo
Value:
((uint32_t (*)(void)) \
ROM_API_AUX_ADC_TABLE[10])

§ ROM_AUXADCUnadjustValueForGainAndOffset

#define ROM_AUXADCUnadjustValueForGainAndOffset
Value:
((int32_t (*)(int32_t adcValue, int32_t gain, int32_t offset)) \
ROM_API_AUX_ADC_TABLE[11])

§ ROM_AUXADCValueToMicrovolts

#define ROM_AUXADCValueToMicrovolts
Value:
((int32_t (*)(int32_t fixedRefVoltage, int32_t adcValue)) \
ROM_API_AUX_ADC_TABLE[12])

§ ROM_AUXTDCConfigSet

#define ROM_AUXTDCConfigSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32StartCondition, uint32_t ui32StopCondition)) \
ROM_API_AUX_TDC_TABLE[0])

§ ROM_AUXTDCMeasurementDone

#define ROM_AUXTDCMeasurementDone
Value:
((uint32_t (*)(uint32_t ui32Base)) \
ROM_API_AUX_TDC_TABLE[1])

§ ROM_DDI16BitfieldRead

#define ROM_DDI16BitfieldRead
Value:
((uint16_t (*)(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift)) \
ROM_API_DDI_TABLE[3])

§ ROM_DDI16BitfieldWrite

#define ROM_DDI16BitfieldWrite
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift, uint16_t ui32Data)) \
ROM_API_DDI_TABLE[1])

§ ROM_DDI16BitRead

#define ROM_DDI16BitRead
Value:
((uint16_t (*)(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask)) \
ROM_API_DDI_TABLE[2])

§ ROM_DDI16BitWrite

#define ROM_DDI16BitWrite
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32WrData)) \
ROM_API_DDI_TABLE[0])

§ ROM_DDI32RegWrite

#define ROM_DDI32RegWrite
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)) \
ROM_API_DDI_TABLE[4])

§ ROM_FlashDisableSectorsForWrite

#define ROM_FlashDisableSectorsForWrite
Value:
((void (*)(void)) \
ROM_API_FLASH_TABLE[9])

§ ROM_FlashEfuseReadRow

#define ROM_FlashEfuseReadRow
Value:
((bool (*)(uint32_t *pui32EfuseData, uint32_t ui32RowAddress)) \
ROM_API_FLASH_TABLE[8])

§ ROM_FlashProtectionGet

#define ROM_FlashProtectionGet
Value:
((uint32_t (*)(uint32_t ui32SectorAddress)) \
ROM_API_FLASH_TABLE[3])

§ ROM_FlashProtectionSave

#define ROM_FlashProtectionSave
Value:
((uint32_t (*)(uint32_t ui32SectorAddress)) \
ROM_API_FLASH_TABLE[4])

§ ROM_FlashProtectionSet

#define ROM_FlashProtectionSet
Value:
((void (*)(uint32_t ui32SectorAddress, uint32_t ui32ProtectMode)) \
ROM_API_FLASH_TABLE[2])

§ ROM_HAPI_TABLE_ADDR

#define ROM_HAPI_TABLE_ADDR   0x10000048

§ ROM_I2CMasterErr

#define ROM_I2CMasterErr
Value:
((uint32_t (*)(uint32_t ui32Base)) \
ROM_API_I2C_TABLE[1])

§ ROM_I2CMasterInitExpClk

#define ROM_I2CMasterInitExpClk
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32I2CClk, bool bFast)) \
ROM_API_I2C_TABLE[0])

§ ROM_I2SPointerSet

#define ROM_I2SPointerSet
Value:
((void (*)(uint32_t ui32Base, bool bInput, void * pNextPointer)) \
ROM_API_I2S_TABLE[0])

§ ROM_I2SSampleStampGet

#define ROM_I2SSampleStampGet
Value:
((uint32_t (*)(uint32_t ui32Base, uint32_t ui32Channel)) \
ROM_API_I2S_TABLE[1])

§ ROM_IntDisable

#define ROM_IntDisable
Value:
((void (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[5])

§ ROM_IntEnable

#define ROM_IntEnable
Value:
((void (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[4])

§ ROM_IntPendClear

#define ROM_IntPendClear
Value:
((void (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[8])

§ ROM_IntPendGet

#define ROM_IntPendGet
Value:
((bool (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[7])

§ ROM_IntPendSet

#define ROM_IntPendSet
Value:
((void (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[6])

§ ROM_IntPriorityGet

#define ROM_IntPriorityGet
Value:
((int32_t (*)(uint32_t ui32Interrupt)) \
ROM_API_INTERRUPT_TABLE[3])

§ ROM_IntPriorityGroupingGet

#define ROM_IntPriorityGroupingGet
Value:
((uint32_t (*)(void)) \
ROM_API_INTERRUPT_TABLE[1])

§ ROM_IntPriorityGroupingSet

#define ROM_IntPriorityGroupingSet
Value:
((void (*)(uint32_t ui32Bits)) \
ROM_API_INTERRUPT_TABLE[0])

§ ROM_IntPrioritySet

#define ROM_IntPrioritySet
Value:
((void (*)(uint32_t ui32Interrupt, uint8_t ui8Priority)) \
ROM_API_INTERRUPT_TABLE[2])

§ ROM_IOCIntDisable

#define ROM_IOCIntDisable
Value:
((void (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[13])

§ ROM_IOCIntEnable

#define ROM_IOCIntEnable
Value:
((void (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[12])

§ ROM_IOCIODrvStrengthSet

#define ROM_IOCIODrvStrengthSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32IOCurrent, uint32_t ui32DrvStrength)) \
ROM_API_IOC_TABLE[10])

§ ROM_IOCIOHystSet

#define ROM_IOCIOHystSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32Hysteresis)) \
ROM_API_IOC_TABLE[7])

§ ROM_IOCIOInputSet

#define ROM_IOCIOInputSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32Input)) \
ROM_API_IOC_TABLE[8])

§ ROM_IOCIOIntSet

#define ROM_IOCIOIntSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32Int, uint32_t ui32EdgeDet)) \
ROM_API_IOC_TABLE[5])

§ ROM_IOCIOModeSet

#define ROM_IOCIOModeSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32IOMode)) \
ROM_API_IOC_TABLE[4])

§ ROM_IOCIOPortIdSet

#define ROM_IOCIOPortIdSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32PortId)) \
ROM_API_IOC_TABLE[11])

§ ROM_IOCIOPortPullSet

#define ROM_IOCIOPortPullSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32Pull)) \
ROM_API_IOC_TABLE[6])

§ ROM_IOCIOShutdownSet

#define ROM_IOCIOShutdownSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32IOShutdown)) \
ROM_API_IOC_TABLE[2])

§ ROM_IOCIOSlewCtrlSet

#define ROM_IOCIOSlewCtrlSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32SlewEnable)) \
ROM_API_IOC_TABLE[9])

§ ROM_IOCPinTypeAux

#define ROM_IOCPinTypeAux
Value:
((void (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[21])

§ ROM_IOCPinTypeGpioInput

#define ROM_IOCPinTypeGpioInput
Value:
((void (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[14])

§ ROM_IOCPinTypeGpioOutput

#define ROM_IOCPinTypeGpioOutput
Value:
((void (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[15])

§ ROM_IOCPinTypeI2c

#define ROM_IOCPinTypeI2c
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Data, uint32_t ui32Clk)) \
ROM_API_IOC_TABLE[19])

§ ROM_IOCPinTypeSsiMaster

#define ROM_IOCPinTypeSsiMaster
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk)) \
ROM_API_IOC_TABLE[17])

§ ROM_IOCPinTypeSsiSlave

#define ROM_IOCPinTypeSsiSlave
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Fss, uint32_t ui32Clk)) \
ROM_API_IOC_TABLE[18])

§ ROM_IOCPinTypeUart

#define ROM_IOCPinTypeUart
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Rx, uint32_t ui32Tx, uint32_t ui32Cts, uint32_t ui32Rts)) \
ROM_API_IOC_TABLE[16])

§ ROM_IOCPortConfigureGet

#define ROM_IOCPortConfigureGet
Value:
((uint32_t (*)(uint32_t ui32IOId)) \
ROM_API_IOC_TABLE[1])

§ ROM_IOCPortConfigureSet

#define ROM_IOCPortConfigureSet
Value:
((void (*)(uint32_t ui32IOId, uint32_t ui32PortId, uint32_t ui32IOConfig)) \
ROM_API_IOC_TABLE[0])

§ ROM_OSC_HPOSCRelativeFrequencyOffsetToRFCoreFormatConvert

#define ROM_OSC_HPOSCRelativeFrequencyOffsetToRFCoreFormatConvert
Value:
((int16_t (*)(int32_t HPOSC_RelFreqOffset)) \
ROM_API_OSC_TABLE[3])

§ ROM_OSCClockSourceGet

#define ROM_OSCClockSourceGet
Value:
((uint32_t (*)(uint32_t ui32SrcClk)) \
ROM_API_OSC_TABLE[0])

Referenced by OSCHF_AttemptToSwitchToXosc(), and OSCHF_SwitchToRcOscTurnOffXosc().

§ ROM_OSCClockSourceSet

#define ROM_OSCClockSourceSet
Value:
((void (*)(uint32_t ui32SrcClk, uint32_t ui32Osc)) \
ROM_API_OSC_TABLE[1])

Referenced by OSCHF_SwitchToRcOscTurnOffXosc(), and OSCHF_TurnOnXosc().

§ ROM_PKAArrayAllZeros

#define ROM_PKAArrayAllZeros
Value:
((bool (*)(const uint8_t *array, uint32_t arrayLength)) \
ROM_API_PKA_TABLE[17])

§ ROM_PKABigNumAddGetResult

#define ROM_PKABigNumAddGetResult
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)) \
ROM_API_PKA_TABLE[0])

§ ROM_PKABigNumAddStart

#define ROM_PKABigNumAddStart
Value:
((uint32_t (*)(const uint8_t *bigNum1, uint32_t bigNum1Length, const uint8_t *bigNum2, uint32_t bigNum2Length, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[10])

§ ROM_PKABigNumCmpGetResult

#define ROM_PKABigNumCmpGetResult
Value:
((uint32_t (*)(void)) \
ROM_API_PKA_TABLE[1])

§ ROM_PKABigNumCmpStart

#define ROM_PKABigNumCmpStart
Value:
((uint32_t (*)(const uint8_t *bigNum1, const uint8_t *bigNum2, uint32_t length)) \
ROM_API_PKA_TABLE[11])

§ ROM_PKABigNumDivideGetQuotient

#define ROM_PKABigNumDivideGetQuotient
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t *length, uint32_t resultQuotientMemAddr)) \
ROM_API_PKA_TABLE[18])

§ ROM_PKABigNumDivideGetRemainder

#define ROM_PKABigNumDivideGetRemainder
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t *length, uint32_t resultRemainderMemAddr)) \
ROM_API_PKA_TABLE[19])

§ ROM_PKABigNumDivideStart

#define ROM_PKABigNumDivideStart
Value:
((uint32_t (*)(const uint8_t *dividend, uint32_t dividendLength, const uint8_t *divisor, uint32_t divisorLength, uint32_t *resultQuotientMemAddr, uint32_t *resultRemainderMemAddr)) \
ROM_API_PKA_TABLE[20])

§ ROM_PKABigNumInvModGetResult

#define ROM_PKABigNumInvModGetResult
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)) \
ROM_API_PKA_TABLE[2])

§ ROM_PKABigNumInvModStart

#define ROM_PKABigNumInvModStart
Value:
((uint32_t (*)(const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[12])

§ ROM_PKABigNumModGetResult

#define ROM_PKABigNumModGetResult
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t length, uint32_t resultPKAMemAddr)) \
ROM_API_PKA_TABLE[3])

§ ROM_PKABigNumModStart

#define ROM_PKABigNumModStart
Value:
((uint32_t (*)(const uint8_t *bigNum, uint32_t bigNumLength, const uint8_t *modulus, uint32_t modulusLength, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[13])

§ ROM_PKABigNumMultGetResult

#define ROM_PKABigNumMultGetResult
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)) \
ROM_API_PKA_TABLE[4])

§ ROM_PKABigNumMultiplyStart

#define ROM_PKABigNumMultiplyStart
Value:
((uint32_t (*)(const uint8_t *multiplicand, uint32_t multiplicandLength, const uint8_t *multiplier, uint32_t multiplierLength, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[14])

§ ROM_PKABigNumSubGetResult

#define ROM_PKABigNumSubGetResult
Value:
((uint32_t (*)(uint8_t *resultBuf, uint32_t *resultLength, uint32_t resultPKAMemAddr)) \
ROM_API_PKA_TABLE[15])

§ ROM_PKABigNumSubStart

#define ROM_PKABigNumSubStart
Value:
((uint32_t (*)(const uint8_t *minuend, uint32_t minuendLength, const uint8_t *subtrahend, uint32_t subtrahendLength, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[16])

§ ROM_PKAEccAddGetResult

#define ROM_PKAEccAddGetResult
Value:
((uint32_t (*)(uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)) \
ROM_API_PKA_TABLE[5])

§ ROM_PKAEccAddStart

#define ROM_PKAEccAddStart
Value:
((uint32_t (*)(const uint8_t *curvePoint1X, const uint8_t *curvePoint1Y, const uint8_t *curvePoint2X, const uint8_t *curvePoint2Y, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[6])

§ ROM_PKAEccMontgomeryMultiplyStart

#define ROM_PKAEccMontgomeryMultiplyStart
Value:
((uint32_t (*)(const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *prime, const uint8_t *a, uint32_t length, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[23])

§ ROM_PKAEccMultiplyGetResult

#define ROM_PKAEccMultiplyGetResult
Value:
((uint32_t (*)(uint8_t *curvePointX, uint8_t *curvePointY, uint32_t resultPKAMemAddr, uint32_t length)) \
ROM_API_PKA_TABLE[7])

§ ROM_PKAEccMultiplyStart

#define ROM_PKAEccMultiplyStart
Value:
((uint32_t (*)(const uint8_t *scalar, const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, uint32_t length, uint32_t *resultPKAMemAddr)) \
ROM_API_PKA_TABLE[8])

§ ROM_PKAEccVerifyPublicKeyWeierstrassStart

#define ROM_PKAEccVerifyPublicKeyWeierstrassStart
Value:
((uint32_t (*)(const uint8_t *curvePointX, const uint8_t *curvePointY, const uint8_t *prime, const uint8_t *a, const uint8_t *b, const uint8_t *order, uint32_t length)) \
ROM_API_PKA_TABLE[21])

§ ROM_PKAGetOpsStatus

#define ROM_PKAGetOpsStatus
Value:
((uint32_t (*)(void)) \
ROM_API_PKA_TABLE[9])

§ ROM_PKAZeroOutArray

#define ROM_PKAZeroOutArray
Value:
((void (*)(const uint8_t *array, uint32_t arrayLength)) \
ROM_API_PKA_TABLE[22])

§ ROM_PowerCtrlSourceSet

#define ROM_PowerCtrlSourceSet
Value:
((void (*)(uint32_t ui32PowerConfig)) \
ROM_API_PWR_CTRL_TABLE[0])

§ ROM_PRCMAudioClockConfigSet

#define ROM_PRCMAudioClockConfigSet
Value:
((void (*)(uint32_t ui32ClkConfig, uint32_t ui32SampleRate)) \
ROM_API_PRCM_TABLE[4])

§ ROM_PRCMAudioClockConfigSetOverride

#define ROM_PRCMAudioClockConfigSetOverride
Value:
((void (*)(uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv)) \
ROM_API_PRCM_TABLE[17])

§ ROM_PRCMDeepSleep

#define ROM_PRCMDeepSleep
Value:
((void (*)(void)) \
ROM_API_PRCM_TABLE[14])

§ ROM_PRCMInfClockConfigureGet

#define ROM_PRCMInfClockConfigureGet
Value:
((uint32_t (*)(uint32_t ui32PowerMode)) \
ROM_API_PRCM_TABLE[1])

§ ROM_PRCMInfClockConfigureSet

#define ROM_PRCMInfClockConfigureSet
Value:
((void (*)(uint32_t ui32ClkDiv, uint32_t ui32PowerMode)) \
ROM_API_PRCM_TABLE[0])

§ ROM_PRCMPeripheralDeepSleepDisable

#define ROM_PRCMPeripheralDeepSleepDisable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[12])

§ ROM_PRCMPeripheralDeepSleepEnable

#define ROM_PRCMPeripheralDeepSleepEnable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[11])

§ ROM_PRCMPeripheralRunDisable

#define ROM_PRCMPeripheralRunDisable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[8])

§ ROM_PRCMPeripheralRunEnable

#define ROM_PRCMPeripheralRunEnable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[7])

§ ROM_PRCMPeripheralSleepDisable

#define ROM_PRCMPeripheralSleepDisable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[10])

§ ROM_PRCMPeripheralSleepEnable

#define ROM_PRCMPeripheralSleepEnable
Value:
((void (*)(uint32_t ui32Peripheral)) \
ROM_API_PRCM_TABLE[9])

§ ROM_PRCMPowerDomainOff

#define ROM_PRCMPowerDomainOff
Value:
((void (*)(uint32_t ui32Domains)) \
ROM_API_PRCM_TABLE[6])

§ ROM_PRCMPowerDomainOn

#define ROM_PRCMPowerDomainOn
Value:
((void (*)(uint32_t ui32Domains)) \
ROM_API_PRCM_TABLE[5])

§ ROM_SetupAfterColdResetWakeupFromShutDownCfg1

#define ROM_SetupAfterColdResetWakeupFromShutDownCfg1
Value:
((void (*)(uint32_t ccfg_ModeConfReg)) \
ROM_API_SETUP_ROM_TABLE[0])

§ ROM_SetupAfterColdResetWakeupFromShutDownCfg2

#define ROM_SetupAfterColdResetWakeupFromShutDownCfg2
Value:
((void (*)(uint32_t ui32Fcfg1Revision, uint32_t ccfg_ModeConfReg)) \
ROM_API_SETUP_ROM_TABLE[1])

§ ROM_SetupAfterColdResetWakeupFromShutDownCfg3

#define ROM_SetupAfterColdResetWakeupFromShutDownCfg3
Value:
((void (*)(uint32_t ccfg_ModeConfReg)) \
ROM_API_SETUP_ROM_TABLE[2])

§ ROM_SetupGetTrimForAdcShModeEn

#define ROM_SetupGetTrimForAdcShModeEn
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[3])

§ ROM_SetupGetTrimForAdcShVbufEn

#define ROM_SetupGetTrimForAdcShVbufEn
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[4])

§ ROM_SetupGetTrimForAmpcompCtrl

#define ROM_SetupGetTrimForAmpcompCtrl
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[5])

§ ROM_SetupGetTrimForAmpcompTh1

#define ROM_SetupGetTrimForAmpcompTh1
Value:
((uint32_t (*)(void)) \
ROM_API_SETUP_ROM_TABLE[6])

§ ROM_SetupGetTrimForAmpcompTh2

#define ROM_SetupGetTrimForAmpcompTh2
Value:
((uint32_t (*)(void)) \
ROM_API_SETUP_ROM_TABLE[7])

§ ROM_SetupGetTrimForAnabypassValue1

#define ROM_SetupGetTrimForAnabypassValue1
Value:
((uint32_t (*)(uint32_t ccfg_ModeConfReg)) \
ROM_API_SETUP_ROM_TABLE[8])

§ ROM_SetupGetTrimForDblrLoopFilterResetVoltage

#define ROM_SetupGetTrimForDblrLoopFilterResetVoltage
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[9])

§ ROM_SetupGetTrimForRadcExtCfg

#define ROM_SetupGetTrimForRadcExtCfg
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[10])

§ ROM_SetupGetTrimForRcOscLfIBiasTrim

#define ROM_SetupGetTrimForRcOscLfIBiasTrim
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[11])

§ ROM_SetupGetTrimForRcOscLfRtuneCtuneTrim

#define ROM_SetupGetTrimForRcOscLfRtuneCtuneTrim
Value:
((uint32_t (*)(void)) \
ROM_API_SETUP_ROM_TABLE[12])

§ ROM_SetupGetTrimForXoscHfCtl

#define ROM_SetupGetTrimForXoscHfCtl
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[13])

§ ROM_SetupGetTrimForXoscHfFastStart

#define ROM_SetupGetTrimForXoscHfFastStart
Value:
((uint32_t (*)(void)) \
ROM_API_SETUP_ROM_TABLE[14])

§ ROM_SetupGetTrimForXoscHfIbiastherm

#define ROM_SetupGetTrimForXoscHfIbiastherm
Value:
((uint32_t (*)(void)) \
ROM_API_SETUP_ROM_TABLE[15])

§ ROM_SetupGetTrimForXoscLfRegulatorAndCmirrwrRatio

#define ROM_SetupGetTrimForXoscLfRegulatorAndCmirrwrRatio
Value:
((uint32_t (*)(uint32_t ui32Fcfg1Revision)) \
ROM_API_SETUP_ROM_TABLE[16])

§ ROM_SetupSetAonRtcSubSecInc

#define ROM_SetupSetAonRtcSubSecInc
Value:
((void (*)(uint32_t subSecInc)) \
ROM_API_SETUP_ROM_TABLE[17])

§ ROM_SetupSetCacheModeAccordingToCcfgSetting

#define ROM_SetupSetCacheModeAccordingToCcfgSetting
Value:
((void (*)(void)) \
ROM_API_SETUP_ROM_TABLE[18])

§ ROM_SetupStepVddrTrimTo

#define ROM_SetupStepVddrTrimTo
Value:
((void (*)(uint32_t toCode)) \
ROM_API_SETUP_ROM_TABLE[19])

§ ROM_SHA2ComputeFinalHash

#define ROM_SHA2ComputeFinalHash
Value:
((uint32_t (*)(const uint8_t *message, uint8_t *resultDigest, uint32_t *intermediateDigest, uint32_t totalMsgLength, uint32_t messageLength, uint32_t hashAlgorithm)) \
ROM_API_SHA2_TABLE[0])

§ ROM_SHA2ComputeHash

#define ROM_SHA2ComputeHash
Value:
((uint32_t (*)(const uint8_t *message, uint8_t *resultDigest, uint32_t totalMsgLength, uint32_t hashAlgorithm)) \
ROM_API_SHA2_TABLE[1])

§ ROM_SHA2ComputeInitialHash

#define ROM_SHA2ComputeInitialHash
Value:
((uint32_t (*)(const uint8_t *message, uint32_t *intermediateDigest, uint32_t hashAlgorithm, uint32_t initialMessageLength)) \
ROM_API_SHA2_TABLE[2])

§ ROM_SHA2ComputeIntermediateHash

#define ROM_SHA2ComputeIntermediateHash
Value:
((uint32_t (*)(const uint8_t *message, uint32_t *intermediateDigest, uint32_t hashAlgorithm, uint32_t intermediateMessageLength)) \
ROM_API_SHA2_TABLE[3])

§ ROM_SHA2StartDMAOperation

#define ROM_SHA2StartDMAOperation
Value:
((void (*)(uint8_t *channel0Addr, uint32_t channel0Length, uint8_t *channel1Addr, uint32_t channel1Length)) \
ROM_API_SHA2_TABLE[4])

§ ROM_SHA2WaitForIRQFlags

#define ROM_SHA2WaitForIRQFlags
Value:
((uint32_t (*)(uint32_t irqFlags)) \
ROM_API_SHA2_TABLE[5])

§ ROM_SMPHAcquire

#define ROM_SMPHAcquire
Value:
((void (*)(uint32_t ui32Semaphore)) \
ROM_API_SMPH_TABLE[0])

§ ROM_SSIConfigSetExpClk

#define ROM_SSIConfigSetExpClk
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32SSIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth)) \
ROM_API_SSI_TABLE[0])

§ ROM_SSIDataGet

#define ROM_SSIDataGet
Value:
((void (*)(uint32_t ui32Base, uint32_t *pui32Data)) \
ROM_API_SSI_TABLE[3])

§ ROM_SSIDataGetNonBlocking

#define ROM_SSIDataGetNonBlocking
Value:
((int32_t (*)(uint32_t ui32Base, uint32_t *pui32Data)) \
ROM_API_SSI_TABLE[4])

§ ROM_SSIDataPut

#define ROM_SSIDataPut
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Data)) \
ROM_API_SSI_TABLE[1])

§ ROM_SSIDataPutNonBlocking

#define ROM_SSIDataPutNonBlocking
Value:
((int32_t (*)(uint32_t ui32Base, uint32_t ui32Data)) \
ROM_API_SSI_TABLE[2])

§ ROM_SysCtrl_DCDC_VoltageConditionalControl

#define ROM_SysCtrl_DCDC_VoltageConditionalControl
Value:
((void (*)(void)) \
ROM_API_SYS_CTRL_TABLE[1])

§ ROM_SysCtrlResetSourceGet

#define ROM_SysCtrlResetSourceGet
Value:
((uint32_t (*)(void)) \
ROM_API_SYS_CTRL_TABLE[0])

§ ROM_TimerConfigure

#define ROM_TimerConfigure
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Config)) \
ROM_API_TIMER_TABLE[0])

§ ROM_TimerIntervalLoadMode

#define ROM_TimerIntervalLoadMode
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode)) \
ROM_API_TIMER_TABLE[5])

§ ROM_TimerLevelControl

#define ROM_TimerLevelControl
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Timer, bool bInvert)) \
ROM_API_TIMER_TABLE[1])

§ ROM_TimerMatchUpdateMode

#define ROM_TimerMatchUpdateMode
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode)) \
ROM_API_TIMER_TABLE[6])

§ ROM_TimerStallControl

#define ROM_TimerStallControl
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Timer, bool bStall)) \
ROM_API_TIMER_TABLE[3])

§ ROM_TimerWaitOnTriggerControl

#define ROM_TimerWaitOnTriggerControl
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Timer, bool bWait)) \
ROM_API_TIMER_TABLE[4])

§ ROM_TRNGConfigure

#define ROM_TRNGConfigure
Value:
((void (*)(uint32_t ui32MinSamplesPerCycle, uint32_t ui32MaxSamplesPerCycle, uint32_t ui32ClocksPerSample)) \
ROM_API_TRNG_TABLE[0])

§ ROM_TRNGNumberGet

#define ROM_TRNGNumberGet
Value:
((uint32_t (*)(uint32_t ui32Word)) \
ROM_API_TRNG_TABLE[1])

§ ROM_UARTCharGet

#define ROM_UARTCharGet
Value:
((int32_t (*)(uint32_t ui32Base)) \
ROM_API_UART_TABLE[5])

§ ROM_UARTCharGetNonBlocking

#define ROM_UARTCharGetNonBlocking
Value:
((int32_t (*)(uint32_t ui32Base)) \
ROM_API_UART_TABLE[4])

§ ROM_UARTCharPut

#define ROM_UARTCharPut
Value:
((void (*)(uint32_t ui32Base, uint8_t ui8Data)) \
ROM_API_UART_TABLE[7])

§ ROM_UARTCharPutNonBlocking

#define ROM_UARTCharPutNonBlocking
Value:
((bool (*)(uint32_t ui32Base, uint8_t ui8Data)) \
ROM_API_UART_TABLE[6])

§ ROM_UARTConfigGetExpClk

#define ROM_UARTConfigGetExpClk
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config)) \
ROM_API_UART_TABLE[2])

§ ROM_UARTConfigSetExpClk

#define ROM_UARTConfigSetExpClk
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config)) \
ROM_API_UART_TABLE[1])

§ ROM_UARTDisable

#define ROM_UARTDisable
Value:
((void (*)(uint32_t ui32Base)) \
ROM_API_UART_TABLE[3])

§ ROM_UARTFIFOLevelGet

#define ROM_UARTFIFOLevelGet
Value:
((void (*)(uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel)) \
ROM_API_UART_TABLE[0])

§ ROM_uDMAChannelAttributeDisable

#define ROM_uDMAChannelAttributeDisable
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr)) \
ROM_API_UDMA_TABLE[1])

§ ROM_uDMAChannelAttributeEnable

#define ROM_uDMAChannelAttributeEnable
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32Attr)) \
ROM_API_UDMA_TABLE[0])

§ ROM_uDMAChannelAttributeGet

#define ROM_uDMAChannelAttributeGet
Value:
((uint32_t (*)(uint32_t ui32Base, uint32_t ui32ChannelNum)) \
ROM_API_UDMA_TABLE[2])

§ ROM_uDMAChannelControlSet

#define ROM_uDMAChannelControlSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Control)) \
ROM_API_UDMA_TABLE[3])

§ ROM_uDMAChannelModeGet

#define ROM_uDMAChannelModeGet
Value:
((uint32_t (*)(uint32_t ui32Base, uint32_t ui32ChannelStructIndex)) \
ROM_API_UDMA_TABLE[7])

§ ROM_uDMAChannelScatterGatherSet

#define ROM_uDMAChannelScatterGatherSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32ChannelNum, uint32_t ui32TaskCount, void *pvTaskList, uint32_t ui32IsPeriphSG)) \
ROM_API_UDMA_TABLE[5])

§ ROM_uDMAChannelSizeGet

#define ROM_uDMAChannelSizeGet
Value:
((uint32_t (*)(uint32_t ui32Base, uint32_t ui32ChannelStructIndex)) \
ROM_API_UDMA_TABLE[6])

§ ROM_uDMAChannelTransferSet

#define ROM_uDMAChannelTransferSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32ChannelStructIndex, uint32_t ui32Mode, void *pvSrcAddr, void *pvDstAddr, uint32_t ui32TransferSize)) \
ROM_API_UDMA_TABLE[4])

§ ROM_VERSION

#define ROM_VERSION   (ROM_API_TABLE[0])

§ ROM_VIMSConfigure

#define ROM_VIMSConfigure
Value:
((void (*)(uint32_t ui32Base, bool bRoundRobin, bool bPrefetch)) \
ROM_API_VIMS_TABLE[0])

§ ROM_VIMSModeGet

#define ROM_VIMSModeGet
Value:
((uint32_t (*)(uint32_t ui32Base)) \
ROM_API_VIMS_TABLE[2])

§ ROM_VIMSModeSafeSet

#define ROM_VIMSModeSafeSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32NewMode, bool blocking)) \
ROM_API_VIMS_TABLE[3])

§ ROM_VIMSModeSet

#define ROM_VIMSModeSet
Value:
((void (*)(uint32_t ui32Base, uint32_t ui32Mode)) \
ROM_API_VIMS_TABLE[1])

Typedef Documentation

§ FPTR_ADCCOMPBIN_T

typedef void(* FPTR_ADCCOMPBIN_T) (uint8_t)

§ FPTR_COMPAIN_T

typedef void(* FPTR_COMPAIN_T) (uint8_t)

§ FPTR_COMPAREF_T

typedef void(* FPTR_COMPAREF_T) (uint8_t)

§ FPTR_CRC32_T

typedef uint32_t(* FPTR_CRC32_T) (uint8_t *, uint32_t, uint32_t)

§ FPTR_DACVREF_T

typedef void(* FPTR_DACVREF_T) (uint8_t)

§ FPTR_FLETCHER32_T

typedef uint32_t(* FPTR_FLETCHER32_T) (uint16_t *, uint16_t, uint16_t)

§ FPTR_GETCHIPID_T

typedef uint32_t(* FPTR_GETCHIPID_T) (void)

§ FPTR_GETFLSIZE_T

typedef uint32_t(* FPTR_GETFLSIZE_T) (void)

§ FPTR_HFSOURCESAFESWITCH_T

typedef void(* FPTR_HFSOURCESAFESWITCH_T) (void)

§ FPTR_MAXVAL_T

typedef uint32_t(* FPTR_MAXVAL_T) (uint32_t *, uint32_t)

§ FPTR_MEANVAL_T

typedef uint32_t(* FPTR_MEANVAL_T) (uint32_t *, uint32_t)

§ FPTR_MINVAL_T

typedef uint32_t(* FPTR_MINVAL_T) (uint32_t *, uint32_t)

§ FPTR_RESERVED1_T

typedef uint32_t(* FPTR_RESERVED1_T) (uint32_t)

§ FPTR_RESERVED2_T

typedef uint32_t(* FPTR_RESERVED2_T) (void)

§ FPTR_RESERVED3_T

typedef uint32_t(* FPTR_RESERVED3_T) (uint8_t *, uint32_t, uint32_t)

§ FPTR_RESERVED4_T

typedef void(* FPTR_RESERVED4_T) (uint32_t)

§ FPTR_RESERVED5_T

typedef void(* FPTR_RESERVED5_T) (uint32_t)

§ FPTR_RESETDEV_T

typedef void(* FPTR_RESETDEV_T) (void)

§ FPTR_STDDVAL_T

typedef uint32_t(* FPTR_STDDVAL_T) (uint32_t *, uint32_t)

Function Documentation

§ MemBusWrkAroundHapiEraseSector()

uint32_t MemBusWrkAroundHapiEraseSector ( uint32_t  ui32Address)
650 {
651  uint32_t ui32ErrorReturn;
652 
653  FlashSectorErasePointer_t FuncPointer;
654  uint32_t ui32RomAddr = HWREG(ROM_HAPI_TABLE_ADDR + (3 * 4));
655 
656  // Call ROM function
657  FuncPointer = (uint32_t (*)(uint32_t)) (ui32RomAddr);
658  ui32ErrorReturn = FuncPointer(ui32Address);
659 
660  // Enable standby in flash bank since ROM function might have disabled it
661  HWREGBITW(FLASH_BASE + FLASH_O_CFG, FLASH_CFG_DIS_STANDBY_BITN ) = 0;
662 
663  // Return status of operation.
664  return(ui32ErrorReturn);
665 }
uint32_t(* FlashSectorErasePointer_t)(uint32_t)
Definition: flash.c:99
#define ROM_HAPI_TABLE_ADDR
Definition: rom.h:59

§ MemBusWrkAroundHapiProgramFlash()

uint32_t MemBusWrkAroundHapiProgramFlash ( uint8_t *  pui8DataBuffer,
uint32_t  ui32Address,
uint32_t  ui32Count 
)
627 {
628  uint32_t ui32ErrorReturn;
629  FlashPrgPointer_t FuncPointer;
630  uint32_t ui32RomAddr = HWREG(ROM_HAPI_TABLE_ADDR + (5 * 4));
631 
632  // Call ROM function
633  FuncPointer = (uint32_t (*)(uint8_t *, uint32_t, uint32_t)) (ui32RomAddr);
634  ui32ErrorReturn = FuncPointer( pui8DataBuffer, ui32Address, ui32Count);
635 
636  // Enable standby in flash bank since ROM function might have disabled it
637  HWREGBITW(FLASH_BASE + FLASH_O_CFG, FLASH_CFG_DIS_STANDBY_BITN ) = 0;
638 
639  // Return status of operation.
640  return(ui32ErrorReturn);
641 }
#define ROM_HAPI_TABLE_ADDR
Definition: rom.h:59
uint32_t(* FlashPrgPointer_t)(uint8_t *, uint32_t, uint32_t)
Definition: flash.c:97