SYS/BIOS  7.00
Data Structures | Macros | Typedefs | Functions
HeapBuf.h File Reference

Detailed Description

Fixed size buffer heap manager.

The HeapBuf manager provides functions to allocate and free storage from a heap of type HeapBuf which inherits from IHeap. HeapBuf manages a single fixed-size buffer, split into equally sized allocable blocks.

The HeapBuf manager is intended as a very fast and deterministic memory manager which can only allocate blocks of a single size. It is ideal for managing a heap that is only used for allocating a single type of object, or for objects that have very similar sizes.

Allocation from and freeing to a HeapBuf instance is non-blocking and deterministic: a call to alloc or free will always take the same amount of time.

Constraints:

Calling Context

Function Hwi Swi Task Main Startup
Params_init Y Y Y Y Y
alloc Y Y Y Y N
construct Y Y Y Y N
create N* N* Y Y N
delete N* N* Y Y N
destruct Y Y Y Y N
free Y Y Y Y N
getStats Y Y Y Y N
getExtendedStats Y Y Y Y N
isBlocking Y Y Y Y N
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. HeapBuf_Module_startupDone() returns true).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. HeapBuf_Module_startupDone() returns false).
  • *: Assuming blocking Heap is used for creation.
  • #include <stdbool.h>
    #include <stddef.h>
    #include <stdint.h>
    #include <ti/sysbios/knl/Queue.h>
    #include <ti/sysbios/runtime/Error.h>
    #include <ti/sysbios/runtime/IHeap.h>
    #include <ti/sysbios/runtime/Memory.h>
    Include dependency graph for HeapBuf.h:
    This graph shows which files directly or indirectly include this file:

    Go to the source code of this file.

    Data Structures

    struct  HeapBuf_ExtendedStats
     Stat structure for the HeapBuf_getExtendedStats function. More...
     
    struct  HeapBuf_Params
     
    struct  HeapBuf_Struct
     

    Macros

    #define HeapBuf_A_nullBuf   "buf parameter cannot be null"
     Null buf parameter. More...
     
    #define HeapBuf_A_bufAlign   "buf not properly aligned"
     Misalligned buffer. More...
     
    #define HeapBuf_A_invalidAlign   "align parameter must be 0 or a power of 2 >= the value of Memory_getMaxDefaultTypeAlign()"
     Invalid alignment. More...
     
    #define HeapBuf_A_invalidRequestedAlign   "align parameter 1) must be 0 or a power of 2 and 2) not greater than the heaps alignment"
     Invalid alignment parameter in the alloc. More...
     
    #define HeapBuf_A_invalidBlockSize   "blockSize must be large enough to hold at least two pointers"
     Assert raised when the blockSize parameter is not large enough to hold two pointers. More...
     
    #define HeapBuf_A_zeroBlocks   "numBlocks cannot be zero"
     Assert raised when the numBlocks parameter is 0. More...
     
    #define HeapBuf_A_zeroBufSize   "bufSize cannot be zero"
     Assert raised when the bufSize parameter is 0. More...
     
    #define HeapBuf_A_invalidBufSize   "HeapBuf_create's bufSize parameter is invalid (too small)"
     Invalid buffer size. More...
     
    #define HeapBuf_A_noBlocksToFree   "Cannot call HeapBuf_free when no blocks have been allocated"
     No allocated blocks. More...
     
    #define HeapBuf_A_invalidFree   "Invalid free"
     Assert raised when an invalid free occurs. More...
     
    #define HeapBuf_E_size   "requested size is too big: handle=0x%x, size=%u"
     Raised when requested size exceeds blockSize. More...
     
    #define ti_sysbios_heaps_HeapBuf_Handle_upCast(handle)   ((IHeap_Handle)(handle))
     cast handle to an IHeap_Handle for use by Memory_alloc, etc. More...
     

    Typedefs

    typedef struct HeapBuf_StructHeapBuf_Handle
     
    typedef HeapBuf_Struct HeapBuf_Object
     

    Functions

    void * HeapBuf_alloc (HeapBuf_Handle heap, size_t size, size_t align, Error_Block *eb)
     All alignment is handled in the create, therefore the align argument in alloc is ignored. More...
     
    void HeapBuf_free (HeapBuf_Handle heap, void *buf, size_t size)
     
    bool HeapBuf_isBlocking (HeapBuf_Handle heap)
     This function always returns false since the alloc/free never block on a resource. More...
     
    void HeapBuf_getStats (HeapBuf_Handle heap, Memory_Stats *statBuf)
     This function returns state information for a HeapBuf. More...
     
    void HeapBuf_getExtendedStats (HeapBuf_Handle heap, HeapBuf_ExtendedStats *statBuf)
     Retrieves the extended statistics for a HeapBuf instance. More...
     
    HeapBuf_Handle HeapBuf_create (const HeapBuf_Params *params, Error_Block *eb)
     Create a HeapBuf heap. More...
     
    HeapBuf_Handle HeapBuf_construct (HeapBuf_Struct *obj, const HeapBuf_Params *params, Error_Block *eb)
     Construct a HeapBuf heap. More...
     
    void HeapBuf_delete (HeapBuf_Handle *heap)
     Delete a HeapBuf heap. More...
     
    void HeapBuf_destruct (HeapBuf_Struct *obj)
     Destruct a HeapBuf heap. More...
     
    void HeapBuf_Params_init (HeapBuf_Params *prms)
     Initialize the HeapBuf_Params structure with default values. More...
     
    HeapBuf_Handle HeapBuf_Object_first (void)
     return handle of the first HeapBuf on HeapBuf list More...
     
    HeapBuf_Handle HeapBuf_Object_next (HeapBuf_Handle heap)
     return handle of the next HeapBuf on HeapBuf list More...
     

    Macro Definition Documentation

    § HeapBuf_A_nullBuf

    #define HeapBuf_A_nullBuf   "buf parameter cannot be null"

    Null buf parameter.

    This Assert is raised when the buf parameter has been omitted (null) for a dynamic create.

    § HeapBuf_A_bufAlign

    #define HeapBuf_A_bufAlign   "buf not properly aligned"

    Misalligned buffer.

    This Assert is raised when the buf parameter has not been aligned on the requested alignment.

    § HeapBuf_A_invalidAlign

    #define HeapBuf_A_invalidAlign   "align parameter must be 0 or a power of 2 >= the value of Memory_getMaxDefaultTypeAlign()"

    Invalid alignment.

    This Assert is raised when the align parameter is not the default value of zero, or a power of 2.

    § HeapBuf_A_invalidRequestedAlign

    #define HeapBuf_A_invalidRequestedAlign   "align parameter 1) must be 0 or a power of 2 and 2) not greater than the heaps alignment"

    Invalid alignment parameter in the alloc.

    This Assert is raised when the align argument is not a power of 2 (or 0). It is also raised if the parameter is greater the alignment specified when creating the heap.

    § HeapBuf_A_invalidBlockSize

    #define HeapBuf_A_invalidBlockSize   "blockSize must be large enough to hold at least two pointers"

    Assert raised when the blockSize parameter is not large enough to hold two pointers.

    § HeapBuf_A_zeroBlocks

    #define HeapBuf_A_zeroBlocks   "numBlocks cannot be zero"

    Assert raised when the numBlocks parameter is 0.

    § HeapBuf_A_zeroBufSize

    #define HeapBuf_A_zeroBufSize   "bufSize cannot be zero"

    Assert raised when the bufSize parameter is 0.

    § HeapBuf_A_invalidBufSize

    #define HeapBuf_A_invalidBufSize   "HeapBuf_create's bufSize parameter is invalid (too small)"

    Invalid buffer size.

    This Assert is raised when the bufSize parameter is too small to handle requested blocks.

    § HeapBuf_A_noBlocksToFree

    #define HeapBuf_A_noBlocksToFree   "Cannot call HeapBuf_free when no blocks have been allocated"

    No allocated blocks.

    This Assert is raised when free is called and there are no blocks allocated.

    § HeapBuf_A_invalidFree

    #define HeapBuf_A_invalidFree   "Invalid free"

    Assert raised when an invalid free occurs.

    This assert can be caused for the following reasons

    • Passing a NULL pointer to the free.
    • The block is not within the heap's buffer range. This can occur if the block is freed to the wrong heap.
    • The block is not on the proper boundary. This can occur if the pointer returned from alloc is changed by the application and not set back to its original value when free is called.

    § HeapBuf_E_size

    #define HeapBuf_E_size   "requested size is too big: handle=0x%x, size=%u"

    Raised when requested size exceeds blockSize.

    § ti_sysbios_heaps_HeapBuf_Handle_upCast

    #define ti_sysbios_heaps_HeapBuf_Handle_upCast (   handle)    ((IHeap_Handle)(handle))

    cast handle to an IHeap_Handle for use by Memory_alloc, etc.

    Parameters
    handleheap handle
    Return values
    IHeap_Handle

    Typedef Documentation

    § HeapBuf_Handle

    typedef struct HeapBuf_Struct * HeapBuf_Handle

    § HeapBuf_Object

    Function Documentation

    § HeapBuf_alloc()

    void* HeapBuf_alloc ( HeapBuf_Handle  heap,
    size_t  size,
    size_t  align,
    Error_Block eb 
    )

    All alignment is handled in the create, therefore the align argument in alloc is ignored.

    HeapBuf_alloc will only fail if there are no available blocks or if the requested block size is larger than the HeapBuf's blockSize. All other requests, regardless of size, will succeed.

    Parameters
    heapheap handle
    sizesize
    alignalignment
    eberror block
    Return values
    addressof allocated block (NULL on error)

    § HeapBuf_free()

    void HeapBuf_free ( HeapBuf_Handle  heap,
    void *  buf,
    size_t  size 
    )

    § HeapBuf_isBlocking()

    bool HeapBuf_isBlocking ( HeapBuf_Handle  heap)

    This function always returns false since the alloc/free never block on a resource.

    Parameters
    heapheap handle
    Return values
    alwaysreturns false

    § HeapBuf_getStats()

    void HeapBuf_getStats ( HeapBuf_Handle  heap,
    Memory_Stats statBuf 
    )

    This function returns state information for a HeapBuf.

    Parameters
    heapheap handle
    statBufpointer to stats object

    § HeapBuf_getExtendedStats()

    void HeapBuf_getExtendedStats ( HeapBuf_Handle  heap,
    HeapBuf_ExtendedStats statBuf 
    )

    Retrieves the extended statistics for a HeapBuf instance.

    This function retrieves the extended statistics for a HeapBuf instance. It does not retrieve the standard xdc.runtime.Memory.Stats information.

    Parameters
    heapheap handle
    statBufpointer to the extended stats structure.

    § HeapBuf_create()

    HeapBuf_Handle HeapBuf_create ( const HeapBuf_Params params,
    Error_Block eb 
    )

    Create a HeapBuf heap.

    Parameters
    paramsoptional parameters
    eberror block
    Return values
    HeapBufhandle (NULL on failure)

    § HeapBuf_construct()

    HeapBuf_Handle HeapBuf_construct ( HeapBuf_Struct obj,
    const HeapBuf_Params params,
    Error_Block eb 
    )

    Construct a HeapBuf heap.

    HeapBuf_construct is equivalent to HeapBuf_create except that the HeapBuf_Struct is pre-allocated.

    Parameters
    objpointer to a HeapBuf object
    paramsoptional parameters
    eberror block
    Return values
    HeapBufhandle (NULL on failure)

    § HeapBuf_delete()

    void HeapBuf_delete ( HeapBuf_Handle heap)

    Delete a HeapBuf heap.

    Note that HeapBuf_delete takes a pointer to a HeapBuf_Handle which enables HeapBuf_delete to set the HeapBuf handle to NULL.

    Parameters
    heappointer to a HeapBuf handle

    § HeapBuf_destruct()

    void HeapBuf_destruct ( HeapBuf_Struct obj)

    Destruct a HeapBuf heap.

    Parameters
    objpointer to a HeapBuf objects

    § HeapBuf_Params_init()

    void HeapBuf_Params_init ( HeapBuf_Params prms)

    Initialize the HeapBuf_Params structure with default values.

    HeapBuf_Params_init initializes the HeapBuf_Params structure with default values. HeapBuf_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

    Parameters
    prmspointer to uninitialized params structure

    § HeapBuf_Object_first()

    HeapBuf_Handle HeapBuf_Object_first ( void  )

    return handle of the first HeapBuf on HeapBuf list

    Return the handle of the first HeapBuf on the create/construct list. NULL if no HeapBufs have been created or constructed.

    Return values
    HeapBufhandle

    § HeapBuf_Object_next()

    HeapBuf_Handle HeapBuf_Object_next ( HeapBuf_Handle  heap)

    return handle of the next HeapBuf on HeapBuf list

    Return the handle of the next HeapBuf on the create/construct list. NULL if no more HeapBufs are on the list.

    Parameters
    heapHeapBuf handle
    Return values
    HeapBufhandle
    © Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy policy | Terms of use | Terms of sale