SYS/BIOS  7.00
Functions
TimestampProvider.h File Reference

Detailed Description

CC26xx RTC Timestamp Provider.

Calling Context

Function Hwi Swi Task Main** Startup***
get32 Y Y Y Y N
get64 Y Y Y Y N
getFreq Y Y Y Y N

#include <xdc/std.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/runtime/Types.h>
#include <ti/sysbios/family/arm/v8m/cc26x4/Timer.h>
#include "TimestampProvider_defs.h"
Include dependency graph for TimestampProvider.h:

Go to the source code of this file.

Functions

uint32_t TimestampProvider_get32 (void)
 Return a 32-bit timestamp. More...
 
void TimestampProvider_get64 (Types_Timestamp64 *timestamp64)
 Return a 64-bit timestamp. More...
 
void TimestampProvider_getFreq (Types_FreqHz *freq)
 Get the timestamp timer's frequency (in Hz) More...
 

Function Documentation

§ TimestampProvider_get32()

uint32_t TimestampProvider_get32 ( void  )

Return a 32-bit timestamp.

Returns a 32-bit timestamp value. Use TimestampProvider_getFreq to convert this value into units of real time.

Return values
32-bittimestamp

§ TimestampProvider_get64()

void TimestampProvider_get64 ( Types_Timestamp64 timestamp64)

Return a 64-bit timestamp.

This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.

If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0. So, it is possible for the lo field to wrap around without any change to the hi field. Use TimestampProvider_getFreq to convert this value into units of real time.

Parameters
timestamp64pointer to 64-bit result

§ TimestampProvider_getFreq()

void TimestampProvider_getFreq ( Types_FreqHz freq)

Get the timestamp timer's frequency (in Hz)

This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written. This function provides a way of converting timestamp values into units of real time.

Parameters
freqpointer to a 64-bit result
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale