![]() |
![]() |
SYS/BIOS
7.00
|
#include <ti/sysbios/knl/Task.h>
Data Fields | |
int | priority |
Task priority. More... | |
void * | stack |
Task stack pointer. Default = null. More... | |
size_t | stackSize |
Task stack size. More... | |
IHeap_Handle | stackHeap |
Mem heap used for dynamically created task stack. More... | |
void * | env |
Global environment struct. More... | |
Task_Mode | mode |
void * | sp |
Task's current stack pointer. More... | |
size_t | used |
int Task_Stat::priority |
Task priority.
void* Task_Stat::stack |
Task stack pointer. Default = null.
Null indicates that the stack is to be allocated by create().
size_t Task_Stat::stackSize |
Task stack size.
IHeap_Handle Task_Stat::stackHeap |
Mem heap used for dynamically created task stack.
The default value of NULL means that BIOS heap is used.
void* Task_Stat::env |
Global environment struct.
Task_Mode Task_Stat::mode |
void* Task_Stat::sp |
Task's current stack pointer.
size_t Task_Stat::used |