SYS/BIOS  7.00
Data Fields
Load_Module_State Struct Reference

#include <ti/sysbios/utils/Load.h>

Collaboration diagram for Load_Module_State:
Collaboration graph
[legend]

Data Fields

Queue_Object taskList
 
int taskHId
 
uint32_t taskStartTime
 
Task_Handle runningTask
 
uint32_t timeElapsed
 
bool firstSwitchDone
 
uint32_t swiStartTime
 
Load_HookContext swiEnv
 
uint32_t swiCnt
 
uint32_t hwiStartTime
 
Load_HookContext hwiEnv
 
uint32_t hwiCnt
 
uint32_t timeSlotCnt
 
uint32_t minLoop
 
uint32_t minIdle
 
uint32_t t0
 
uint32_t idleCnt
 
uint32_t cpuLoad
 

Field Documentation

§ taskList

Queue_Object Load_Module_State::taskList

§ taskHId

int Load_Module_State::taskHId

§ taskStartTime

uint32_t Load_Module_State::taskStartTime

§ runningTask

Task_Handle Load_Module_State::runningTask

§ timeElapsed

uint32_t Load_Module_State::timeElapsed

§ firstSwitchDone

bool Load_Module_State::firstSwitchDone

§ swiStartTime

uint32_t Load_Module_State::swiStartTime

§ swiEnv

Load_HookContext Load_Module_State::swiEnv

§ swiCnt

uint32_t Load_Module_State::swiCnt

§ hwiStartTime

uint32_t Load_Module_State::hwiStartTime

§ hwiEnv

Load_HookContext Load_Module_State::hwiEnv

§ hwiCnt

uint32_t Load_Module_State::hwiCnt

§ timeSlotCnt

uint32_t Load_Module_State::timeSlotCnt

§ minLoop

uint32_t Load_Module_State::minLoop

§ minIdle

uint32_t Load_Module_State::minIdle

§ t0

uint32_t Load_Module_State::t0

§ idleCnt

uint32_t Load_Module_State::idleCnt

§ cpuLoad

uint32_t Load_Module_State::cpuLoad

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale