SYS/BIOS  7.00
Data Structures | Typedefs | Functions
GateSwi.h File Reference

Detailed Description

Software Interrupt Gate.

GateSwi uses Swi_disable() and Swi_restore() as the resource locking mechanism. This gate can be used whenever the resource is being shared by Tasks or Swis.

The duration between the enter and leave should be as short as possible to minimize Swi latency.

Calling Context

Function Hwi Swi Task Main Startup
Params_init Y Y Y Y Y
query Y Y Y Y Y
construct Y Y Y Y N
create N* N* Y Y N
delete N* N* Y Y N
destruct Y Y Y Y N
enter N Y Y Y** Y**
leave N Y Y Y** Y**
Definitions:
  • Hwi: API is callable from a Hwi thread.
  • Swi: API is callable from a Swi thread.
  • Task: API is callable from a Task thread.
  • Main: API is callable during any of these phases:
    • In your module startup after this module is started (e.g. GateSwi_Module_startupDone() returns true).
    • During xdc.runtime.Startup.lastFxns.
    • During main().
    • During BIOS.startupFxns.
  • Startup: API is callable during any of these phases:
    • During xdc.runtime.Startup.firstFxns.
    • In your module startup before this module is started (e.g. GateSwi_Module_startupDone() returns false).
  • *: Assuming blocking Heap is used for creation.
  • **: Must be used in enter/leave pairs.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/knl/Swi.h>
#include <ti/sysbios/runtime/Error.h>
Include dependency graph for GateSwi.h:

Go to the source code of this file.

Data Structures

struct  GateSwi_Params
 
struct  GateSwi_Struct
 

Typedefs

typedef struct GateSwi_Params GateSwi_Params
 
typedef struct GateSwi_Struct GateSwi_Struct
 
typedef struct GateSwi_Struct GateSwi_Object
 
typedef GateSwi_ObjectGateSwi_Handle
 

Functions

bool GateSwi_canBePreempted (void)
 query Gate 'preempt' characteristics More...
 
bool GateSwi_canBlock (void)
 query Gate 'blocking' characteristics More...
 
GateSwi_Handle GateSwi_create (const GateSwi_Params *prms, Error_Block *eb)
 Create a GateSwi gate. More...
 
GateSwi_Handle GateSwi_construct (GateSwi_Struct *obj, const GateSwi_Params *prms)
 Construct a GateSwi gate. More...
 
void GateSwi_delete (GateSwi_Handle *gate)
 Delete a GateSwi gate. More...
 
void GateSwi_destruct (GateSwi_Struct *obj)
 Destruct a GateSwi gate. More...
 
void GateSwi_Params_init (GateSwi_Params *prms)
 Initialize the GateSwi_Params structure with default values. More...
 
intptr_t GateSwi_enter (GateSwi_Handle gate)
 enter the GateSwi gate More...
 
void GateSwi_leave (GateSwi_Handle gate, intptr_t key)
 leave the GateSwi gate More...
 

Typedef Documentation

§ GateSwi_Params

§ GateSwi_Struct

§ GateSwi_Object

§ GateSwi_Handle

Function Documentation

§ GateSwi_canBePreempted()

bool GateSwi_canBePreempted ( void  )

query Gate 'preempt' characteristics

GateSwi can be preempted by an hardware interrupt. Always returns true.

Return values
true

§ GateSwi_canBlock()

bool GateSwi_canBlock ( void  )

query Gate 'blocking' characteristics

GateSwi enter will never block. This API always returns false.

Return values
false

§ GateSwi_create()

GateSwi_Handle GateSwi_create ( const GateSwi_Params prms,
Error_Block eb 
)

Create a GateSwi gate.

Parameters
prmsoptional parameters
eberror block
Return values
GateSwihandle (NULL on failure)

§ GateSwi_construct()

GateSwi_Handle GateSwi_construct ( GateSwi_Struct obj,
const GateSwi_Params prms 
)

Construct a GateSwi gate.

GateSwi_construct is equivalent to GateHwi_create except that the GateSwi_Struct is pre-allocated.

Parameters
objpointer to a GateSwi object
prmsoptional parameters
Return values
GateSwihandle (NULL on failure)

§ GateSwi_delete()

void GateSwi_delete ( GateSwi_Handle gate)

Delete a GateSwi gate.

Note that GateSwi_delete takes a pointer to a GateHwi_Handle which enables GateSwi_delete to set the GateHwi handle to NULL.

Parameters
gatepointer to a GateSwi handle

§ GateSwi_destruct()

void GateSwi_destruct ( GateSwi_Struct obj)

Destruct a GateSwi gate.

Parameters
objpointer to a GateSwi objects

§ GateSwi_Params_init()

void GateSwi_Params_init ( GateSwi_Params prms)

Initialize the GateSwi_Params structure with default values.

GateSwi_Params_init initializes the GateHwi_Params structure with default values. GateSwi_Params_init should always be called before setting individual parameter fields. This allows new fields to be added in the future with compatible defaults – existing source code does not need to change when new fields are added.

Parameters
prmspointer to uninitialized params structure

§ GateSwi_enter()

intptr_t GateSwi_enter ( GateSwi_Handle  gate)

enter the GateSwi gate

GateSwi_enter enters the GateHwi gate and returns a key for use by GateSwi_enter. GateHwi_enter calls can be nested and the key is used to unlock the gate on the final call to GateSwi_leave.

Parameters
gateGateSwi handle
Return values
opaquekey to be passed to GateSwi_leave()

§ GateSwi_leave()

void GateSwi_leave ( GateSwi_Handle  gate,
intptr_t  key 
)

leave the GateSwi gate

GateSwi_leave exits the GateHwi gate if key matches the outermost call to GateSwi_enter. If GateHwi_enter calls are nested, the key will keep the nested calls from leaving the gate.

Parameters
gateGateSwi handle
keyopaque key to unlock the gate
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale