SYS/BIOS
7.00
|
Go to the source code of this file.
Enumerations | |
enum | svc_num_t { TZ_INIT_CONTEXT_SYSTEM, TZ_ALLOC_MODULE_CONTEXT, TZ_FREE_MODULE_CONTEXT, TZ_LOAD_CONTEXT, TZ_STORE_CONTEXT } |
Functions | |
uint32_t | initContextSystem () |
uint32_t | allocModuleContext (uint32_t modId) |
uint32_t | freeModuleContext (uint32_t modId) |
uint32_t | loadContext (uint32_t modId) |
uint32_t | storeContext (uint32_t modId) |
enum svc_num_t |
uint32_t initContextSystem | ( | ) |
uint32_t allocModuleContext | ( | uint32_t | modId | ) |
uint32_t freeModuleContext | ( | uint32_t | modId | ) |
uint32_t loadContext | ( | uint32_t | modId | ) |
uint32_t storeContext | ( | uint32_t | modId | ) |