![]() |
![]() |
SYS/BIOS
7.00
|
#include <ti/sysbios/knl/Task.h>
Data Fields | |
char * | name |
Optional name for the object. NULL by default. More... | |
uintptr_t | arg0 |
Task function argument. Default is 0. More... | |
uintptr_t | arg1 |
Task function argument. Default is 0. More... | |
int | priority |
Task priority. More... | |
void * | stack |
Task stack pointer. Default = null. More... | |
size_t | stackSize |
Task stack size. More... | |
IHeap_Handle | stackHeap |
Mem heap used for dynamically created task stack. More... | |
void * | env |
Global environment struct. More... | |
bool | vitalTaskFlag |
Exit system immediately when the last task with this flag set to true has terminated. More... | |
char* Task_Params::name |
Optional name for the object. NULL by default.
uintptr_t Task_Params::arg0 |
Task function argument. Default is 0.
uintptr_t Task_Params::arg1 |
Task function argument. Default is 0.
int Task_Params::priority |
Task priority.
void* Task_Params::stack |
Task stack pointer. Default = null.
NULL indicates that the stack is to be allocated by create().
size_t Task_Params::stackSize |
Task stack size.
IHeap_Handle Task_Params::stackHeap |
Mem heap used for dynamically created task stack.
The default value of NULL means that BIOS heap is used.
void* Task_Params::env |
Global environment struct.
bool Task_Params::vitalTaskFlag |
Exit system immediately when the last task with this flag set to true has terminated.
Default is true.