![]() |
![]() |
SYS/BIOS
7.00
|
Stat structure for the HeapMem_getExtendedStats function. More...
#include <ti/sysbios/heaps/HeapMem.h>
Data Fields | |
void * | buf |
Buffer being managed by this heap instance. More... | |
size_t | size |
Size of buffer being managed by this heap instance. More... | |
Stat structure for the HeapMem_getExtendedStats function.
void* HeapMem_ExtendedStats::buf |
Buffer being managed by this heap instance.
This parameter is ignored in the static HeapMem.create() call. It is a required parameter in the dynamic HeapMem_create() call.
HeapMem requires that the buffer be aligned on a target-specific minimum alignment, and will adjust the buffer's start address and size as necessary to satisfy this requirement.
size_t HeapMem_ExtendedStats::size |
Size of buffer being managed by this heap instance.
The usable size may be smaller depending on alignment requirements.