![]() |
![]() |
SYS/BIOS
7.00
|
Basic system services.
This module provides basic low-level "system" services; e.g., character output, printf
-like output, and exit handling.
#include <stdarg.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
Macros | |
#define | System_A_cannotFitIntoArg "sizeof(float) > sizeof(intptr_t)" |
Assert that the target's float type fits in an intptr_t More... | |
Typedefs | |
typedef void(* | System_AtexitHandler) (int arg1) |
System 's atexit function prototype. More... | |
typedef void(* | System_AbortFxn) (void) |
System abort function prototype. More... | |
typedef void(* | System_ExitFxn) (int arg1) |
System exit function prototype. More... | |
Functions | |
void | System_abort (const char *str) |
Print a message and abort currently running executable. More... | |
void | System_abortStd (void) |
ANSI C Standard implementation of abortFxn function. More... | |
void | System_abortSpin (void) |
Lightweight implementation of abortFxn function. More... | |
bool | System_atexit (System_AtexitHandler handler) |
Add an exit handler. More... | |
void | System_exit (int stat) |
Exit currently running executable. More... | |
void | System_exitStd (int stat) |
Implements an exitFxn function. More... | |
void | System_exitSpin (int stat) |
Implements an exitFxn function. More... | |
void | System_putch (char ch) |
Output a single character. More... | |
void | System_flush (void) |
Flush standard System I/O. More... | |
int | System_printf (const char *fmt,...) |
A smaller faster printf. More... | |
int | System_sprintf (char buf[], const char *fmt,...) |
Write formated output to a character buffer. More... | |
int | System_vprintf (const char *fmt, va_list va) |
A va_list printf. More... | |
int | System_vsprintf (char buf[], const char *fmt, va_list va) |
A va_list sprintf. More... | |
int | System_snprintf (char buf[], size_t n, const char *fmt,...) |
Write formated output to a character buffer. More... | |
int | System_vsnprintf (char buf[], size_t n, const char *fmt, va_list va) |
A va_list snprintf. More... | |
Variables | |
const int | System_maxAtexitHandlers |
Maximum number of dynamic atexit handlers allowed in the system. More... | |
const System_AbortFxn | System_abortFxn |
Abort handler function. More... | |
const System_ExitFxn | System_exitFxn |
Exit handler function. More... | |
#define System_A_cannotFitIntoArg "sizeof(float) > sizeof(intptr_t)" |
Assert that the target's float
type fits in an intptr_t
This assertion is triggered when the f
format specifier is used, the argument treated as an intptr_t
, but for the current target sizeof(Float)
> sizeof(intptr_t)
.
typedef void(* System_AtexitHandler) (int arg1) |
System
's atexit function prototype.
Functions of this type can be added to the list of functions that are executed during application termination.
typedef void(* System_AbortFxn) (void) |
System abort function prototype.
Functions of this type can be plugged into System
's abort function that will be executed during abnormal application termination.
typedef void(* System_ExitFxn) (int arg1) |
System exit function prototype.
Functions of this type can be plugged into System
's exit function that will be executed during normal application termination.
void System_abort | ( | const char * | str | ) |
Print a message and abort currently running executable.
This is called when an executable abnormally terminates. No exit functions bound via System_atexit()
or the ANSI C Standard Library atexit()
functions are executed.
str | abort message (not a format string) |
void System_abortStd | ( | void | ) |
ANSI C Standard implementation of abortFxn function.
This function calls ANSI C Standard abort()
to terminate currently running executable. This function is used by default in System_abortFxn.
void System_abortSpin | ( | void | ) |
Lightweight implementation of abortFxn function.
This functions loops indefinitely. This can used as an alternative System_abortFxn when a lightweight implementation is required instead of the ANSI C Standard abort()
.
bool System_atexit | ( | System_AtexitHandler | handler | ) |
Add an exit handler.
System_atexit
pushes handler
onto an internal stack of functions to be executed when system is exiting (e.g. System_exit
is called). Up to System_maxAtexitHandlers functions can be specified in this manner. During the exit processing, the functions are popped off the internal stack and called until the stack is empty.
The System
gate is entered before the System_atexit
functions are called.
Returns true
on success. If false
is returned, the exit handler was not added and it will not be called during an exit.
handler | the AtexitHandler to invoke during system |
true | if handler was registered successfully, false otherwise |
void System_exit | ( | int | stat | ) |
Exit currently running executable.
This function is called when an executable needs to terminate normally. This function processes all functions bound via System_atexit
and then calls System_exitFxn.
stat | exit status to return to calling environment. |
void System_exitStd | ( | int | stat | ) |
Implements an exitFxn
function.
This function calls ANSI C Standard exit()
to terminate currently running executable normally. This function is used by default in System_exitFxn.
stat | exit status to return to calling environment. |
void System_exitSpin | ( | int | stat | ) |
Implements an exitFxn
function.
This functions loops indefinitely. This can used as an alternative System_exitFxn when a light weight implementation is required instead of the ANSI C Standard exit()
.
stat | exit status to return to calling environment. |
void System_putch | ( | char | ch | ) |
Output a single character.
The SystemSupport module's putch
function is called by this function.
ch | character to be output. |
void System_flush | ( | void | ) |
Flush standard System I/O.
This function causes any buffered output characters are "written" to the output device.
The SystemSupport module's flush
function is called by this function.
int System_printf | ( | const char * | fmt, |
... | |||
) |
A smaller faster printf.
This function behaves much like the ANSI C Standard printf
but does not support the full range of format strings specified by the C Standard. In addition, several non-standard format specifiers are recognized.
The format string is a character string composed of zero or more directives: ordinary characters (not %), which are copied unchanged to the output stream; and conversion specifications, each of which results in fetching zero or more subsequent arguments. Each conversion specification is introduced by the character %, and ends with a conversion specifier. In between there may be (in this order) zero or more flags, an optional minimum field width, an optional precision and an optional length modifier.
The following flags are supported:
-
The converted value is to be left adjusted on the field boundary (the default is right justification.) - 0
The value should be zero padded. For d, i, o, u, and x conversions, the converted value is padded on the left with zeros rather than blanks.The optional field width specifier is a decimal digit string (with nonzero first digit) specifying a minimum field width. If the converted value has fewer characters than the field width, it will be padded with spaces on the left (or right, if the left-adjustment flag has been given). Instead of a decimal digit string one may write *
to specify that the field width is given in the next argument. A negative field width is taken as a '-' flag followed by a positive field width.
The optional precision specifier is a period ('.') followed by an optional decimal digit string. Instead of a decimal digit string one may write *
to specify that the precision is given in the next argument which must be of type int.
If the precision is given as just '.', or the precision is negative, the precision is taken to be zero. This gives the minimum number of digits to appear for d, i, o, u, and x conversions, or the maximum number of characters to be printed from a string for s conversions.
The optional length modifier is a single character from the following list.
l
A following integer conversion corresponds to a long int or unsigned long int argumentThe following conversion specifiers are supported.
d
, i
signed integer - u
unsigned decimal - x
unsigned hex - o
unsigned octal - p
pointer (@ + hex num) - c
character - s
stringThe following conversion specifiers are optionally supported. See the System_extendedFormats configuration parameter for more information about how to enable these conversion specifiers.
fmt | a 'printf-style' format string |
number | of characters written |
int System_sprintf | ( | char | buf[], |
const char * | fmt, | ||
... | |||
) |
Write formated output to a character buffer.
This function is identical to System_printf except that the output is copied to the specified character buffer buf
followed by a terminating '\0' character.
System_sprintf
returns the number of characters output not including the '\0' termination character.
buf | a character output buffer |
fmt | a 'printf-style' format string |
number | of characters written |
int System_vprintf | ( | const char * | fmt, |
va_list | va | ||
) |
A va_list printf.
This function is identical to System_printf except that its arguments are passed via a va_list (a "varargs list").
by the fmt string
System_vprintf
returns the number of characters output.
fmt | a standard 'printf-style' format string. |
va | an args list that points to the arguments referenced |
number | of characters written |
int System_vsprintf | ( | char | buf[], |
const char * | fmt, | ||
va_list | va | ||
) |
A va_list
sprintf.
This function is identical to System_sprintf except that its arguments are passed via a va_list
(a "varargs list").
by the fmt
string
vsprintf
returns the number of characters output.
buf | a character output buffer |
fmt | a standard 'printf -style' format string. |
va | an arguments list that points to the arguments referenced |
number | of characters written |
int System_snprintf | ( | char | buf[], |
size_t | n, | ||
const char * | fmt, | ||
... | |||
) |
Write formated output to a character buffer.
This function is identical to System_sprintf except that at most n
characters are copied to the specified character buffer buf
. If n is zero, nothing is written to character buffer. Otherwise, output characters beyond the n
- 1 are discarded rather than being written to the character buf, and a null character is written at the end of the characters written into the buffer.
the output buffer buf
snprintf
returns the number of characters that would have been written had n
been sufficiently large, not counting the terminating '\0' character.
buf | a character output buffer |
n | the maximum number of characters, including '\0', written to |
fmt | a 'printf-style' format string |
number | of characters written |
int System_vsnprintf | ( | char | buf[], |
size_t | n, | ||
const char * | fmt, | ||
va_list | va | ||
) |
A va_list
snprintf.
This function is identical to System_snprintf except that its arguments are passed via a va_list
(a "varargs list").
output buffer
by the fmt
string
vsnprintf
returns the number of characters that would have been written had n
been sufficiently large, not counting the terminating '\0' character.
buf | a character output buffer |
n | at most number of characters including '\0' written to |
fmt | a standard 'printf -style' format string. |
va | an arguments list that points to the arguments referenced |
number | of characters written |
const int System_maxAtexitHandlers |
Maximum number of dynamic atexit handlers allowed in the system.
Maximum number of System
atexit
handlers set during runtime via the System_atexit function.
const System_AbortFxn System_abortFxn |
Abort handler function.
This configuration parameter allows user to plug in their own abort function. By default System_abortStd which calls ANSI C Standard abort()
is plugged in. Alternatively System_abortSpin can be plugged which loops infinitely.
const System_ExitFxn System_exitFxn |
Exit handler function.
This configuration parameter allows user to plug in their own exit function. By default System_exitStd which calls ANSI C Standard exit()
is plugged in. Alternatively System_exitSpin can be plugged which loops infinitely.