![]() |
![]() |
TI-15.4 Stack API
4.30.00.34
|
#include <api_mac.h>
Data Fields | |
uint8_t | logicalChannel |
uint8_t | channelPage |
uint8_t | phyID |
uint8_t | trackBeacon |
MAC_MlmeSyncReq type
uint8_t _apimac_mlmesyncreq::logicalChannel |
The logical channel to use
uint8_t _apimac_mlmesyncreq::channelPage |
The channel page to use
uint8_t _apimac_mlmesyncreq::phyID |
PHY ID corresponding to the PHY descriptor to use
uint8_t _apimac_mlmesyncreq::trackBeacon |
Set to TRUE to continue tracking beacons after synchronizing with the first beacon. Set to FALSE to only synchronize with the first beacon