TI BLE5-Stack API Documentation  2.02.03.00
Data Fields
hciEvt_BLECteConnectionIqReport_t Struct Reference

LE CTE Connection IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connEvent
 connection event
 
uint16 connHandle
 connection handle
 
uint8 cteType
 cte type
 
uint8 dataChIndex
 index of data channel
 
osal_event_hdr_t hdr
 osal event header
 
int8 * iqSamples
 list of interleaved I/Q samples
 
uint8 phy
 current phy
 
uint16 rssi
 current rssi
 
uint8 rssiAntenna
 antenna ID
 
uint8 sampleCount
 number of samples
 
uint8 slotDuration
 sampling slot 1us or 2us
 
uint8 status
 packet status (success or CRC error)
 

Detailed Description

LE CTE Connection IQ Report Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale