TI BLE5-Stack API Documentation  2.02.03.00
Macros
OAD Service UUIDs

Macros

#define OAD_EXT_CTRL_UUID   0xFFC5
 
#define OAD_IMG_BLOCK_UUID   0xFFC2
 
#define OAD_IMG_COUNT_UUID   0xFFC3
 
#define OAD_IMG_IDENTIFY_UUID   0xFFC1
 
#define OAD_IMG_STATUS_UUID   0xFFC4
 
#define OAD_SERVICE_UUID   0xFFC0
 

Detailed Description

OAD Service UUIDs: Warning! The image count and image status chars are deprecated their functionality has been moved to the control point

Macro Definition Documentation

§ OAD_EXT_CTRL_UUID

#define OAD_EXT_CTRL_UUID   0xFFC5

16-bit root of the OAD Extended Control Point Characteristic UUID.

§ OAD_IMG_BLOCK_UUID

#define OAD_IMG_BLOCK_UUID   0xFFC2

16-bit root of the OAD Image Block Characteristic UUID.

§ OAD_IMG_COUNT_UUID

#define OAD_IMG_COUNT_UUID   0xFFC3

16-bit root of the OAD Image Count Characteristic UUID.

Warning
This characteristic is deprecated

§ OAD_IMG_IDENTIFY_UUID

#define OAD_IMG_IDENTIFY_UUID   0xFFC1

16-bit root of the OAD Image Identify Characteristic UUID.

§ OAD_IMG_STATUS_UUID

#define OAD_IMG_STATUS_UUID   0xFFC4

16-bit root of the OAD Image Status Characteristic UUID.

Warning
This characteristic is deprecated. Status info is now reported through the extended control characteristic.

§ OAD_SERVICE_UUID

#define OAD_SERVICE_UUID   0xFFC0

16-bit root of the OAD Service UUID.

Note
the service and chars will use the 128-bit TI base UUID
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale