![]() |
0.01.00
|
This file contains definitions of spinel API. More...
#include <stdarg.h>#include <stdbool.h>#include <stdint.h>Go to the source code of this file.
Classes | |
| struct | spinel_eui64_t |
| struct | spinel_net_xpanid_t |
| struct | spinel_net_pskc_t |
| struct | spinel_eui48_t |
| struct | spinel_ipv6addr_t |
Macros | |
| #define | __BEGIN_DECLS |
| #define | __END_DECLS |
| #define | SPINEL_API_EXTERN extern |
| #define | SPINEL_API_NONNULL_ALL |
| #define | SPINEL_API_WARN_UNUSED_RESULT |
| #define | SPINEL_PROTOCOL_VERSION_THREAD_MAJOR 4 |
| #define | SPINEL_PROTOCOL_VERSION_THREAD_MINOR 3 |
| #define | SPINEL_FRAME_MAX_SIZE 1300 |
| #define | SPINEL_ENCRYPTER_EXTRA_DATA_SIZE 0 |
| The size of extra data to be allocated for spinel frame buffer, needed by Spinel Encrypter. | |
| #define | SPINEL_FRAME_BUFFER_SIZE (SPINEL_FRAME_MAX_SIZE + SPINEL_ENCRYPTER_EXTRA_DATA_SIZE) |
| The size of buffer large enough to fit one whole spinel frame with extra data needed by Spinel Encrypter. | |
| #define | SPINEL_BIT_MASK(bit_index, field_bit_count) ((1 << ((field_bit_count)-1)) >> (bit_index)) |
| Macro for generating bit masks using bit index from the spec. | |
| #define | SPINEL_HEADER_FLAG 0x80 |
| #define | SPINEL_HEADER_TID_SHIFT 0 |
| #define | SPINEL_HEADER_TID_MASK (15 << SPINEL_HEADER_TID_SHIFT) |
| #define | SPINEL_HEADER_IID_SHIFT 4 |
| #define | SPINEL_HEADER_IID_MASK (3 << SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_IID_0 (0 << SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_IID_1 (1 << SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_IID_2 (2 << SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_IID_3 (3 << SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_GET_IID(x) (((x)&SPINEL_HEADER_IID_MASK) >> SPINEL_HEADER_IID_SHIFT) |
| #define | SPINEL_HEADER_GET_TID(x) (spinel_tid_t)(((x)&SPINEL_HEADER_TID_MASK) >> SPINEL_HEADER_TID_SHIFT) |
| #define | SPINEL_GET_NEXT_TID(x) (spinel_tid_t)((x) >= 0xF ? 1 : (x) + 1) |
| #define | SPINEL_BEACON_THREAD_FLAG_VERSION_SHIFT 4 |
| #define | SPINEL_BEACON_THREAD_FLAG_VERSION_MASK (0xf << SPINEL_BEACON_THREAD_FLAG_VERSION_SHIFT) |
| #define | SPINEL_BEACON_THREAD_FLAG_JOINABLE (1 << 0) |
| #define | SPINEL_BEACON_THREAD_FLAG_NATIVE (1 << 3) |
| #define | SPINEL_DATATYPE_NULL_S "" |
| #define | SPINEL_DATATYPE_VOID_S "." |
| #define | SPINEL_DATATYPE_BOOL_S "b" |
| #define | SPINEL_DATATYPE_UINT8_S "C" |
| #define | SPINEL_DATATYPE_INT8_S "c" |
| #define | SPINEL_DATATYPE_UINT16_S "S" |
| #define | SPINEL_DATATYPE_INT16_S "s" |
| #define | SPINEL_DATATYPE_UINT32_S "L" |
| #define | SPINEL_DATATYPE_INT32_S "l" |
| #define | SPINEL_DATATYPE_UINT64_S "X" |
| #define | SPINEL_DATATYPE_INT64_S "x" |
| #define | SPINEL_DATATYPE_UINT_PACKED_S "i" |
| #define | SPINEL_DATATYPE_IPv6ADDR_S "6" |
| #define | SPINEL_DATATYPE_EUI64_S "E" |
| #define | SPINEL_DATATYPE_EUI48_S "e" |
| #define | SPINEL_DATATYPE_DATA_WLEN_S "d" |
| #define | SPINEL_DATATYPE_DATA_S "D" |
| #define | SPINEL_DATATYPE_UTF8_S "U" |
| Zero-Terminated UTF8-Encoded String. | |
| #define | SPINEL_DATATYPE_ARRAY_S(x) "A(" x ")" |
| #define | SPINEL_DATATYPE_STRUCT_S(x) "t(" x ")" |
| #define | SPINEL_DATATYPE_ARRAY_STRUCT_S(x) SPINEL_DATATYPE_ARRAY_S(SPINEL_DATATYPE_STRUCT_WLEN_S(x)) |
| #define | SPINEL_DATATYPE_COMMAND_S |
| #define | SPINEL_DATATYPE_COMMAND_PROP_S |
| #define | SPINEL_DATATYPE_MAC_SCAN_RESULT_S(mac_format_str, net_format_str) |
| #define | SPINEL_802_15_4_DATATYPE_MAC_SCAN_RESULT_V1_S |
| #define | SPINEL_NET_DATATYPE_MAC_SCAN_RESULT_V1_S |
| #define | SPINEL_NET_DATATYPE_MAC_SCAN_RESULT_V2_S |
| #define | SPINEL_MAX_UINT_PACKED 2097151 |
Typedefs | |
| typedef int | spinel_ssize_t |
| typedef unsigned int | spinel_size_t |
| typedef uint8_t | spinel_tid_t |
| typedef unsigned int | spinel_cid_t |
| typedef char | spinel_datatype_t |
Enumerations | |
| enum | spinel_status_t { SPINEL_STATUS_OK = 0, SPINEL_STATUS_FAILURE = 1, SPINEL_STATUS_UNIMPLEMENTED = 2, SPINEL_STATUS_INVALID_ARGUMENT = 3, SPINEL_STATUS_INVALID_STATE = 4, SPINEL_STATUS_INVALID_COMMAND = 5, SPINEL_STATUS_INVALID_INTERFACE = 6, SPINEL_STATUS_INTERNAL_ERROR = 7, SPINEL_STATUS_SECURITY_ERROR = 8, SPINEL_STATUS_PARSE_ERROR = 9, SPINEL_STATUS_IN_PROGRESS = 10, SPINEL_STATUS_NOMEM = 11, SPINEL_STATUS_BUSY = 12, SPINEL_STATUS_PROP_NOT_FOUND = 13, SPINEL_STATUS_DROPPED = 14, SPINEL_STATUS_EMPTY = 15, SPINEL_STATUS_CMD_TOO_BIG = 16, SPINEL_STATUS_NO_ACK = 17, SPINEL_STATUS_CCA_FAILURE = 18, SPINEL_STATUS_ALREADY = 19, SPINEL_STATUS_ITEM_NOT_FOUND = 20, SPINEL_STATUS_INVALID_COMMAND_FOR_PROP = 21, SPINEL_STATUS_JOIN__BEGIN = 104, SPINEL_STATUS_JOIN_FAILURE = SPINEL_STATUS_JOIN__BEGIN + 0, SPINEL_STATUS_JOIN_SECURITY = SPINEL_STATUS_JOIN__BEGIN + 1, SPINEL_STATUS_JOIN_NO_PEERS = SPINEL_STATUS_JOIN__BEGIN + 2, SPINEL_STATUS_JOIN_INCOMPATIBLE = SPINEL_STATUS_JOIN__BEGIN + 3, SPINEL_STATUS_JOIN_RSP_TIMEOUT = SPINEL_STATUS_JOIN__BEGIN + 4, SPINEL_STATUS_JOIN_SUCCESS = SPINEL_STATUS_JOIN__BEGIN + 5, SPINEL_STATUS_JOIN__END = 112, SPINEL_STATUS_RESET__BEGIN = 112, SPINEL_STATUS_RESET_POWER_ON = SPINEL_STATUS_RESET__BEGIN + 0, SPINEL_STATUS_RESET_EXTERNAL = SPINEL_STATUS_RESET__BEGIN + 1, SPINEL_STATUS_RESET_SOFTWARE = SPINEL_STATUS_RESET__BEGIN + 2, SPINEL_STATUS_RESET_FAULT = SPINEL_STATUS_RESET__BEGIN + 3, SPINEL_STATUS_RESET_CRASH = SPINEL_STATUS_RESET__BEGIN + 4, SPINEL_STATUS_RESET_ASSERT = SPINEL_STATUS_RESET__BEGIN + 5, SPINEL_STATUS_RESET_OTHER = SPINEL_STATUS_RESET__BEGIN + 6, SPINEL_STATUS_RESET_UNKNOWN = SPINEL_STATUS_RESET__BEGIN + 7, SPINEL_STATUS_RESET_WATCHDOG = SPINEL_STATUS_RESET__BEGIN + 8, SPINEL_STATUS_RESET__END = 128, SPINEL_STATUS_VENDOR__BEGIN = 15360, SPINEL_STATUS_VENDOR__END = 16384, SPINEL_STATUS_STACK_NATIVE__BEGIN = 16384, SPINEL_STATUS_STACK_NATIVE__END = 81920, SPINEL_STATUS_EXPERIMENTAL__BEGIN = 2000000, SPINEL_STATUS_EXPERIMENTAL__END = 2097152 } |
| enum | spinel_net_role_t { SPINEL_NET_ROLE_DETACHED = 0, SPINEL_NET_ROLE_CHILD = 1, SPINEL_NET_ROLE_ROUTER = 2, SPINEL_NET_ROLE_LEADER = 3 } |
| enum | spinel_ipv6_icmp_ping_offload_mode_t { SPINEL_IPV6_ICMP_PING_OFFLOAD_DISABLED = 0, SPINEL_IPV6_ICMP_PING_OFFLOAD_UNICAST_ONLY = 1, SPINEL_IPV6_ICMP_PING_OFFLOAD_MULTICAST_ONLY = 2, SPINEL_IPV6_ICMP_PING_OFFLOAD_ALL = 3 } |
| enum | spinel_scan_state_t { SPINEL_SCAN_STATE_IDLE = 0, SPINEL_SCAN_STATE_BEACON = 1, SPINEL_SCAN_STATE_ENERGY = 2, SPINEL_SCAN_STATE_DISCOVER = 3 } |
| enum | spinel_mcu_power_state_t { SPINEL_MCU_POWER_STATE_ON = 0, SPINEL_MCU_POWER_STATE_LOW_POWER = 1, SPINEL_MCU_POWER_STATE_OFF = 2 } |
| enum | spinel_power_state_t { SPINEL_POWER_STATE_OFFLINE = 0, SPINEL_POWER_STATE_DEEP_SLEEP = 1, SPINEL_POWER_STATE_STANDBY = 2, SPINEL_POWER_STATE_LOW_POWER = 3, SPINEL_POWER_STATE_ONLINE = 4 } |
| enum | spinel_host_power_state_t { SPINEL_HOST_POWER_STATE_OFFLINE = 0, SPINEL_HOST_POWER_STATE_DEEP_SLEEP = 1, SPINEL_HOST_POWER_STATE_RESERVED = 2, SPINEL_HOST_POWER_STATE_LOW_POWER = 3, SPINEL_HOST_POWER_STATE_ONLINE = 4 } |
| enum | { SPINEL_NET_FLAG_ON_MESH = (1 << 0), SPINEL_NET_FLAG_DEFAULT_ROUTE = (1 << 1), SPINEL_NET_FLAG_CONFIGURE = (1 << 2), SPINEL_NET_FLAG_DHCP = (1 << 3), SPINEL_NET_FLAG_SLAAC = (1 << 4), SPINEL_NET_FLAG_PREFERRED = (1 << 5), SPINEL_NET_FLAG_PREFERENCE_OFFSET = 6, SPINEL_NET_FLAG_PREFERENCE_MASK = (3 << SPINEL_NET_FLAG_PREFERENCE_OFFSET) } |
| enum | { SPINEL_ROUTE_PREFERENCE_HIGH = (1 << SPINEL_NET_FLAG_PREFERENCE_OFFSET), SPINEL_ROUTE_PREFERENCE_MEDIUM = (0 << SPINEL_NET_FLAG_PREFERENCE_OFFSET), SPINEL_ROUTE_PREFERENCE_LOW = (3 << SPINEL_NET_FLAG_PREFERENCE_OFFSET) } |
| enum | { SPINEL_THREAD_MODE_FULL_NETWORK_DATA = (1 << 0), SPINEL_THREAD_MODE_FULL_FUNCTION_DEV = (1 << 1), SPINEL_THREAD_MODE_SECURE_DATA_REQUEST = (1 << 2), SPINEL_THREAD_MODE_RX_ON_WHEN_IDLE = (1 << 3) } |
| enum | { SPINEL_GPIO_FLAG_DIR_INPUT = 0, SPINEL_GPIO_FLAG_DIR_OUTPUT = SPINEL_BIT_MASK(0, 8), SPINEL_GPIO_FLAG_PULL_UP = SPINEL_BIT_MASK(1, 8), SPINEL_GPIO_FLAG_PULL_DOWN = SPINEL_BIT_MASK(2, 8), SPINEL_GPIO_FLAG_OPEN_DRAIN = SPINEL_BIT_MASK(2, 8), SPINEL_GPIO_FLAG_TRIGGER_NONE = 0, SPINEL_GPIO_FLAG_TRIGGER_RISING = SPINEL_BIT_MASK(3, 8), SPINEL_GPIO_FLAG_TRIGGER_FALLING = SPINEL_BIT_MASK(4, 8), SPINEL_GPIO_FLAG_TRIGGER_ANY = SPINEL_GPIO_FLAG_TRIGGER_RISING | SPINEL_GPIO_FLAG_TRIGGER_FALLING } |
| enum | { SPINEL_PROTOCOL_TYPE_BOOTLOADER = 0, SPINEL_PROTOCOL_TYPE_ZIGBEE_IP = 2, SPINEL_PROTOCOL_TYPE_THREAD = 3 } |
| enum | { SPINEL_MAC_PROMISCUOUS_MODE_OFF = 0, SPINEL_MAC_PROMISCUOUS_MODE_NETWORK = 1, SPINEL_MAC_PROMISCUOUS_MODE_FULL = 2 } |
| enum | { SPINEL_NCP_LOG_LEVEL_EMERG = 0, SPINEL_NCP_LOG_LEVEL_ALERT = 1, SPINEL_NCP_LOG_LEVEL_CRIT = 2, SPINEL_NCP_LOG_LEVEL_ERR = 3, SPINEL_NCP_LOG_LEVEL_WARN = 4, SPINEL_NCP_LOG_LEVEL_NOTICE = 5, SPINEL_NCP_LOG_LEVEL_INFO = 6, SPINEL_NCP_LOG_LEVEL_DEBUG = 7 } |
| enum | { SPINEL_NCP_LOG_REGION_NONE = 0, SPINEL_NCP_LOG_REGION_OT_API = 1, SPINEL_NCP_LOG_REGION_OT_MLE = 2, SPINEL_NCP_LOG_REGION_OT_ARP = 3, SPINEL_NCP_LOG_REGION_OT_NET_DATA = 4, SPINEL_NCP_LOG_REGION_OT_ICMP = 5, SPINEL_NCP_LOG_REGION_OT_IP6 = 6, SPINEL_NCP_LOG_REGION_OT_MAC = 7, SPINEL_NCP_LOG_REGION_OT_MEM = 8, SPINEL_NCP_LOG_REGION_OT_NCP = 9, SPINEL_NCP_LOG_REGION_OT_MESH_COP = 10, SPINEL_NCP_LOG_REGION_OT_NET_DIAG = 11, SPINEL_NCP_LOG_REGION_OT_PLATFORM = 12, SPINEL_NCP_LOG_REGION_OT_COAP = 13, SPINEL_NCP_LOG_REGION_OT_CLI = 14, SPINEL_NCP_LOG_REGION_OT_CORE = 15, SPINEL_NCP_LOG_REGION_OT_UTIL = 16 } |
| enum | { SPINEL_MESHCOP_COMMISSIONER_STATE_DISABLED = 0, SPINEL_MESHCOP_COMMISSIONER_STATE_PETITION = 1, SPINEL_MESHCOP_COMMISSIONER_STATE_ACTIVE = 2 } |
| enum | { SPINEL_MD_FLAG_TX = 0x0001, SPINEL_MD_FLAG_BAD_FCS = 0x0004, SPINEL_MD_FLAG_DUPE = 0x0008, SPINEL_MD_FLAG_RESERVED = 0xFFF2 } |
| enum | { SPINEL_CMD_NOOP = 0, SPINEL_CMD_RESET = 1, SPINEL_CMD_PROP_VALUE_GET = 2, SPINEL_CMD_PROP_VALUE_SET = 3, SPINEL_CMD_PROP_VALUE_INSERT = 4, SPINEL_CMD_PROP_VALUE_REMOVE = 5, SPINEL_CMD_PROP_VALUE_IS = 6, SPINEL_CMD_PROP_VALUE_INSERTED = 7, SPINEL_CMD_PROP_VALUE_REMOVED = 8, SPINEL_CMD_NET_SAVE = 9, SPINEL_CMD_NET_CLEAR = 10, SPINEL_CMD_NET_RECALL = 11, SPINEL_CMD_HBO_OFFLOAD = 12, SPINEL_CMD_HBO_RECLAIM = 13, SPINEL_CMD_HBO_DROP = 14, SPINEL_CMD_HBO_OFFLOADED = 15, SPINEL_CMD_HBO_RECLAIMED = 16, SPINEL_CMD_HBO_DROPED = 17, SPINEL_CMD_PEEK = 18, SPINEL_CMD_PEEK_RET = 19, SPINEL_CMD_POKE = 20, SPINEL_CMD_PROP_VALUE_MULTI_GET = 21, SPINEL_CMD_PROP_VALUE_MULTI_SET = 22, SPINEL_CMD_PROP_VALUES_ARE = 23, SPINEL_CMD_NEST__BEGIN = 15296, SPINEL_CMD_NEST__END = 15360, SPINEL_CMD_VENDOR__BEGIN = 15360, SPINEL_CMD_VENDOR__END = 16384, SPINEL_CMD_EXPERIMENTAL__BEGIN = 2000000, SPINEL_CMD_EXPERIMENTAL__END = 2097152 } |
| enum | { SPINEL_CAP_LOCK = 1, SPINEL_CAP_NET_SAVE = 2, SPINEL_CAP_HBO = 3, SPINEL_CAP_POWER_SAVE = 4, SPINEL_CAP_COUNTERS = 5, SPINEL_CAP_JAM_DETECT = 6, SPINEL_CAP_PEEK_POKE = 7, SPINEL_CAP_WRITABLE_RAW_STREAM = 8, SPINEL_CAP_GPIO = 9, SPINEL_CAP_TRNG = 10, SPINEL_CAP_CMD_MULTI = 11, SPINEL_CAP_UNSOL_UPDATE_FILTER = 12, SPINEL_CAP_MCU_POWER_STATE = 13, SPINEL_CAP_802_15_4__BEGIN = 16, SPINEL_CAP_802_15_4_2003 = (SPINEL_CAP_802_15_4__BEGIN + 0), SPINEL_CAP_802_15_4_2006 = (SPINEL_CAP_802_15_4__BEGIN + 1), SPINEL_CAP_802_15_4_2011 = (SPINEL_CAP_802_15_4__BEGIN + 2), SPINEL_CAP_802_15_4_PIB = (SPINEL_CAP_802_15_4__BEGIN + 5), SPINEL_CAP_802_15_4_2450MHZ_OQPSK = (SPINEL_CAP_802_15_4__BEGIN + 8), SPINEL_CAP_802_15_4_915MHZ_OQPSK = (SPINEL_CAP_802_15_4__BEGIN + 9), SPINEL_CAP_802_15_4_868MHZ_OQPSK = (SPINEL_CAP_802_15_4__BEGIN + 10), SPINEL_CAP_802_15_4_915MHZ_BPSK = (SPINEL_CAP_802_15_4__BEGIN + 11), SPINEL_CAP_802_15_4_868MHZ_BPSK = (SPINEL_CAP_802_15_4__BEGIN + 12), SPINEL_CAP_802_15_4_915MHZ_ASK = (SPINEL_CAP_802_15_4__BEGIN + 13), SPINEL_CAP_802_15_4_868MHZ_ASK = (SPINEL_CAP_802_15_4__BEGIN + 14), SPINEL_CAP_802_15_4__END = 32, SPINEL_CAP_ROLE__BEGIN = 48, SPINEL_CAP_ROLE_ROUTER = (SPINEL_CAP_ROLE__BEGIN + 0), SPINEL_CAP_ROLE_SLEEPY = (SPINEL_CAP_ROLE__BEGIN + 1), SPINEL_CAP_ROLE__END = 52, SPINEL_CAP_NET__BEGIN = 52, SPINEL_CAP_NET_THREAD_1_0 = (SPINEL_CAP_NET__BEGIN + 0), SPINEL_CAP_NET__END = 64, SPINEL_CAP_OPENTHREAD__BEGIN = 512, SPINEL_CAP_MAC_WHITELIST = (SPINEL_CAP_OPENTHREAD__BEGIN + 0), SPINEL_CAP_MAC_RAW = (SPINEL_CAP_OPENTHREAD__BEGIN + 1), SPINEL_CAP_OOB_STEERING_DATA = (SPINEL_CAP_OPENTHREAD__BEGIN + 2), SPINEL_CAP_CHANNEL_MONITOR = (SPINEL_CAP_OPENTHREAD__BEGIN + 3), SPINEL_CAP_ERROR_RATE_TRACKING = (SPINEL_CAP_OPENTHREAD__BEGIN + 4), SPINEL_CAP_CHANNEL_MANAGER = (SPINEL_CAP_OPENTHREAD__BEGIN + 5), SPINEL_CAP_OPENTHREAD_LOG_METADATA = (SPINEL_CAP_OPENTHREAD__BEGIN + 6), SPINEL_CAP_TIME_SYNC = (SPINEL_CAP_OPENTHREAD__BEGIN + 7), SPINEL_CAP_CHILD_SUPERVISION = (SPINEL_CAP_OPENTHREAD__BEGIN + 8), SPINEL_CAP_OPENTHREAD__END = 640, SPINEL_CAP_THREAD__BEGIN = 1024, SPINEL_CAP_THREAD_COMMISSIONER = (SPINEL_CAP_THREAD__BEGIN + 0), SPINEL_CAP_THREAD_TMF_PROXY = (SPINEL_CAP_THREAD__BEGIN + 1), SPINEL_CAP_THREAD_UDP_PROXY = (SPINEL_CAP_THREAD__BEGIN + 2), SPINEL_CAP_THREAD_JOINER = (SPINEL_CAP_THREAD__BEGIN + 3), SPINEL_CAP_THREAD__END = 1152, SPINEL_CAP_NEST__BEGIN = 15296, SPINEL_CAP_NEST_LEGACY_INTERFACE = (SPINEL_CAP_NEST__BEGIN + 0), SPINEL_CAP_NEST_LEGACY_NET_WAKE = (SPINEL_CAP_NEST__BEGIN + 1), SPINEL_CAP_NEST_TRANSMIT_HOOK = (SPINEL_CAP_NEST__BEGIN + 2), SPINEL_CAP_NEST__END = 15360, SPINEL_CAP_VENDOR__BEGIN = 15360, SPINEL_CAP_VENDOR__END = 16384, SPINEL_CAP_EXPERIMENTAL__BEGIN = 2000000, SPINEL_CAP_EXPERIMENTAL__END = 2097152 } |
| enum | spinel_prop_key_t { SPINEL_PROP_LAST_STATUS = 0, SPINEL_PROP_PROTOCOL_VERSION = 1, SPINEL_PROP_NCP_VERSION = 2, SPINEL_PROP_INTERFACE_TYPE = 3, SPINEL_PROP_VENDOR_ID = 4, SPINEL_PROP_CAPS = 5, SPINEL_PROP_INTERFACE_COUNT = 6, SPINEL_PROP_POWER_STATE = 7, SPINEL_PROP_HWADDR = 8, SPINEL_PROP_LOCK = 9, SPINEL_PROP_HBO_MEM_MAX = 10, SPINEL_PROP_HBO_BLOCK_MAX = 11, SPINEL_PROP_HOST_POWER_STATE = 12, SPINEL_PROP_MCU_POWER_STATE = 13, SPINEL_PROP_BASE_EXT__BEGIN = 0x1000, SPINEL_PROP_GPIO_CONFIG = SPINEL_PROP_BASE_EXT__BEGIN + 0, SPINEL_PROP_GPIO_STATE = SPINEL_PROP_BASE_EXT__BEGIN + 2, SPINEL_PROP_GPIO_STATE_SET = SPINEL_PROP_BASE_EXT__BEGIN + 3, SPINEL_PROP_GPIO_STATE_CLEAR = SPINEL_PROP_BASE_EXT__BEGIN + 4, SPINEL_PROP_TRNG_32 = SPINEL_PROP_BASE_EXT__BEGIN + 5, SPINEL_PROP_TRNG_128 = SPINEL_PROP_BASE_EXT__BEGIN + 6, SPINEL_PROP_TRNG_RAW_32 = SPINEL_PROP_BASE_EXT__BEGIN + 7, SPINEL_PROP_UNSOL_UPDATE_FILTER = SPINEL_PROP_BASE_EXT__BEGIN + 8, SPINEL_PROP_UNSOL_UPDATE_LIST = SPINEL_PROP_BASE_EXT__BEGIN + 9, SPINEL_PROP_BASE_EXT__END = 0x1100, SPINEL_PROP_PHY__BEGIN = 0x20, SPINEL_PROP_PHY_ENABLED = SPINEL_PROP_PHY__BEGIN + 0, SPINEL_PROP_PHY_CHAN = SPINEL_PROP_PHY__BEGIN + 1, SPINEL_PROP_PHY_CHAN_SUPPORTED = SPINEL_PROP_PHY__BEGIN + 2, SPINEL_PROP_PHY_FREQ = SPINEL_PROP_PHY__BEGIN + 3, SPINEL_PROP_PHY_CCA_THRESHOLD = SPINEL_PROP_PHY__BEGIN + 4, SPINEL_PROP_PHY_TX_POWER = SPINEL_PROP_PHY__BEGIN + 5, SPINEL_PROP_PHY_RSSI = SPINEL_PROP_PHY__BEGIN + 6, SPINEL_PROP_PHY_RX_SENSITIVITY = SPINEL_PROP_PHY__BEGIN + 7, SPINEL_PROP_PHY__END = 0x30, SPINEL_PROP_PHY_EXT__BEGIN = 0x1200, SPINEL_PROP_JAM_DETECT_ENABLE = SPINEL_PROP_PHY_EXT__BEGIN + 0, SPINEL_PROP_JAM_DETECTED = SPINEL_PROP_PHY_EXT__BEGIN + 1, SPINEL_PROP_JAM_DETECT_RSSI_THRESHOLD = SPINEL_PROP_PHY_EXT__BEGIN + 2, SPINEL_PROP_JAM_DETECT_WINDOW = SPINEL_PROP_PHY_EXT__BEGIN + 3, SPINEL_PROP_JAM_DETECT_BUSY = SPINEL_PROP_PHY_EXT__BEGIN + 4, SPINEL_PROP_JAM_DETECT_HISTORY_BITMAP = SPINEL_PROP_PHY_EXT__BEGIN + 5, SPINEL_PROP_CHANNEL_MONITOR_SAMPLE_INTERVAL = SPINEL_PROP_PHY_EXT__BEGIN + 6, SPINEL_PROP_CHANNEL_MONITOR_RSSI_THRESHOLD = SPINEL_PROP_PHY_EXT__BEGIN + 7, SPINEL_PROP_CHANNEL_MONITOR_SAMPLE_WINDOW = SPINEL_PROP_PHY_EXT__BEGIN + 8, SPINEL_PROP_CHANNEL_MONITOR_SAMPLE_COUNT = SPINEL_PROP_PHY_EXT__BEGIN + 9, SPINEL_PROP_CHANNEL_MONITOR_CHANNEL_OCCUPANCY = SPINEL_PROP_PHY_EXT__BEGIN + 10, SPINEL_PROP_PHY_EXT__END = 0x1300, SPINEL_PROP_MAC__BEGIN = 0x30, SPINEL_PROP_MAC_SCAN_STATE = SPINEL_PROP_MAC__BEGIN + 0, SPINEL_PROP_MAC_SCAN_MASK = SPINEL_PROP_MAC__BEGIN + 1, SPINEL_PROP_MAC_SCAN_PERIOD = SPINEL_PROP_MAC__BEGIN + 2, SPINEL_PROP_MAC_SCAN_BEACON = SPINEL_PROP_MAC__BEGIN + 3, SPINEL_PROP_MAC_15_4_LADDR = SPINEL_PROP_MAC__BEGIN + 4, SPINEL_PROP_MAC_15_4_SADDR = SPINEL_PROP_MAC__BEGIN + 5, SPINEL_PROP_MAC_15_4_PANID = SPINEL_PROP_MAC__BEGIN + 6, SPINEL_PROP_MAC_RAW_STREAM_ENABLED = SPINEL_PROP_MAC__BEGIN + 7, SPINEL_PROP_MAC_PROMISCUOUS_MODE = SPINEL_PROP_MAC__BEGIN + 8, SPINEL_PROP_MAC_ENERGY_SCAN_RESULT = SPINEL_PROP_MAC__BEGIN + 9, SPINEL_PROP_MAC_DATA_POLL_PERIOD = SPINEL_PROP_MAC__BEGIN + 10, SPINEL_PROP_MAC__END = 0x40, SPINEL_PROP_MAC_EXT__BEGIN = 0x1300, SPINEL_PROP_MAC_WHITELIST = SPINEL_PROP_MAC_EXT__BEGIN + 0, SPINEL_PROP_MAC_WHITELIST_ENABLED = SPINEL_PROP_MAC_EXT__BEGIN + 1, SPINEL_PROP_MAC_EXTENDED_ADDR = SPINEL_PROP_MAC_EXT__BEGIN + 2, SPINEL_PROP_MAC_SRC_MATCH_ENABLED = SPINEL_PROP_MAC_EXT__BEGIN + 3, SPINEL_PROP_MAC_SRC_MATCH_SHORT_ADDRESSES = SPINEL_PROP_MAC_EXT__BEGIN + 4, SPINEL_PROP_MAC_SRC_MATCH_EXTENDED_ADDRESSES = SPINEL_PROP_MAC_EXT__BEGIN + 5, SPINEL_PROP_MAC_BLACKLIST = SPINEL_PROP_MAC_EXT__BEGIN + 6, SPINEL_PROP_MAC_BLACKLIST_ENABLED = SPINEL_PROP_MAC_EXT__BEGIN + 7, SPINEL_PROP_MAC_FIXED_RSS = SPINEL_PROP_MAC_EXT__BEGIN + 8, SPINEL_PROP_MAC_CCA_FAILURE_RATE = SPINEL_PROP_MAC_EXT__BEGIN + 9, SPINEL_PROP_MAC_EXT__END = 0x1400, SPINEL_PROP_NET__BEGIN = 0x40, SPINEL_PROP_NET_SAVED = SPINEL_PROP_NET__BEGIN + 0, SPINEL_PROP_NET_IF_UP = SPINEL_PROP_NET__BEGIN + 1, SPINEL_PROP_NET_STACK_UP = SPINEL_PROP_NET__BEGIN + 2, SPINEL_PROP_NET_ROLE = SPINEL_PROP_NET__BEGIN + 3, SPINEL_PROP_NET_NETWORK_NAME = SPINEL_PROP_NET__BEGIN + 4, SPINEL_PROP_NET_XPANID = SPINEL_PROP_NET__BEGIN + 5, SPINEL_PROP_NET_MASTER_KEY = SPINEL_PROP_NET__BEGIN + 6, SPINEL_PROP_NET_KEY_SEQUENCE_COUNTER = SPINEL_PROP_NET__BEGIN + 7, SPINEL_PROP_NET_PARTITION_ID = SPINEL_PROP_NET__BEGIN + 8, SPINEL_PROP_NET_REQUIRE_JOIN_EXISTING = SPINEL_PROP_NET__BEGIN + 9, SPINEL_PROP_NET_KEY_SWITCH_GUARDTIME = SPINEL_PROP_NET__BEGIN + 10, SPINEL_PROP_NET_PSKC = SPINEL_PROP_NET__BEGIN + 11, SPINEL_PROP_NET__END = 0x50, SPINEL_PROP_NET_EXT__BEGIN = 0x1400, SPINEL_PROP_NET_EXT__END = 0x1500, SPINEL_PROP_THREAD__BEGIN = 0x50, SPINEL_PROP_THREAD_LEADER_ADDR = SPINEL_PROP_THREAD__BEGIN + 0, SPINEL_PROP_THREAD_PARENT = SPINEL_PROP_THREAD__BEGIN + 1, SPINEL_PROP_THREAD_CHILD_TABLE = SPINEL_PROP_THREAD__BEGIN + 2, SPINEL_PROP_THREAD_LEADER_RID = SPINEL_PROP_THREAD__BEGIN + 3, SPINEL_PROP_THREAD_LEADER_WEIGHT = SPINEL_PROP_THREAD__BEGIN + 4, SPINEL_PROP_THREAD_LOCAL_LEADER_WEIGHT = SPINEL_PROP_THREAD__BEGIN + 5, SPINEL_PROP_THREAD_NETWORK_DATA = SPINEL_PROP_THREAD__BEGIN + 6, SPINEL_PROP_THREAD_NETWORK_DATA_VERSION = SPINEL_PROP_THREAD__BEGIN + 7, SPINEL_PROP_THREAD_STABLE_NETWORK_DATA = SPINEL_PROP_THREAD__BEGIN + 8, SPINEL_PROP_THREAD_STABLE_NETWORK_DATA_VERSION = SPINEL_PROP_THREAD__BEGIN + 9, SPINEL_PROP_THREAD_ON_MESH_NETS = SPINEL_PROP_THREAD__BEGIN + 10, SPINEL_PROP_THREAD_OFF_MESH_ROUTES = SPINEL_PROP_THREAD__BEGIN + 11, SPINEL_PROP_THREAD_ASSISTING_PORTS = SPINEL_PROP_THREAD__BEGIN + 12, SPINEL_PROP_THREAD_ALLOW_LOCAL_NET_DATA_CHANGE = SPINEL_PROP_THREAD__BEGIN + 13, SPINEL_PROP_THREAD_MODE = SPINEL_PROP_THREAD__BEGIN + 14, SPINEL_PROP_THREAD__END = 0x60, SPINEL_PROP_THREAD_EXT__BEGIN = 0x1500, SPINEL_PROP_THREAD_CHILD_TIMEOUT = SPINEL_PROP_THREAD_EXT__BEGIN + 0, SPINEL_PROP_THREAD_RLOC16 = SPINEL_PROP_THREAD_EXT__BEGIN + 1, SPINEL_PROP_THREAD_ROUTER_UPGRADE_THRESHOLD = SPINEL_PROP_THREAD_EXT__BEGIN + 2, SPINEL_PROP_THREAD_CONTEXT_REUSE_DELAY = SPINEL_PROP_THREAD_EXT__BEGIN + 3, SPINEL_PROP_THREAD_NETWORK_ID_TIMEOUT = SPINEL_PROP_THREAD_EXT__BEGIN + 4, SPINEL_PROP_THREAD_ACTIVE_ROUTER_IDS = SPINEL_PROP_THREAD_EXT__BEGIN + 5, SPINEL_PROP_THREAD_RLOC16_DEBUG_PASSTHRU = SPINEL_PROP_THREAD_EXT__BEGIN + 6, SPINEL_PROP_THREAD_ROUTER_ROLE_ENABLED = SPINEL_PROP_THREAD_EXT__BEGIN + 7, SPINEL_PROP_THREAD_ROUTER_DOWNGRADE_THRESHOLD = SPINEL_PROP_THREAD_EXT__BEGIN + 8, SPINEL_PROP_THREAD_ROUTER_SELECTION_JITTER = SPINEL_PROP_THREAD_EXT__BEGIN + 9, SPINEL_PROP_THREAD_PREFERRED_ROUTER_ID = SPINEL_PROP_THREAD_EXT__BEGIN + 10, SPINEL_PROP_THREAD_NEIGHBOR_TABLE = SPINEL_PROP_THREAD_EXT__BEGIN + 11, SPINEL_PROP_THREAD_CHILD_COUNT_MAX = SPINEL_PROP_THREAD_EXT__BEGIN + 12, SPINEL_PROP_THREAD_LEADER_NETWORK_DATA = SPINEL_PROP_THREAD_EXT__BEGIN + 13, SPINEL_PROP_THREAD_STABLE_LEADER_NETWORK_DATA = SPINEL_PROP_THREAD_EXT__BEGIN + 14, SPINEL_PROP_THREAD_JOINERS = SPINEL_PROP_THREAD_EXT__BEGIN + 15, SPINEL_PROP_THREAD_COMMISSIONER_ENABLED = SPINEL_PROP_THREAD_EXT__BEGIN + 16, SPINEL_PROP_THREAD_TMF_PROXY_ENABLED = SPINEL_PROP_THREAD_EXT__BEGIN + 17, SPINEL_PROP_THREAD_TMF_PROXY_STREAM = SPINEL_PROP_THREAD_EXT__BEGIN + 18, SPINEL_PROP_THREAD_DISCOVERY_SCAN_JOINER_FLAG = SPINEL_PROP_THREAD_EXT__BEGIN + 19, SPINEL_PROP_THREAD_DISCOVERY_SCAN_ENABLE_FILTERING = SPINEL_PROP_THREAD_EXT__BEGIN + 20, SPINEL_PROP_THREAD_DISCOVERY_SCAN_PANID = SPINEL_PROP_THREAD_EXT__BEGIN + 21, SPINEL_PROP_THREAD_STEERING_DATA = SPINEL_PROP_THREAD_EXT__BEGIN + 22, SPINEL_PROP_THREAD_ROUTER_TABLE = SPINEL_PROP_THREAD_EXT__BEGIN + 23, SPINEL_PROP_THREAD_ACTIVE_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 24, SPINEL_PROP_THREAD_PENDING_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 25, SPINEL_PROP_THREAD_MGMT_SET_ACTIVE_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 26, SPINEL_PROP_THREAD_MGMT_SET_PENDING_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 27, SPINEL_PROP_DATASET_ACTIVE_TIMESTAMP = SPINEL_PROP_THREAD_EXT__BEGIN + 28, SPINEL_PROP_DATASET_PENDING_TIMESTAMP = SPINEL_PROP_THREAD_EXT__BEGIN + 29, SPINEL_PROP_DATASET_DELAY_TIMER = SPINEL_PROP_THREAD_EXT__BEGIN + 30, SPINEL_PROP_DATASET_SECURITY_POLICY = SPINEL_PROP_THREAD_EXT__BEGIN + 31, SPINEL_PROP_DATASET_RAW_TLVS = SPINEL_PROP_THREAD_EXT__BEGIN + 32, SPINEL_PROP_THREAD_CHILD_TABLE_ADDRESSES = SPINEL_PROP_THREAD_EXT__BEGIN + 33, SPINEL_PROP_THREAD_NEIGHBOR_TABLE_ERROR_RATES = SPINEL_PROP_THREAD_EXT__BEGIN + 34, SPINEL_PROP_THREAD_ADDRESS_CACHE_TABLE = SPINEL_PROP_THREAD_EXT__BEGIN + 35, SPINEL_PROP_THREAD_UDP_PROXY_STREAM = SPINEL_PROP_THREAD_EXT__BEGIN + 36, SPINEL_PROP_THREAD_MGMT_GET_ACTIVE_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 37, SPINEL_PROP_THREAD_MGMT_GET_PENDING_DATASET = SPINEL_PROP_THREAD_EXT__BEGIN + 38, SPINEL_PROP_DATASET_DEST_ADDRESS = SPINEL_PROP_THREAD_EXT__BEGIN + 39, SPINEL_PROP_THREAD_EXT__END = 0x1600, SPINEL_PROP_IPV6__BEGIN = 0x60, SPINEL_PROP_IPV6_LL_ADDR = SPINEL_PROP_IPV6__BEGIN + 0, SPINEL_PROP_IPV6_ML_ADDR = SPINEL_PROP_IPV6__BEGIN + 1, SPINEL_PROP_IPV6_ML_PREFIX = SPINEL_PROP_IPV6__BEGIN + 2, SPINEL_PROP_IPV6_ADDRESS_TABLE = SPINEL_PROP_IPV6__BEGIN + 3, SPINEL_PROP_IPV6_ROUTE_TABLE, SPINEL_PROP_IPV6_ICMP_PING_OFFLOAD = SPINEL_PROP_IPV6__BEGIN + 5, SPINEL_PROP_IPV6_MULTICAST_ADDRESS_TABLE = SPINEL_PROP_IPV6__BEGIN + 6, SPINEL_PROP_IPV6_ICMP_PING_OFFLOAD_MODE = SPINEL_PROP_IPV6__BEGIN + 7, SPINEL_PROP_IPV6__END = 0x70, SPINEL_PROP_IPV6_EXT__BEGIN = 0x1600, SPINEL_PROP_IPV6_EXT__END = 0x1700, SPINEL_PROP_STREAM__BEGIN = 0x70, SPINEL_PROP_STREAM_DEBUG = SPINEL_PROP_STREAM__BEGIN + 0, SPINEL_PROP_STREAM_RAW = SPINEL_PROP_STREAM__BEGIN + 1, SPINEL_PROP_STREAM_NET = SPINEL_PROP_STREAM__BEGIN + 2, SPINEL_PROP_STREAM_NET_INSECURE = SPINEL_PROP_STREAM__BEGIN + 3, SPINEL_PROP_STREAM_LOG = SPINEL_PROP_STREAM__BEGIN + 4, SPINEL_PROP_STREAM__END = 0x80, SPINEL_PROP_STREAM_EXT__BEGIN = 0x1700, SPINEL_PROP_STREAM_EXT__END = 0x1800, SPINEL_PROP_MESHCOP__BEGIN = 0x80, SPINEL_PROP_MESHCOP_JOINER_STATE = SPINEL_PROP_MESHCOP__BEGIN + 0, SPINEL_PROP_MESHCOP_JOINER_COMMISSIONING = SPINEL_PROP_MESHCOP__BEGIN + 1, SPINEL_PROP_MESHCOP_COMMISSIONER_STATE = SPINEL_PROP_MESHCOP__BEGIN + 2, SPINEL_PROP_MESHCOP_COMMISSIONER_JOINERS = SPINEL_PROP_MESHCOP__BEGIN + 3, SPINEL_PROP_MESHCOP_COMMISSIONER_PROVISIONING_URL = SPINEL_PROP_MESHCOP__BEGIN + 4, SPINEL_PROP_MESHCOP_COMMISSIONER_SESSION_ID = SPINEL_PROP_MESHCOP__BEGIN + 5, SPINEL_PROP_MESHCOP__END = 0x90, SPINEL_PROP_MESHCOP_EXT__BEGIN = 0x1800, SPINEL_PROP_MESHCOP_COMMISSIONER_ANNOUNCE_BEGIN = SPINEL_PROP_MESHCOP_EXT__BEGIN + 0, SPINEL_PROP_MESHCOP_COMMISSIONER_ENERGY_SCAN = SPINEL_PROP_MESHCOP_EXT__BEGIN + 1, SPINEL_PROP_MESHCOP_COMMISSIONER_ENERGY_SCAN_RESULT = SPINEL_PROP_MESHCOP_EXT__BEGIN + 2, SPINEL_PROP_MESHCOP_COMMISSIONER_PAN_ID_QUERY = SPINEL_PROP_MESHCOP_EXT__BEGIN + 3, SPINEL_PROP_MESHCOP_COMMISSIONER_PAN_ID_CONFLICT_RESULT = SPINEL_PROP_MESHCOP_EXT__BEGIN + 4, SPINEL_PROP_MESHCOP_COMMISSIONER_MGMT_GET = SPINEL_PROP_MESHCOP_EXT__BEGIN + 5, SPINEL_PROP_MESHCOP_COMMISSIONER_MGMT_SET = SPINEL_PROP_MESHCOP_EXT__BEGIN + 6, SPINEL_PROP_MESHCOP_EXT__END = 0x1900, SPINEL_PROP_OPENTHREAD__BEGIN = 0x1900, SPINEL_PROP_CHANNEL_MANAGER_NEW_CHANNEL = SPINEL_PROP_OPENTHREAD__BEGIN + 0, SPINEL_PROP_CHANNEL_MANAGER_DELAY = SPINEL_PROP_OPENTHREAD__BEGIN + 1, SPINEL_PROP_CHANNEL_MANAGER_SUPPORTED_CHANNELS = SPINEL_PROP_OPENTHREAD__BEGIN + 2, SPINEL_PROP_CHANNEL_MANAGER_FAVORED_CHANNELS = SPINEL_PROP_OPENTHREAD__BEGIN + 3, SPINEL_PROP_CHANNEL_MANAGER_CHANNEL_SELECT = SPINEL_PROP_OPENTHREAD__BEGIN + 4, SPINEL_PROP_CHANNEL_MANAGER_AUTO_SELECT_ENABLED = SPINEL_PROP_OPENTHREAD__BEGIN + 5, SPINEL_PROP_CHANNEL_MANAGER_AUTO_SELECT_INTERVAL = SPINEL_PROP_OPENTHREAD__BEGIN + 6, SPINEL_PROP_THREAD_NETWORK_TIME = SPINEL_PROP_OPENTHREAD__BEGIN + 7, SPINEL_PROP_TIME_SYNC_PERIOD = SPINEL_PROP_OPENTHREAD__BEGIN + 8, SPINEL_PROP_TIME_SYNC_XTAL_THRESHOLD = SPINEL_PROP_OPENTHREAD__BEGIN + 9, SPINEL_PROP_CHILD_SUPERVISION_INTERVAL = SPINEL_PROP_OPENTHREAD__BEGIN + 10, SPINEL_PROP_CHILD_SUPERVISION_CHECK_TIMEOUT = SPINEL_PROP_OPENTHREAD__BEGIN + 11, SPINEL_PROP_OPENTHREAD__END = 0x2000, SPINEL_PROP_INTERFACE__BEGIN = 0x100, SPINEL_PROP_UART_BITRATE = SPINEL_PROP_INTERFACE__BEGIN + 0, SPINEL_PROP_UART_XON_XOFF = SPINEL_PROP_INTERFACE__BEGIN + 1, SPINEL_PROP_INTERFACE__END = 0x200, SPINEL_PROP_15_4_PIB__BEGIN = 0x400, SPINEL_PROP_15_4_PIB_PHY_CHANNELS_SUPPORTED = SPINEL_PROP_15_4_PIB__BEGIN + 0x01, SPINEL_PROP_15_4_PIB_MAC_PROMISCUOUS_MODE = SPINEL_PROP_15_4_PIB__BEGIN + 0x51, SPINEL_PROP_15_4_PIB_MAC_SECURITY_ENABLED = SPINEL_PROP_15_4_PIB__BEGIN + 0x5d, SPINEL_PROP_15_4_PIB__END = 0x500, SPINEL_PROP_CNTR__BEGIN = 0x500, SPINEL_PROP_CNTR_RESET = SPINEL_PROP_CNTR__BEGIN + 0, SPINEL_PROP_CNTR_TX_PKT_TOTAL = SPINEL_PROP_CNTR__BEGIN + 1, SPINEL_PROP_CNTR_TX_PKT_ACK_REQ = SPINEL_PROP_CNTR__BEGIN + 2, SPINEL_PROP_CNTR_TX_PKT_ACKED = SPINEL_PROP_CNTR__BEGIN + 3, SPINEL_PROP_CNTR_TX_PKT_NO_ACK_REQ = SPINEL_PROP_CNTR__BEGIN + 4, SPINEL_PROP_CNTR_TX_PKT_DATA = SPINEL_PROP_CNTR__BEGIN + 5, SPINEL_PROP_CNTR_TX_PKT_DATA_POLL = SPINEL_PROP_CNTR__BEGIN + 6, SPINEL_PROP_CNTR_TX_PKT_BEACON = SPINEL_PROP_CNTR__BEGIN + 7, SPINEL_PROP_CNTR_TX_PKT_BEACON_REQ = SPINEL_PROP_CNTR__BEGIN + 8, SPINEL_PROP_CNTR_TX_PKT_OTHER = SPINEL_PROP_CNTR__BEGIN + 9, SPINEL_PROP_CNTR_TX_PKT_RETRY = SPINEL_PROP_CNTR__BEGIN + 10, SPINEL_PROP_CNTR_TX_ERR_CCA = SPINEL_PROP_CNTR__BEGIN + 11, SPINEL_PROP_CNTR_TX_PKT_UNICAST = SPINEL_PROP_CNTR__BEGIN + 12, SPINEL_PROP_CNTR_TX_PKT_BROADCAST = SPINEL_PROP_CNTR__BEGIN + 13, SPINEL_PROP_CNTR_TX_ERR_ABORT = SPINEL_PROP_CNTR__BEGIN + 14, SPINEL_PROP_CNTR_RX_PKT_TOTAL = SPINEL_PROP_CNTR__BEGIN + 100, SPINEL_PROP_CNTR_RX_PKT_DATA = SPINEL_PROP_CNTR__BEGIN + 101, SPINEL_PROP_CNTR_RX_PKT_DATA_POLL = SPINEL_PROP_CNTR__BEGIN + 102, SPINEL_PROP_CNTR_RX_PKT_BEACON = SPINEL_PROP_CNTR__BEGIN + 103, SPINEL_PROP_CNTR_RX_PKT_BEACON_REQ = SPINEL_PROP_CNTR__BEGIN + 104, SPINEL_PROP_CNTR_RX_PKT_OTHER = SPINEL_PROP_CNTR__BEGIN + 105, SPINEL_PROP_CNTR_RX_PKT_FILT_WL = SPINEL_PROP_CNTR__BEGIN + 106, SPINEL_PROP_CNTR_RX_PKT_FILT_DA = SPINEL_PROP_CNTR__BEGIN + 107, SPINEL_PROP_CNTR_RX_ERR_EMPTY = SPINEL_PROP_CNTR__BEGIN + 108, SPINEL_PROP_CNTR_RX_ERR_UKWN_NBR = SPINEL_PROP_CNTR__BEGIN + 109, SPINEL_PROP_CNTR_RX_ERR_NVLD_SADDR = SPINEL_PROP_CNTR__BEGIN + 110, SPINEL_PROP_CNTR_RX_ERR_SECURITY = SPINEL_PROP_CNTR__BEGIN + 111, SPINEL_PROP_CNTR_RX_ERR_BAD_FCS = SPINEL_PROP_CNTR__BEGIN + 112, SPINEL_PROP_CNTR_RX_ERR_OTHER = SPINEL_PROP_CNTR__BEGIN + 113, SPINEL_PROP_CNTR_RX_PKT_DUP = SPINEL_PROP_CNTR__BEGIN + 114, SPINEL_PROP_CNTR_RX_PKT_UNICAST = SPINEL_PROP_CNTR__BEGIN + 115, SPINEL_PROP_CNTR_RX_PKT_BROADCAST = SPINEL_PROP_CNTR__BEGIN + 116, SPINEL_PROP_CNTR_TX_IP_SEC_TOTAL = SPINEL_PROP_CNTR__BEGIN + 200, SPINEL_PROP_CNTR_TX_IP_INSEC_TOTAL = SPINEL_PROP_CNTR__BEGIN + 201, SPINEL_PROP_CNTR_TX_IP_DROPPED = SPINEL_PROP_CNTR__BEGIN + 202, SPINEL_PROP_CNTR_RX_IP_SEC_TOTAL = SPINEL_PROP_CNTR__BEGIN + 203, SPINEL_PROP_CNTR_RX_IP_INSEC_TOTAL = SPINEL_PROP_CNTR__BEGIN + 204, SPINEL_PROP_CNTR_RX_IP_DROPPED = SPINEL_PROP_CNTR__BEGIN + 205, SPINEL_PROP_CNTR_TX_SPINEL_TOTAL = SPINEL_PROP_CNTR__BEGIN + 300, SPINEL_PROP_CNTR_RX_SPINEL_TOTAL = SPINEL_PROP_CNTR__BEGIN + 301, SPINEL_PROP_CNTR_RX_SPINEL_ERR = SPINEL_PROP_CNTR__BEGIN + 302, SPINEL_PROP_CNTR_RX_SPINEL_OUT_OF_ORDER_TID = SPINEL_PROP_CNTR__BEGIN + 303, SPINEL_PROP_CNTR_IP_TX_SUCCESS = SPINEL_PROP_CNTR__BEGIN + 304, SPINEL_PROP_CNTR_IP_RX_SUCCESS = SPINEL_PROP_CNTR__BEGIN + 305, SPINEL_PROP_CNTR_IP_TX_FAILURE = SPINEL_PROP_CNTR__BEGIN + 306, SPINEL_PROP_CNTR_IP_RX_FAILURE = SPINEL_PROP_CNTR__BEGIN + 307, SPINEL_PROP_MSG_BUFFER_COUNTERS = SPINEL_PROP_CNTR__BEGIN + 400, SPINEL_PROP_CNTR_ALL_MAC_COUNTERS = SPINEL_PROP_CNTR__BEGIN + 401, SPINEL_PROP_CNTR__END = 0x800, SPINEL_PROP_NEST__BEGIN = 0x3BC0, SPINEL_PROP_NEST_STREAM_MFG = SPINEL_PROP_NEST__BEGIN + 0, SPINEL_PROP_NEST_LEGACY_ULA_PREFIX = SPINEL_PROP_NEST__BEGIN + 1, SPINEL_PROP_NEST_LEGACY_LAST_NODE_JOINED = SPINEL_PROP_NEST__BEGIN + 2, SPINEL_PROP_NEST__END = 0x3C00, SPINEL_PROP_VENDOR__BEGIN = 0x3C00, SPINEL_PROP_VENDOR__END = 0x4000, SPINEL_PROP_DEBUG__BEGIN = 0x4000, SPINEL_PROP_DEBUG_TEST_ASSERT = SPINEL_PROP_DEBUG__BEGIN + 0, SPINEL_PROP_DEBUG_NCP_LOG_LEVEL = SPINEL_PROP_DEBUG__BEGIN + 1, SPINEL_PROP_DEBUG_TEST_WATCHDOG = SPINEL_PROP_DEBUG__BEGIN + 2, SPINEL_PROP_DEBUG__END = 0x4400, SPINEL_PROP_EXPERIMENTAL__BEGIN = 2000000, SPINEL_PROP_EXPERIMENTAL__END = 2097152 } |
| Property Keys. More... | |
| enum | { SPINEL_DATATYPE_NULL_C = 0, SPINEL_DATATYPE_VOID_C = '.', SPINEL_DATATYPE_BOOL_C = 'b', SPINEL_DATATYPE_UINT8_C = 'C', SPINEL_DATATYPE_INT8_C = 'c', SPINEL_DATATYPE_UINT16_C = 'S', SPINEL_DATATYPE_INT16_C = 's', SPINEL_DATATYPE_UINT32_C = 'L', SPINEL_DATATYPE_INT32_C = 'l', SPINEL_DATATYPE_UINT64_C = 'X', SPINEL_DATATYPE_INT64_C = 'x', SPINEL_DATATYPE_UINT_PACKED_C = 'i', SPINEL_DATATYPE_IPv6ADDR_C = '6', SPINEL_DATATYPE_EUI64_C = 'E', SPINEL_DATATYPE_EUI48_C = 'e', SPINEL_DATATYPE_DATA_WLEN_C = 'd', SPINEL_DATATYPE_DATA_C = 'D', SPINEL_DATATYPE_UTF8_C = 'U', SPINEL_DATATYPE_STRUCT_C = 't', SPINEL_DATATYPE_ARRAY_C = 'A' } |
Functions | |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_pack (uint8_t *data_out, spinel_size_t data_len, const char *pack_format,...) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_vpack (uint8_t *data_out, spinel_size_t data_len, const char *pack_format, va_list args) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_unpack (const uint8_t *data_in, spinel_size_t data_len, const char *pack_format,...) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_unpack_in_place (const uint8_t *data_in, spinel_size_t data_len, const char *pack_format,...) |
| This function parses spinel data similar to sscanf(). More... | |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_vunpack (const uint8_t *data_in, spinel_size_t data_len, const char *pack_format, va_list args) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_datatype_vunpack_in_place (const uint8_t *data_in, spinel_size_t data_len, const char *pack_format, va_list args) |
| This function parses spinel data similar to vsscanf(). More... | |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_packed_uint_decode (const uint8_t *bytes, spinel_size_t len, unsigned int *value) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_packed_uint_encode (uint8_t *bytes, spinel_size_t len, unsigned int value) |
| SPINEL_API_EXTERN spinel_ssize_t | spinel_packed_uint_size (unsigned int value) |
| SPINEL_API_EXTERN const char * | spinel_next_packed_datatype (const char *pack_format) |
| SPINEL_API_EXTERN const char * | spinel_prop_key_to_cstr (spinel_prop_key_t prop_key) |
| SPINEL_API_EXTERN const char * | spinel_net_role_to_cstr (uint8_t net_role) |
| SPINEL_API_EXTERN const char * | spinel_mcu_power_state_to_cstr (spinel_mcu_power_state_t mcu_power_state) |
| SPINEL_API_EXTERN const char * | spinel_status_to_cstr (spinel_status_t status) |
| SPINEL_API_EXTERN const char * | spinel_capability_to_cstr (unsigned int capability) |
This file contains definitions of spinel API.
| #define SPINEL_802_15_4_DATATYPE_MAC_SCAN_RESULT_V1_S |
| #define SPINEL_DATATYPE_COMMAND_PROP_S |
| #define SPINEL_DATATYPE_COMMAND_S |
| #define SPINEL_DATATYPE_MAC_SCAN_RESULT_S | ( | mac_format_str, | |
| net_format_str | |||
| ) |
| #define SPINEL_NET_DATATYPE_MAC_SCAN_RESULT_V1_S |
| #define SPINEL_NET_DATATYPE_MAC_SCAN_RESULT_V2_S |
| anonymous enum |
| anonymous enum |
| enum spinel_prop_key_t |
Property Keys.
The properties are broken up into several sections, each with a reserved ranges of property identifiers:
| Name | Range (Inclusive) | Description |
|---|---|---|
| Core | 0x000 - 0x01F, 0x1000 - 0x11FF | Spinel core |
| PHY | 0x020 - 0x02F, 0x1200 - 0x12FF | Radio PHY layer |
| MAC | 0x030 - 0x03F, 0x1300 - 0x13FF | MAC layer |
| NET | 0x040 - 0x04F, 0x1400 - 0x14FF | Network |
| Thread | 0x050 - 0x05F, 0x1500 - 0x15FF | Thread |
| IPv6 | 0x060 - 0x06F, 0x1600 - 0x16FF | IPv6 |
| Stream | 0x070 - 0x07F, 0x1700 - 0x17FF | Stream |
| MeshCop | 0x080 - 0x08F, 0x1800 - 0x18FF | Thread Mesh Commissioning |
| OpenThread | 0x1900 - 0x19FF | OpenThread specific |
| Interface | 0x100 - 0x1FF | Interface (e.g., UART) |
| PIB | 0x400 - 0x4FF | 802.15.4 PIB |
| Counter | 0x500 - 0x7FF | Counters (MAC, IP, etc). |
| Nest | 0x3BC0 - 0x3BFF | Nest (legacy) |
| Vendor | 0x3C00 - 0x3FFF | Vendor specific |
| Debug | 0x4000 - 0x43FF | Debug related |
| Experimental | 2,000,000 - 2,097,151 | Experimental use only |
| enum spinel_status_t |
| SPINEL_API_EXTERN spinel_ssize_t spinel_datatype_unpack_in_place | ( | const uint8_t * | data_in, |
| spinel_size_t | data_len, | ||
| const char * | pack_format, | ||
| ... | |||
| ) |
This function parses spinel data similar to sscanf().
This function actually calls spinel_datatype_vunpack_in_place() to parse data.
| [in] | data_in | A pointer to the data to parse. |
| [in] | data_len | The length of data_in in bytes. |
| [in] | pack_format | C string that contains a format string follows the same specification of spinel. |
| [in] | ... | Additional arguments depending on the format string pack_format. |
spinel_datatype_unpack():spinel_datatype_unpack() expects them of pointer to data type pointer. For example, if SPINEL_DATATYPE_EUI64_C is present in pack_format, this function expects a spinel_eui64_t * is included in variable arguments, while spinel_datatype_unpack() expects a spinel_eui64_t ** is included.SPINEL_DATATYPE_UTF8_C, this function expects two arguments, the first of type char * and the second is of type size_t to indicate length of the provided buffer in the first argument just like strncpy(), while spinel_datatype_unpack() only expects a const char **.| SPINEL_API_EXTERN spinel_ssize_t spinel_datatype_vunpack_in_place | ( | const uint8_t * | data_in, |
| spinel_size_t | data_len, | ||
| const char * | pack_format, | ||
| va_list | args | ||
| ) |
This function parses spinel data similar to vsscanf().
| [in] | data_in | A pointer to the data to parse. |
| [in] | data_len | The length of data_in in bytes. |
| [in] | pack_format | C string that contains a format string follows the same specification of spinel. |
| [in] | args | A value identifying a variable arguments list. |
spinel_datatype_vunpack():spinel_datatype_vunpack() expects them of pointer to data type pointer. For example, if SPINEL_DATATYPE_EUI64_C is present in pack_format, this function expects a spinel_eui64_t * is included in variable arguments, while spinel_datatype_vunpack() expects a spinel_eui64_t ** is included.SPINEL_DATATYPE_UTF8_C, this function expects two arguments, the first of type char * and the second is of type size_t to indicate length of the provided buffer in the first argument just like strncpy(), while spinel_datatype_vunpack() only expects a const char **.