![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.00.00.00
|
Macros | |
| #define | ATT_ERR_ATTR_NOT_FOUND 0x0a |
| No attribute found within the given attribute handle range. | |
| #define | ATT_ERR_ATTR_NOT_LONG 0x0b |
| Attribute cannot be read or written using the Read Blob Request or Prepare Write Request. | |
| #define | ATT_ERR_INSUFFICIENT_AUTHEN 0x05 |
| The attribute requires authentication before it can be read or written. | |
| #define | ATT_ERR_INSUFFICIENT_AUTHOR 0x08 |
| The attribute requires an authorization before it can be read or written. | |
| #define | ATT_ERR_INSUFFICIENT_ENCRYPT 0x0f |
| The attribute requires encryption before it can be read or written. | |
| #define | ATT_ERR_INSUFFICIENT_KEY_SIZE 0x0c |
| The Encryption Key Size used for encrypting this link is insufficient. | |
| #define | ATT_ERR_INSUFFICIENT_RESOURCES 0x11 |
| Insufficient Resources to complete the request. | |
| #define | ATT_ERR_INVALID_HANDLE 0x01 |
| Attribute handle value given was not valid on this attribute server. | |
| #define | ATT_ERR_INVALID_OFFSET 0x07 |
| Offset specified was past the end of the attribute. | |
| #define | ATT_ERR_INVALID_PDU 0x04 |
| The attribute PDU was invalid. | |
| #define | ATT_ERR_INVALID_VALUE 0x80 |
| The attribute value is invalid for the operation. | |
| #define | ATT_ERR_INVALID_VALUE_SIZE 0x0d |
| The attribute value length is invalid for the operation. | |
| #define | ATT_ERR_PREPARE_QUEUE_FULL 0x09 |
| Too many prepare writes have been queued. | |
| #define | ATT_ERR_READ_NOT_PERMITTED 0x02 |
| Attribute cannot be read. | |
| #define | ATT_ERR_UNLIKELY 0x0e |
| The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested. | |
| #define | ATT_ERR_UNSUPPORTED_GRP_TYPE 0x10 |
| The attribute type is not a supported grouping attribute as defined by a higher layer specification. | |
| #define | ATT_ERR_UNSUPPORTED_REQ 0x06 |
| Attribute server doesn't support the request received from the attribute client. | |
| #define | ATT_ERR_WRITE_NOT_PERMITTED 0x03 |
| Attribute cannot be written. | |