ECDSA Parameters. More...
#include <ECDSA.h>
Data Fields | |
ECDSA_ReturnBehavior | returnBehavior |
ECDSA_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
ECDSA Parameters.
ECDSA Parameters are used to with the ECDSA_open() call. Default values for these parameters are set using ECDSA_Params_init().
ECDSA_ReturnBehavior ECDSA_Params_::returnBehavior |
Blocking, callback, or polling return behavior
ECDSA_CallbackFxn ECDSA_Params_::callbackFxn |
Callback function pointer
uint32_t ECDSA_Params_::timeout |
Timeout in system ticks before the operation fails and returns
void* ECDSA_Params_::custom |
Custom argument used by driver implementation