![]() |
![]() |
TRNG driver header.
============================================================================
The True Random Number Generator (TRNG) module generates numbers of variable lengths from a source of entropy. The output is suitable for applications requiring cryptographically random numbers such as keying material for private or symmetric keys.
Before starting a TRNG operation, the application must do the following:
TRNG_generateEntropy() provides the most basic functionality. Use it to generate random numbers of a specified width without further restrictions. An example use-case would be generating a symmetric key for AES encryption and / or authentication.
TRNG_generateEntropyLessThan() returns a random number with the restriction that the random number be less than a specified value. The algorithm used to ensure negligible biasing of the resultant random number is implementation dependent.
TRNG_generateEntropyNonZeroLessThan() also returns a random number with the restriction that the number be less than a specified value. Further, the number will not be zero either. This call specifically is useful if you are trying to generate a private key for use with elliptic curve cryptography. Private keys commonly have the restriction that they be within [1, n - 1], where n is the order of the curve. This function guarantees that you will have an unbiased number in that range when it returns. The algorithm used to ensure negligible biasing of the resultant random number is implementation dependent.
While TRNG_generateEntropyNonZeroLessThan() is guaranteed to produce entropy fit for use in ECC operations, it may not be the most sensible choice. TRNG_generateEntropyNonZeroLessThan() requires overhead both in code size and in run-time and thus power consumption. The order of a curve is often a large number very close to the upper bound of numbers that fit the curve parameter width. This means that, for many curves, it is improbable that a randomly generated number is an invalid private key. The ECDH public key generation functions will reject invalid private keys with an error code. This lets you implement rejection sampling by using the basic TRNG_generateEntropy() to generate a random number and simply generating a new one if the ECDH public key generation function rejects it.
Not all implementations support the more specialized functions as they require efficient operations on large numbers. Usually, this means the device needs a large number maths accelerator or public key accelerator.
After the TRNG operation completes, the application should either start another operation or close the driver by calling TRNG_close().
In order to use the TRNG APIs, the application is required to provide device-specific TRNG configuration in the Board.c file. The TRNG driver interface defines a configuration data structure:
The application must declare an array of TRNG_Config elements, named TRNG_config[]. Each element of TRNG_config[] must be populated with pointers to a device specific TRNG driver implementation's driver object and hardware attributes. The hardware attributes define properties such as the TRNG peripheral's base address. Each element in TRNG_config[] corresponds to a TRNG instance and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as TRNG0 or TRNG1). For example, it is possible to use TRNG_config[0] for TRNG1. Multiple drivers and driver instances may all access the same underlying hardware. This is transparent to the application. Mutual exclusion is performed automatically by the drivers as necessary.
Because the TRNG configuration is very device dependent, you will need to check the doxygen for the device specific TRNG implementation. There you will find a description of the TRNG hardware attributes. Please also refer to the Board.c file of any of your examples to see the TRNG configuration.
The TRNG_Params structure is passed to the TRNG_open() call. If NULL is passed for the parameters, TRNG_open() uses default parameters. A TRNG_Params structure is initialized with default values by passing it to TRNG_Params_init(). Some of the TRNG parameters are described below. To see brief descriptions of all the parameters, see TRNG_Params.
### Generate symmetric encryption key #
### Generate ECC private key #
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Go to the source code of this file.
Data Structures | |
struct | TRNG_Config_ |
TRNG Global configuration. More... | |
struct | TRNG_Params_ |
TRNG Parameters. More... | |
Macros | |
#define | TRNG_CMD_RESERVED (32) |
#define | TRNG_STATUS_RESERVED (-32) |
#define | TRNG_STATUS_SUCCESS (0) |
Successful status code. More... | |
#define | TRNG_STATUS_ERROR (-1) |
Generic error status code. More... | |
#define | TRNG_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by TRNG_control() for undefined command codes. More... | |
#define | TRNG_STATUS_RESOURCE_UNAVAILABLE (-3) |
An error status code returned if the hardware or software resource is currently unavailable. More... | |
Typedefs | |
typedef struct TRNG_Config_ * | TRNG_Handle |
A handle that is returned from a TRNG_open() call. More... | |
typedef enum TRNG_ReturnBehavior_ | TRNG_ReturnBehavior |
The way in which TRNG function calls return after generating the requested entropy. More... | |
typedef struct TRNG_Config_ | TRNG_Config |
TRNG Global configuration. More... | |
typedef void(* | TRNG_CallbackFxn) (TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy) |
The definition of a callback function used by the TRNG driver when used in TRNG_RETURN_BEHAVIOR_CALLBACK. More... | |
typedef struct TRNG_Params_ | TRNG_Params |
TRNG Parameters. More... | |
Enumerations | |
enum | TRNG_ReturnBehavior_ { TRNG_RETURN_BEHAVIOR_CALLBACK = 1, TRNG_RETURN_BEHAVIOR_BLOCKING = 2, TRNG_RETURN_BEHAVIOR_POLLING = 4 } |
The way in which TRNG function calls return after generating the requested entropy. More... | |
Functions | |
void | TRNG_init (void) |
This function initializes the TRNG module. More... | |
void | TRNG_Params_init (TRNG_Params *params) |
Function to initialize the TRNG_Params struct to its defaults. More... | |
TRNG_Handle | TRNG_open (uint_least8_t index, TRNG_Params *params) |
This function opens a given TRNG peripheral. More... | |
void | TRNG_close (TRNG_Handle handle) |
Function to close a TRNG peripheral specified by the TRNG handle. More... | |
int_fast16_t | TRNG_control (TRNG_Handle handle, uint32_t cmd, void *args) |
Function performs implementation specific features on a given TRNG_Handle. More... | |
int_fast16_t | TRNG_generateEntropyLessThan (TRNG_Handle handle, CryptoKey *entropy, const uint8_t *upperBound) |
Generate a random number smaller than a number. More... | |
int_fast16_t | TRNG_generateEntropyNonZeroLessThan (TRNG_Handle handle, CryptoKey *entropy, const uint8_t *upperBound) |
Generate a random number smaller than a number but greater than 0. More... | |
int_fast16_t | TRNG_generateEntropy (TRNG_Handle handle, CryptoKey *entropy) |
Generate a random number. More... | |
Variables | |
const TRNG_Params | TRNG_defaultParams |
Default TRNG_Params structure. More... | |
typedef struct TRNG_Config_* TRNG_Handle |
A handle that is returned from a TRNG_open() call.
typedef enum TRNG_ReturnBehavior_ TRNG_ReturnBehavior |
The way in which TRNG function calls return after generating the requested entropy.
Not all TRNG operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
TRNG functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
Task | Hwi | Swi | |
---|---|---|---|
TRNG_RETURN_BEHAVIOR_CALLBACK | X | X | X |
TRNG_RETURN_BEHAVIOR_BLOCKING | X | ||
TRNG_RETURN_BEHAVIOR_POLLING | X | X | X |
typedef struct TRNG_Config_ TRNG_Config |
TRNG Global configuration.
The TRNG_Config structure contains a set of pointers used to characterize the TRNG driver implementation.
This structure needs to be defined before calling TRNG_init() and it must not be changed thereafter.
typedef void(* TRNG_CallbackFxn) (TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy) |
The definition of a callback function used by the TRNG driver when used in TRNG_RETURN_BEHAVIOR_CALLBACK.
handle | Handle of the client that started the TRNG operation. |
returnValue | Return status code describing the outcome of the operation. |
entropy | The CryptoKey that describes the location the generated entropy will be copied to. |
typedef struct TRNG_Params_ TRNG_Params |
TRNG Parameters.
TRNG Parameters are used to with the TRNG_open() call. Default values for these parameters are set using TRNG_Params_init().
enum TRNG_ReturnBehavior_ |
The way in which TRNG function calls return after generating the requested entropy.
Not all TRNG operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
TRNG functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
Task | Hwi | Swi | |
---|---|---|---|
TRNG_RETURN_BEHAVIOR_CALLBACK | X | X | X |
TRNG_RETURN_BEHAVIOR_BLOCKING | X | ||
TRNG_RETURN_BEHAVIOR_POLLING | X | X | X |
void TRNG_init | ( | void | ) |
This function initializes the TRNG module.
void TRNG_Params_init | ( | TRNG_Params * | params | ) |
Function to initialize the TRNG_Params struct to its defaults.
params | An pointer to TRNG_Params structure for initialization |
Defaults values are: returnBehavior = TRNG_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL
TRNG_Handle TRNG_open | ( | uint_least8_t | index, |
TRNG_Params * | params | ||
) |
This function opens a given TRNG peripheral.
index | Logical peripheral number for the TRNG indexed into the TRNG_config table |
params | Pointer to an parameter block, if NULL it will use default values. |
void TRNG_close | ( | TRNG_Handle | handle | ) |
Function to close a TRNG peripheral specified by the TRNG handle.
handle | A TRNG handle returned from TRNG_open() |
int_fast16_t TRNG_control | ( | TRNG_Handle | handle, |
uint32_t | cmd, | ||
void * | args | ||
) |
Function performs implementation specific features on a given TRNG_Handle.
Commands for TRNG_control can originate from TRNG.h or from implementation specific TRNG*.h (TRNGCC26XX.h, TRNGMSP432.h, etc.. ) files. While commands from TRNG.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific TRNG*.h files add unique driver capabilities but are not API portable across all TRNG driver implementations.
Commands supported by TRNG.h follow a TRNG_CMD_<cmd> naming convention.
Commands supported by TRNG*.h follow a TRNG*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See TRNG_control command codes for command codes.
See TRNG_control return status codes for status codes.
handle | A TRNG handle returned from TRNG_open() |
cmd | TRNG.h or TRNG*.h commands. |
args | An optional R/W (read/write) command argument accompanied with cmd |
int_fast16_t TRNG_generateEntropyLessThan | ( | TRNG_Handle | handle, |
CryptoKey * | entropy, | ||
const uint8_t * | upperBound | ||
) |
Generate a random number smaller than a number.
Generates a random bitstream of the size defined in the entropy
CryptoKey in the range 0 <= entropy
buffer < upperBound
. The entropy will be generated and stored according to the storage requirements defined in the CryptoKey.
upperBound
must have the same length as defined in entropy
.
handle | A TRNG handle returned from TRNG_open(). |
entropy | A blank, initialized CryptoKey describing the target location the entropy shall be stored in. |
upperBound | The uppper bound of numbers returned, exclusive. |
int_fast16_t TRNG_generateEntropyNonZeroLessThan | ( | TRNG_Handle | handle, |
CryptoKey * | entropy, | ||
const uint8_t * | upperBound | ||
) |
Generate a random number smaller than a number but greater than 0.
Generates a random bitstream of the size defined in the entropy
CryptoKey in the range 0 < entropy
buffer < upperBound
. The entropy will be generated and stored according to the storage requirements defined in the CryptoKey.
upperBound
must have the same length as defined in entropy
.
handle | A TRNG handle returned from TRNG_open(). |
entropy | A blank, initialized CryptoKey describing the target location the entropy shall be stored in. |
upperBound | The uppper bound of numbers returned, exclusive. |
int_fast16_t TRNG_generateEntropy | ( | TRNG_Handle | handle, |
CryptoKey * | entropy | ||
) |
Generate a random number.
Generates a random bitstream of the size defined in the entropy
CryptoKey in the range 0 <= entropy
buffer < 2 ^ (entropy length * 8). The entropy will be generated and stored according to the storage requirements defined in the CryptoKey.
handle | A TRNG handle returned from TRNG_open(). |
entropy | A blank, initialized CryptoKey describing the target location the entropy shall be stored in. |
const TRNG_Params TRNG_defaultParams |
Default TRNG_Params structure.