This module includes functions to manage local network data with the OpenThread Border Router.
More...
|
| OTAPI otError OTCALL | otBorderRouterGetNetData (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| | This method provides a full or stable copy of the local Thread Network Data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterAddOnMeshPrefix (otInstance *aInstance, const otBorderRouterConfig *aConfig) |
| | Add a border router configuration to the local network data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterRemoveOnMeshPrefix (otInstance *aInstance, const otIp6Prefix *aPrefix) |
| | Remove a border router configuration from the local network data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig) |
| | This function gets the next On Mesh Prefix in the local Network Data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterAddRoute (otInstance *aInstance, const otExternalRouteConfig *aConfig) |
| | Add an external route configuration to the local network data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterRemoveRoute (otInstance *aInstance, const otIp6Prefix *aPrefix) |
| | Remove an external route configuration from the local network data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig) |
| | This function gets the next external route in the local Network Data. More...
|
| |
| OTAPI otError OTCALL | otBorderRouterRegister (otInstance *aInstance) |
| | Immediately register the local network data with the Leader. More...
|
| |
This module includes functions to manage local network data with the OpenThread Border Router.
§ otBorderRouterAddOnMeshPrefix()
Add a border router configuration to the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aConfig | A pointer to the border router configuration. |
- Return values
-
| OT_ERROR_NONE | Successfully added the configuration to the local network data. |
| OT_ERROR_INVALID_ARGS | One or more configuration parameters were invalid. |
| OT_ERROR_NO_BUFS | Not enough room is available to add the configuration to the local network data. |
- See also
- otBorderRouterRemoveOnMeshPrefix
-
otBorderRouterRegister
§ otBorderRouterAddRoute()
Add an external route configuration to the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aConfig | A pointer to the external route configuration. |
- Return values
-
| OT_ERROR_NONE | Successfully added the configuration to the local network data. |
| OT_ERROR_INVALID_ARGS | One or more configuration parameters were invalid. |
| OT_ERROR_NO_BUFS | Not enough room is available to add the configuration to the local network data. |
- See also
- otBorderRouterRemoveRoute
-
otBorderRouterRegister
§ otBorderRouterGetNetData()
This method provides a full or stable copy of the local Thread Network Data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStable | TRUE when copying the stable version, FALSE when copying the full version. |
| [out] | aData | A pointer to the data buffer. |
| [in,out] | aDataLength | On entry, size of the data buffer pointed to by aData. On exit, number of copied bytes. |
§ otBorderRouterGetNextOnMeshPrefix()
This function gets the next On Mesh Prefix in the local Network Data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first on-mesh entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to the On Mesh Prefix information. |
- Return values
-
| OT_ERROR_NONE | Successfully found the next On Mesh prefix. |
| OT_ERROR_NOT_FOUND | No subsequent On Mesh prefix exists in the Thread Network Data. |
§ otBorderRouterGetNextRoute()
This function gets the next external route in the local Network Data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first external route entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to the External Route information. |
- Return values
-
| OT_ERROR_NONE | Successfully found the next External Route. |
| OT_ERROR_NOT_FOUND | No subsequent external route entry exists in the Thread Network Data. |
§ otBorderRouterRegister()
§ otBorderRouterRemoveOnMeshPrefix()
Remove a border router configuration from the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aPrefix | A pointer to an IPv6 prefix. |
- Return values
-
| OT_ERROR_NONE | Successfully removed the configuration from the local network data. |
| OT_ERROR_NOT_FOUND | Could not find the Border Router entry. |
- See also
- otBorderRouterAddOnMeshPrefix
-
otBorderRouterRegister
§ otBorderRouterRemoveRoute()
Remove an external route configuration from the local network data.
- Parameters
-
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aPrefix | A pointer to an IPv6 prefix. |
- Return values
-
| OT_ERROR_NONE | Successfully removed the configuration from the local network data. |
| OT_ERROR_NOT_FOUND | Could not find the Border Router entry. |
- See also
- otBorderRouterAddRoute
-
otBorderRouterRegister