![]() |
![]() |
Macros | |
| #define | SPI_STATUS_SUCCESS (0) |
| Successful status code returned by SPI_control(). More... | |
| #define | SPI_STATUS_ERROR (-1) |
| Generic error status code returned by SPI_control(). More... | |
| #define | SPI_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by SPI_control() for undefined command codes. More... | |
SPI_STATUS_* macros are general status codes returned by SPI_control()
SPICC26XXDMA_STATUS_* macros are command codes only defined in the SPICC26XXDMA.h driver implementation and need to:
| #define SPI_STATUS_SUCCESS (0) |
Successful status code returned by SPI_control().
SPI_control() returns SPI_STATUS_SUCCESS if the control code was executed successfully.
| #define SPI_STATUS_ERROR (-1) |
Generic error status code returned by SPI_control().
SPI_control() returns SPI_STATUS_ERROR if the control code was not executed successfully.
| #define SPI_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SPI_control() for undefined command codes.
SPI_control() returns SPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.