Create a Downloadable Thread Image

The only supported out-of-box example of a downloadable image for Thread is the oad_cli_<BOARD>_tirtos_ccs project. This is a modified version of the cli_ftd_<BOARD>_tirtos_ccs project. We will be looking at the differences between the two example applications as a case study for adding OAD support to an existing project.

Changes to linker script

One of the major changes between the downloadable CLI example application and the regular CLI example is the linker script. Changes include; reserving space for the metadata headers, reserving the last page of flash, moving the CCFG, and.

To reserve the necessary memory for the image header, a memory section was added to the flash map, this can be seen on line 94 below. As mentioned in OAD Image Header the required size and position is fixed at the base of the flash layout and is 0x100 bytes in size.

Another memory section is reserved for the reset vectors. To ensure that the application’s reset vectors are placed at 0x100, this section is explicitly placed on line 95 below. The length of that section is set at 0x100 to ensure that more than enough room is reserved for the reset vectors.

Finally, as noted in Boot Image Manager (BIM) we need to reserve enough space for the BIM itself. This is defined as the last page in our flash map. This reservation can be seen by noticing that the FLASH_BULK section is 3 pages smaller than the flash size on line 96 below. A section is also added for a debug BIM and CCFG on line 99 below, this is used to place a pre-built BIM and CCFG.

Note

The author of this OAD example application choose to reserve the second and third to last pages of flash for NV storage. This is different than the regular CLI example. Both approaches are valid.

 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
MEMORY
{
    /* Application stored in and executes from internal flash */
    FLASH_IMG_HDR   : origin = FLASH_BASE + 0x000 , length = 0x100
    FLASH_ENTRY     : origin = FLASH_BASE + 0x100 , length = 0x100
    FLASH_BULK (RX) : origin = FLASH_BASE + 0x200 , length = (FLASH_SIZE - (3 * FLASH_SECTOR_SIZE) - 0x200)

    // For CCS - the FLASH_NV is defined by other means
    FLASH_BIM_CCFG (RX)  : origin = FLASH_BIM_CCFG_BASE , length = FLASH_BIM_CCFG_SIZE
    /* Application uses internal RAM for data */
    SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
    /* Application can use GPRAM region as RAM if cache is disabled in the CCFG
    (DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
    GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
}

Then the two new sections need to be filled with information. Place the OAD image header in the flash image header section. And, move the interrupt vectors into the new flash entry section. Don’t forget to rename the placements for the old flash section.

115
116
117
118
119
120
121
122
123
124
125
GROUP > FLASH_IMG_HDR
{
    .oad_image_header
}

GROUP > FLASH_ENTRY
{
    .resetVecs
    .intvecs
    EntrySection LOAD_START(prgEntryAddr)
}

Remove the now unused ccfg placement. For our ti-cgt toolchain examples this usually shows up as .ccfg           :   > FLASH (HIGH) in the linker script.

Remove or change project files

Some files need to be removed from the project to allow placement to continue. Some files need to be added to the project to build the image header. And some files can be optionally added to improve the debug and development experience.

Remove the ccfg.c file from the project. This will prevent the CCFG from being added to the final built image. The CCFG is now owned by the BIM project, and the CC13X2 will use that CCFG.

Add the oad_image_header.c and oad_image_header.h files to your project. These can be copied from the oad_cli_<BOARD>_tirtos_ccs project directly. These source files define the OAD image header that is placed at the origin of the image.

Optionally add the files bim_oad_debug_image_bim.c and bim_oad_debug_image_bim.h files to your project. These are not required for creating a downloadable image. These source files add a C array at the end of flash that is a known good BIM image. This only serves to make programming and debugging within the CCS environment easy. It may be advisable for you to look at the BIM project, or to create your own.

Consult the main_oad.c source file in oad_cli_<BOARD>_tirtos_ccs for a mechanism to erase the CRC metadata in the image header. This will allow you to invalidate your running image and force BIM to reload the factory image.

Add the post-build steps to the project

Finally we need to define the post-build step that takes the *.out file to a *.hex file and finally creating the downloadable *.bin file.

First we need to define the location of the OAD image tool. Open the project properties by right clicking on the project in the project explorer and selecting Properties. Then navigate to the Linked Resources page by selecting ResourceLinked Resources. From there add a new path variable by clicking New... as seen below.

Name OAD_IMAGE_TOOL
Location ${COM_TI_SIMPLELINK_CC13X2_SDK_INSTALL_DIR}\tools\common\oad\bin\${OsType}\oad_image_tool
../_images/fig-define-image-tool.png

Figure 73. Defining the OAD image tool location

Note

CCS may complain that the location does not exist, this is due to the ${OsType} build variable in the path. This variable is only valid at build time.

Finally we need to add the post-build steps to the configuration. In the project’s Properties, navigate to the Build page by selecting Build. Then select the Steps tab and add the following lines to the Post-build steps text box.

${CG_TOOL_HEX} -order MS --memwidth=8 --romwidth=8 --intel -o ${ProjName}.hex ${ProjName}.out
${OAD_IMAGE_TOOL} --verbose ccs ${PROJECT_LOC}/${ConfigName} 7 -hex1 ${ProjName}.hex -o ${ProjName}_oad

This will add the two necessary steps to flatten the image into a *.hex, and create the downloadable *.bin binary.