Setting up the BLE OAD Environment

This section will cover the steps required to setup a BLE OAD environment.

The BLE OAD topology is described below. Refer to Figure 65. for a review of the devices involved in an OAD.

  • OAD Distributor: BTool connected to Host Test on CC13X2 LaunchPad.
  • OAD Target: BLE sample application (simple_peripheral, project_zero) with OAD functionality enabled.

Note

TI provides mobile applications that support OAD, these are outside of the scope of the OAD guide. Refer to the Quick Start Guide for more information.

Prerequisites

This section requires the following hardware and software components

  • 2x CC13X2 LaunchPad
  • SimpleLink CC13X2 SDK installed
  • UNIFLASH installed

OAD Target Setup

In order to perform a BLE OAD, an OAD capable image must be loaded onto the OAD target device. This section will cover the steps required to load the CC13X2 LaunchPad with an OAD enabled BLE image.

  1. Navigate to the simple_peripheral_oad_offchip folder inside the TI-OpenThread Stack.

  2. Import the project into the workspace of your selected IDE.

    • See the Quick Start Guide for instructions on how to work with your selected IDE.
  3. Build the stack project

  4. Build and flash the app project (use debug configuration)

  5. Build the flash the BIM project (Important: Use debug configuration)

    • The BIM debug configuration does not do CRC checks on the image, making it possible to flash an image straight from the IDE.
    • If your device does not boot, it is likely that the release version of BIM, see Loading a Production Image for more info.
  6. Verify the device has booted up and is advertising

    • Verification: Open a terminal window with 115200 8N1 to the XDS110 Class Application/User UART port corresponding to your CC13X2 LaunchPad.
    • The console should display the text below, use it to get the BLE address.
    ../_images/sbp_oad_boot_screen.png
  7. Alternatively, you can get the BLE address of the device using UNIFLASH.

    • See the screenshot below for how to do this in UNIFLASH.
    ../_images/verify_bdaddr_uniflash.png

OAD Distributor Setup

As per the Introduction section, the OAD Distributor is the device responsible for fragmenting an OAD enabled image in to chunks of OAD blocks and sending each block over the to the OAD Target device as they are requested.

In the case of BLE, the OAD Distributor is a combination of BTool running on the PC connected to host_test running on a CC13X2 LaunchPad. host_test is a BLE enabled network processor application. BTool is a PC tool that is capable of interfacing to host_test and performing various BLE functions in addition to OAD. For more information, refer to the host_test README file or the BTool User’s Guide.

Flashing the host_test Image

See below for the steps to setup the host_test image on a CC13X2 LaunchPad.

  1. Navigate to hexfiles folder within the TI-OpenThread Stack.
  2. Select the host_test_*.hex file.
  3. Flash the above hexfile using UNIFLASH. See image below
../_images/host_test_uniflash.png

Connecting BTool to host_test

BTool and host_test communicate via USB through the XDS110 UART back channel. See below for a diagram

../_images/ditaa-a59affabe57be29f72a0c4b1672569165bb04124.png
  1. Find the port used by the UART backchannel of the CC13X2 LaunchPad running host_test. This is the one with the name XDS110 Class Application/User UART

  2. Open BTool (see the BTool executible in the tools folder of the TI-OpenThread Stack)

  3. Use the following serial port settings, hit OK

    • Port: <PORT_FROM_ABOVE_STEP>
    • Other settings: 115200 8N1
  4. This should open and initialize the host_test device.

  5. Pressing the scan button should populate a list of devices in the log

    • A screenshot of a properly initialized BTool session is shown below
    ../_images/btool_init_success.png