![]() |
0.01.00
|
Public Member Functions | |
| ThreadNetif (Instance &aInstance) | |
| This constructor initializes the Thread network interface. More... | |
| otError | Up (void) |
| This method enables the Thread network interface. | |
| otError | Down (void) |
| This method disables the Thread network interface. | |
| bool | IsUp (void) const |
| This method indicates whether or not the Thread network interface is enabled. More... | |
| virtual otError | GetLinkAddress (Ip6::LinkAddress &aAddress) const |
| This method retrieves the link address. More... | |
| virtual otError | SendMessage (Message &aMessage) |
| This method submits a message to the network interface. More... | |
| virtual otError | RouteLookup (const Ip6::Address &aSource, const Ip6::Address &aDestination, uint8_t *aPrefixMatch) |
| This method performs a route lookup. More... | |
| Coap::Coap & | GetCoap (void) |
| This method returns a reference to the CoAP object. More... | |
| Ip6::Filter & | GetIp6Filter (void) |
| This method returns a reference to the IPv6 filter object. More... | |
| KeyManager & | GetKeyManager (void) |
| This method returns a reference to the key manager object. More... | |
| Lowpan::Lowpan & | GetLowpan (void) |
| This method returns a reference to the lowpan object. More... | |
| Mac::Mac & | GetMac (void) |
| This method returns a reference to the mac object. More... | |
| Mle::MleRouter & | GetMle (void) |
| This method returns a reference to the mle object. More... | |
| MeshForwarder & | GetMeshForwarder (void) |
| This method returns a reference to the mesh forwarder object. More... | |
| NetworkData::Leader & | GetNetworkDataLeader (void) |
| This method returns a reference to the network data leader object. More... | |
| MeshCoP::ActiveDataset & | GetActiveDataset (void) |
| This method returns a reference to the active dataset object. More... | |
| MeshCoP::PendingDataset & | GetPendingDataset (void) |
| This method returns a reference to the pending dataset object. More... | |
| AnnounceBeginServer & | GetAnnounceBeginServer (void) |
| This method returns a reference to the announce begin server object. More... | |
| Utils::ChildSupervisor & | GetChildSupervisor (void) |
| This method returns a reference to the child supervisor object. More... | |
| Utils::SupervisionListener & | GetSupervisionListener (void) |
| This method returns a reference to the supervision listener object. More... | |
| EnergyScanServer & | GetEnergyScanServer (void) |
| This method returns a reference to the energy scan server object. More... | |
| PanIdQueryServer & | GetPanIdQueryServer (void) |
| This method returns a reference to the PAN ID query server object. More... | |
| bool | IsTmfMessage (const Ip6::MessageInfo &aMessageInfo) |
| This method returns whether Thread Management Framework Addressing Rules are met. More... | |
Public Member Functions inherited from ot::Ip6::Netif | |
| Netif (Instance &aInstance, int8_t aInterfaceId) | |
| This constructor initializes the network interface. More... | |
| Netif * | GetNext (void) const |
| This method returns the next network interface in the list. More... | |
| int8_t | GetInterfaceId (void) const |
| This method returns the network interface identifier. More... | |
| const NetifUnicastAddress * | GetUnicastAddresses (void) const |
| This method returns a pointer to the list of unicast addresses. More... | |
| otError | AddUnicastAddress (NetifUnicastAddress &aAddress) |
| This method adds a unicast address to the network interface. More... | |
| otError | RemoveUnicastAddress (const NetifUnicastAddress &aAddress) |
| This method removes a unicast address from the network interface. More... | |
| otError | AddExternalUnicastAddress (const NetifUnicastAddress &aAddress) |
| This method adds an external (to OpenThread) unicast address to the network interface. More... | |
| otError | RemoveExternalUnicastAddress (const Address &aAddress) |
| This method removes a external (to OpenThread) unicast address from the network interface. More... | |
| void | RemoveAllExternalUnicastAddresses (void) |
| This method removes all the previously added external (to OpenThread) unicast addresses from the network interface. | |
| bool | IsUnicastAddress (const Address &aAddress) const |
| This method indicates whether or not an address is assigned to this interface. More... | |
| bool | IsMulticastSubscribed (const Address &aAddress) const |
| This method indicates whether or not the network interface is subscribed to a multicast address. More... | |
| otError | SubscribeAllRoutersMulticast (void) |
| This method subscribes the network interface to the link-local and realm-local all routers address. More... | |
| otError | UnsubscribeAllRoutersMulticast (void) |
| This method unsubscribes the network interface to the link-local and realm-local all routers address. More... | |
| const NetifMulticastAddress * | GetMulticastAddresses (void) const |
| This method returns a pointer to the list of multicast addresses. More... | |
| otError | SubscribeMulticast (NetifMulticastAddress &aAddress) |
| This method subscribes the network interface to a multicast address. More... | |
| otError | UnsubscribeMulticast (const NetifMulticastAddress &aAddress) |
| This method unsubscribes the network interface to a multicast address. More... | |
| otError | GetNextExternalMulticast (uint8_t &aIterator, Address &aAddress) |
| This method provides the next external multicast address that the network interface subscribed. More... | |
| otError | SubscribeExternalMulticast (const Address &aAddress) |
| This method subscribes the network interface to the external (to OpenThread) multicast address. More... | |
| otError | UnsubscribeExternalMulticast (const Address &aAddress) |
| This method unsubscribes the network interface to the external (to OpenThread) multicast address. More... | |
| void | UnsubscribeAllExternalMulticastAddresses (void) |
| This method unsubscribes the network interface from all previously added external (to OpenThread) multicast addresses. | |
| bool | IsMulticastPromiscuousEnabled (void) |
| This method checks if multicast promiscuous mode is enabled on the network interface. More... | |
| void | SetMulticastPromiscuous (bool aEnabled) |
| This method enables multicast promiscuous mode on the network interface. More... | |
Public Member Functions inherited from ot::InstanceLocator | |
| Instance & | GetInstance (void) const |
| This method returns a reference to the parent OpenThread Instance. More... | |
| Ip6::Ip6 & | GetIp6 (void) const |
| This method returns a reference to the Ip6. More... | |
| ThreadNetif & | GetNetif (void) const |
| This method returns a reference to the thread network interface. More... | |
| Notifier & | GetNotifier (void) const |
| This method returns a reference to the Notifier. More... | |
Additional Inherited Members | |
Protected Member Functions inherited from ot::InstanceLocator | |
| InstanceLocator (Instance &aInstance) | |
| This constructor initializes the object. More... | |
|
explicit |
This constructor initializes the Thread network interface.
| [in] | aInstance | A reference to the OpenThread instance. |
|
inline |
This method returns a reference to the active dataset object.
|
inline |
This method returns a reference to the announce begin server object.
|
inline |
This method returns a reference to the child supervisor object.
|
inline |
This method returns a reference to the CoAP object.
|
inline |
This method returns a reference to the energy scan server object.
|
inline |
This method returns a reference to the IPv6 filter object.
|
inline |
This method returns a reference to the key manager object.
|
virtual |
This method retrieves the link address.
| [out] | aAddress | A reference to the link address. |
Implements ot::Ip6::Netif.
|
inline |
This method returns a reference to the lowpan object.
|
inline |
This method returns a reference to the mac object.
|
inline |
This method returns a reference to the mesh forwarder object.
|
inline |
This method returns a reference to the mle object.
|
inline |
This method returns a reference to the network data leader object.
|
inline |
This method returns a reference to the PAN ID query server object.
|
inline |
This method returns a reference to the pending dataset object.
|
inline |
This method returns a reference to the supervision listener object.
| bool ot::ThreadNetif::IsTmfMessage | ( | const Ip6::MessageInfo & | aMessageInfo | ) |
This method returns whether Thread Management Framework Addressing Rules are met.
| TRUE | if Thread Management Framework Addressing Rules are met. |
| FALSE | if Thread Management Framework Addressing Rules are not met. |
|
inline |
This method indicates whether or not the Thread network interface is enabled.
| TRUE | If the Thread network interface is enabled. |
| FALSE | If the Thread network interface is not enabled. |
|
virtual |
This method performs a route lookup.
| [in] | aSource | A reference to the IPv6 source address. |
| [in] | aDestination | A reference to the IPv6 destination address. |
| [out] | aPrefixMatch | A pointer where the number of prefix match bits for the chosen route is stored. |
| OT_ERROR_NONE | Successfully found a route. |
| OT_ERROR_NO_ROUTE | Could not find a valid route. |
Implements ot::Ip6::Netif.
This method submits a message to the network interface.
| [in] | aMessage | A reference to the message. |
| OT_ERROR_NONE | Successfully submitted the message to the interface. |
Implements ot::Ip6::Netif.