TI-15.4 Stack API
4.20.00.14
|
#include <api_mac.h>
Data Fields | |
uint16_t | panID |
uint16_t | shortAddress |
ApiMac_sAddrExt_t | extAddress |
Device Descriptor
uint16_t _apimac_devicedescriptor::panID |
The 16-bit PAN identifier of the device
uint16_t _apimac_devicedescriptor::shortAddress |
The 16-bit short address of the device
ApiMac_sAddrExt_t _apimac_devicedescriptor::extAddress |
The 64-bit IEEE extended address of the device. This element is also used inunsecuring operations on incoming frames.