#include <rf_ble_cmd.h>
§ nTxConnectReq
uint8_t rfc_bleInitiatorOutput_s::nTxConnectReq |
Number of transmitted CONNECT_IND (CONNECT_REQ) packets.
§ nRxAdvOk
uint8_t rfc_bleInitiatorOutput_s::nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored.
§ nRxAdvIgnored
uint16_t rfc_bleInitiatorOutput_s::nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored.
§ nRxAdvNok
uint16_t rfc_bleInitiatorOutput_s::nRxAdvNok |
Number of ADV*_IND packets received with CRC error.
§ nRxAdvBufFull
uint8_t rfc_bleInitiatorOutput_s::nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue.
§ lastRssi
int8_t rfc_bleInitiatorOutput_s::lastRssi |
The RSSI of the last received packet (signed)
§ timeStamp
ratmr_t rfc_bleInitiatorOutput_s::timeStamp |
Time stamp of the received ADV*_IND packet that caused transmission of CONNECT_IND (CONNECT_REQ)
The documentation for this struct was generated from the following file: