![]() |
![]() |
TI Easylink API
4.20.00.04
|
Structure for the RX'ed Packet. More...
#include <EasyLink.h>
Public Attributes | |
uint8_t | dstAddr [8] |
Dst Address of RX'ed packet. | |
int8_t | rssi |
rssi of RX'ed packet | |
uint32_t | absTime |
uint32_t | rxTimeout |
uint8_t | len |
length of RX'ed packet | |
uint8_t | payload [128] |
payload of RX'ed packet | |
Structure for the RX'ed Packet.
uint32_t EasyLink_RxPacket::absTime |
Absolute time to turn on Rx when passed (0 for immediate), Or Absolute time that packet was Rx when returned.
uint32_t EasyLink_RxPacket::rxTimeout |
Relative time in ticks from Rx start to Rx TimeOut a value of 0 means no timeout